Start a Movement Challenge
  • Challenges & Projects
  • Design Challenges
  • Start a Movement Challenge
  • More
  • Cancel
Start a Movement Challenge
Forum RangeDetect Rover 4# Quick-built Rover Platform
  • Blog
  • Forum
  • Projects
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join Start a Movement Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 47 subscribers
  • Views 762 views
  • Users 0 members are here
Related

RangeDetect Rover 4# Quick-built Rover Platform

fyaocn
fyaocn over 1 year ago

4# Quick-built Rover Platform

Table of Contents

  • 1 Select Material for Quick-Build
  • 2 Wheels and shaft coupler
  • 3 Chassis
  • 4 Bodywork and Compartment

1 Select Material for Quick-Build

This rover for this project is for prototype, the material shall be easy to cut and flexible to arrange. Hard wood and stacked carton box are used for the framework to hold the stepper motor and TMC5272 driver board.

2 Wheels and shaft coupler

This is shaft coupler with conveyer belt slot.

image

The stepper motor shaft with 5mm diameter. The wheel is 2mm with notch. Best shaft reducer is the one hand-cut on hardwook.

image

This is preassembled shaft coupler and wheel. 

image

image

To save time, this passive ball-type wheel is used as rear wheel.

image

3 Chassis

One hard-pressed carton box is idea for chassis, two stepper motors fixed with screws on opposite sides.

image

image

The torch by the stepper is enough to drive the wheel without gearbox

image

4 Bodywork and Compartment

The box is enough to hold all parts with ease.

image

Then, the rover platform is ready to go.

  • Sign in to reply
  • Cancel
  • DAB
    DAB over 1 year ago

    Looks good.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Christopher678
    Christopher678 over 1 year ago

    Looks fantastic