Summer of FPGA
  • Challenges & Projects
  • Design Challenges
  • Summer of FPGA
  • More
  • Cancel
Summer of FPGA
Blog Number Plate Recognition #2: Working with Verilog
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: taifur
  • Date Created: 4 Jan 2022 12:29 PM Date Created
  • Views 1245 views
  • Likes 3 likes
  • Comments 0 comments
  • xilinx
  • fpga
  • Digilent Cmod S7
  • vivado
  • basic
  • verilog
  • summer of fpga
Related
Recommended

Number Plate Recognition #2: Working with Verilog

taifur
taifur
4 Jan 2022

What is Verilog

Verilog is a Hardware Description Language (HDL). It is a language used for describing a digital system like a network switch or a microprocessor or a memory or a flip−flop. It means, by using an HDL we can describe any digital hardware at any level. Designs, which are described in HDL are independent of technology, very easy for designing and debugging, and are normally more useful than schematics, particularly for large circuits. Verilog is extensively used in FPGA development. 

Verilog supports a digital design at mainly four levels of abstraction. These are −

  • Behavioral level
  • Register-transfer level
  • Gate level
  • Switch level

Behavioral level is the highest level of abstraction providel by Verilog. A module can be implemented in terms of the desired design algorithm without concern for the hardware implementation details. Designing at this level is very similar to C programming.

In gate level design the module is implemented in terms of logic gates and interconnections between these gates. Design at this level is similar to describing a design in terms of a gate-level logic diagram.

The switch level is the lowest level of abstraction provided by Verilog. A module can be implemented in terms of switches, storage nodes, and the interconnections between them. Design at this level requires knowledge of switch-level implementation details.

Verilog allows the designer to mix and match all four levels of abstractions in a design.If a design contains four modules, Verilog allows each of the modules to be written at a different level of abstraction.

Normally, the higher the level of abstraction, the more flexible and technologyindependent the design. As one goes lower toward switch-level design, the design becomes technology-dependent and inflexible. A small modification can cause a significant number of changes in the design.

In this blog post, I will try to show the design of a 4-bit full adder using Verilog and Vivado tools in multiple abstraction level. We will test the design in Cmod 7 board. 

Making the Circuit

We will use a 8 bit DIP switch for providing 4-bit data to the FPGA. 

image

The connection of the DIP switch with FPGA will be as follows:

image

 

For displaying the result we will use the builtin LEDs (LED1-LED4) in the Cmod 7 board. 

image

Verilog Code

Create a new project in Vivado and create a Verilog source file named add4bit and add the following lines of code.

Verilog code for the full adder using behavioral code:

`timescale 1ns / 1ps


module add4bit(A, B, Cin, SUM, Cout);

input [3:0] A, B;
input Cin;

output [3:0] SUM;
output Cout;

assign {Cout, SUM} = A + B + Cin;

endmodule

When programming an FPGA through software such as Xilinx's Vivado, you need to inform the software what physical pins on the FPGA you plan on using or connecting to in relation to the HDL code that you wrote to describe the behavior of the FPGA. For example in our adder circuit, we are going to use 4 LEDs for the output, and LEDs are connected according to the following schematic in the Cmod 7 board.

image

Usually we create a hardware interface in HDL and then constrain the corresponding inputs and outputs on that interface to (essentially) whichever pins you want on the FPGA, making FPGAs very flexible for complex and custom designs.

For our connections the XDC files or constraint files is:

set_property IOSTANDARD LVCMOS33 [get_ports {A[3]}]
set_property IOSTANDARD LVCMOS33 [get_ports {A[2]}]
set_property IOSTANDARD LVCMOS33 [get_ports {A[1]}]
set_property IOSTANDARD LVCMOS33 [get_ports {A[0]}]
set_property IOSTANDARD LVCMOS33 [get_ports {B[3]}]
set_property IOSTANDARD LVCMOS33 [get_ports {B[2]}]
set_property IOSTANDARD LVCMOS33 [get_ports {B[1]}]
set_property IOSTANDARD LVCMOS33 [get_ports {B[0]}]
set_property IOSTANDARD LVCMOS33 [get_ports {SUM[3]}]
set_property IOSTANDARD LVCMOS33 [get_ports {SUM[2]}]
set_property IOSTANDARD LVCMOS33 [get_ports {SUM[1]}]
set_property IOSTANDARD LVCMOS33 [get_ports {SUM[0]}]
set_property PACKAGE_PIN A2 [get_ports {A[0]}]
set_property PACKAGE_PIN B2 [get_ports {A[1]}]
set_property PACKAGE_PIN B1 [get_ports {A[2]}]
set_property PACKAGE_PIN C1 [get_ports {A[3]}]
set_property PACKAGE_PIN B3 [get_ports {B[0]}]
set_property PACKAGE_PIN B4 [get_ports {B[1]}]
set_property PACKAGE_PIN A3 [get_ports {B[2]}]
set_property PACKAGE_PIN A4 [get_ports {B[3]}]
set_property PACKAGE_PIN E2 [get_ports {SUM[0]}]
set_property PACKAGE_PIN K1 [get_ports {SUM[1]}]
set_property PACKAGE_PIN J1 [get_ports {SUM[2]}]
set_property PACKAGE_PIN E1 [get_ports {SUM[3]}]
set_property IOSTANDARD LVCMOS33 [get_ports Cin]
set_property IOSTANDARD LVCMOS33 [get_ports Cout]
set_property PACKAGE_PIN C5 [get_ports Cin]
set_property PACKAGE_PIN F2 [get_ports Cout]

After RTL analysis of the above Verilog code we will get the following schematic.

image

After RTL analysis the constrain file can be made graphically in Vivado from I/O Planing option from the top right corner of the Vivado. Then you can select the direction of the pins and the voltage level from the I/O ports tab shown in the following figure. 

image

You can also write Verilog code using structural method. The structural Verilog code for the full adder based on its logic diagram can be define as follows:

image
module fulladder(X, Y, Ci, S, Co);
  input X, Y, Ci;
  output S, Co;
  wire w1,w2,w3;
  //Structural code for one bit full adder
  xor G1(w1, X, Y);
  xor G2(S, w1, Ci);
  and G3(w2, w1, Ci);
  and G4(w3, X, Y);
  or G5(Co, w2, w3);
endmodule
Then, instantiate the full adders in a Verilog module to create a 4-bit ripple-carry adder using structural modeling. 

Following is the Verilog code for the 4-bit ripple-carry adder:

module rippe_adder(X, Y, S, Co);
 input [3:0] X, Y;// Two 4-bit inputs
 output [3:0] S;
 output Co;
 wire w1, w2, w3;
 // instantiating 4 1-bit full adders in Verilog
 fulladder u1(X[0], Y[0], 1'b0, S[0], w1);
 fulladder u2(X[1], Y[1], w1, S[1], w2);
 fulladder u3(X[2], Y[2], w2, S[2], w3);
 fulladder u4(X[3], Y[3], w3, S[3], Co);
endmodule

The following image represents the hardware connection for Cmod 7 board: I used 1ohm resistor instead of jumper wire for connecting the switch with 3.3V supply. Direct connection will be ok.