Summer of FPGA
  • Challenges & Projects
  • Design Challenges
  • Summer of FPGA
  • More
  • Cancel
Summer of FPGA
Blog Number Plate Recognition #5: Connecting OV7670 Camera to Cmod 7
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: taifur
  • Date Created: 22 Jan 2022 2:38 AM Date Created
  • Views 3737 views
  • Likes 4 likes
  • Comments 0 comments
  • spartan 7
  • xilinx
  • summer of fpgas
  • verilog
  • summer of fpga
Related
Recommended

Number Plate Recognition #5: Connecting OV7670 Camera to Cmod 7

taifur
taifur
22 Jan 2022

For image recognition first, we need to capture an image using the FPGA. We will use an OV7670 CMOS camera for capturing real-time images for our project. The OV7670 is a CMOS parallel camera with VGA resolution from OmniVision. The camera has an image array of 656x488 pixels, of which 640x480 pixels are active. The camera can operate from 1.7 to 3V. The camera interface consists of a parallel 8-bit bus, synchronization signals VSYNC and HSYNC, pixel clock, master clock, and reset and power down signals.

image

image

image

Source: https://www.hackster.io/dhq/fpga-camera-system-14d6ea

The camera interfacing code consists of two main modules. The input capture image and the camera configuration image. The input capture code is responsible for transmitting the pixels to the frame buffer. This module decodes the pixels coming from the camera. Each pixel is packed into 2 consecutive bytes. The Input capture module converts this to RGB444. This is done to save space since the VGA interface uses an RGB444 interface. The camera supports multiple pixel image formats however the one selected in this application is RGB565 meaning Red, Green, and Blue gets 5, 6, and 5 pixels each respectively.

image

The camera is configured via SCCB (Serial Camera Communication Bus). This is mostly compatible with I2C.

To interface with the OV7670 camera, the followings are the most critical steps and modules:
1. Camera configuration (OV7670_controller.vhd): To configure the OV7670 camera properly, check its datasheet to know which communication protocol it supports for configuration and capturing data. In this case, it is an I2C-like SSCB interface so an I2C code is needed to communicate with the camera, configure it, and get image data. To configure it properly, check the device control register list. Beside the configuration for the output format (RGB, QVGA, QCIF, etc.), RGB format (RGB565, RGB555, etc.), timing signals (PCLK, HREF, VSYNC),   the matrix coefficients including MTX1-MTX6 are important factors deciding the output image quality. 
image
I2C-like SCCB interface for communicating with the OV7670 camera
2. Capturing image data (OV7670_capture.vhd): After configuring the camera, the next step is to capture the image data. One more time, check the datasheet of the camera to see the output timing diagram of your selected output format. For example, in this project, the RGB565 format is chosen so the output timing diagram for RGB565 is used for properly capturing the RGB data from the output signals of the camera. Based on the timing diagram as follows, the OV7670_capture.vhd is designed.
image
 
3. Saving Image Data (frame_buffer.vhd): After being able to configure the camera and capture the image data properly, the image data is stored in an intermediate memory. To use the same settings for the camera and VGA controller with a full 640x480 image size without exceeding the BRAM of FPGA, the trick is to save only one pixel every 4 pixels for the 640x480 size. 
We can get the newly updated frame buffer with 17-bit RAM address as follows:
LIBRARY ieee;
USE ieee.std_logic_1164.ALL;
USE ieee.numeric_std.ALL;

LIBRARY blk_mem_gen_v8_4_0;
USE blk_mem_gen_v8_4_0.blk_mem_gen_v8_4_0;

ENTITY frame_buffer IS
  PORT (
    clka : IN STD_LOGIC;
    wea : IN STD_LOGIC_VECTOR(0 DOWNTO 0);
    addra : IN STD_LOGIC_VECTOR(16 DOWNTO 0);
    dina : IN STD_LOGIC_VECTOR(11 DOWNTO 0);
    clkb : IN STD_LOGIC;
    addrb : IN STD_LOGIC_VECTOR(16 DOWNTO 0);
    doutb : OUT STD_LOGIC_VECTOR(11 DOWNTO 0)
  );
END frame_buffer;

The top-level VHDL sample code for the OV7670 camera for an FPGA is:

library IEEE;
use IEEE.STD_LOGIC_1164.ALL;
entity top_level is
    Port ( clk100          : in  STD_LOGIC;
           btnl            : in  STD_LOGIC;
           btnc            : in  STD_LOGIC;
           btnr            : in  STD_LOGIC;
           config_finished : out STD_LOGIC;
           
           vga_hsync : out  STD_LOGIC;
           vga_vsync : out  STD_LOGIC;
           vga_r     : out  STD_LOGIC_vector(3 downto 0);
           vga_g     : out  STD_LOGIC_vector(3 downto 0);
           vga_b     : out  STD_LOGIC_vector(3 downto 0);
           
           ov7670_pclk  : in  STD_LOGIC;
           ov7670_xclk  : out STD_LOGIC;
           ov7670_vsync : in  STD_LOGIC;
           ov7670_href  : in  STD_LOGIC;
           ov7670_data  : in  STD_LOGIC_vector(7 downto 0);
           ov7670_sioc  : out STD_LOGIC;
           ov7670_siod  : inout STD_LOGIC;
           ov7670_pwdn  : out STD_LOGIC;
           ov7670_reset : out STD_LOGIC
           );
end top_level;
architecture Behavioral of top_level is

 COMPONENT VGA
 PORT(
  CLK25 : IN std_logic;    
                rez_160x120 : IN std_logic;
                rez_320x240 : IN std_logic;
  Hsync : OUT std_logic;
  Vsync : OUT std_logic;
  Nblank : OUT std_logic;      
  clkout : OUT std_logic;
  activeArea : OUT std_logic;
  Nsync : OUT std_logic
  );
 END COMPONENT;

 COMPONENT ov7670_controller
 PORT(
  clk : IN std_logic;
  resend : IN std_logic;    
  siod : INOUT std_logic;      
  config_finished : OUT std_logic;
  sioc : OUT std_logic;
  reset : OUT std_logic;
  pwdn : OUT std_logic;
  xclk : OUT std_logic
  );
 END COMPONENT;

 COMPONENT debounce
 PORT(
  clk : IN std_logic;
  i : IN std_logic;          
  o : OUT std_logic
  );
 END COMPONENT;

 COMPONENT frame_buffer
  PORT (
      clka : IN STD_LOGIC;
      wea : IN STD_LOGIC_VECTOR(0 DOWNTO 0);
      addra : IN STD_LOGIC_VECTOR(16 DOWNTO 0);
      dina : IN STD_LOGIC_VECTOR(11 DOWNTO 0);
      clkb : IN STD_LOGIC;
      addrb : IN STD_LOGIC_VECTOR(16 DOWNTO 0);
      doutb : OUT STD_LOGIC_VECTOR(11 DOWNTO 0)
    );
 END COMPONENT;
 COMPONENT ov7670_capture
 PORT(
                rez_160x120 : IN std_logic;
                rez_320x240 : IN std_logic;
  pclk : IN std_logic;
  vsync : IN std_logic;
  href : IN std_logic;
  d : IN std_logic_vector(7 downto 0);          
  addr : OUT std_logic_vector(18 downto 0);
  dout : OUT std_logic_vector(11 downto 0);
  we : OUT std_logic
  );
 END COMPONENT;
 COMPONENT RGB
 PORT(
  Din : IN std_logic_vector(11 downto 0);
  Nblank : IN std_logic;          
  R : OUT std_logic_vector(7 downto 0);
  G : OUT std_logic_vector(7 downto 0);
  B : OUT std_logic_vector(7 downto 0)
  );
 END COMPONENT;
 component clocking
 port (
                CLK_100           : in     std_logic;
                -- Clock out ports
                CLK_50          : out    std_logic;
                CLK_25          : out    std_logic);
 end component;
 COMPONENT Address_Generator
 PORT(
  CLK25       : IN  std_logic;
                rez_160x120 : IN std_logic;
                rez_320x240 : IN std_logic;
  enable      : IN  std_logic;       
                vsync       : in  STD_LOGIC;
  address     : OUT std_logic_vector(18 downto 0)
  );
 END COMPONENT;
   signal clk_camera : std_logic;
   signal clk_vga    : std_logic;
   signal wren       : std_logic_vector(0 downto 0);
   signal resend     : std_logic;
   signal nBlank     : std_logic;
   signal vSync      : std_logic;
   signal nSync      : std_logic;
   
   signal wraddress  : std_logic_vector(18 downto 0);
   signal wrdata     : std_logic_vector(11 downto 0);
   
   signal rdaddress  : std_logic_vector(18 downto 0);
   signal rddata     : std_logic_vector(11 downto 0);
   signal red,green,blue : std_logic_vector(7 downto 0);
   signal activeArea : std_logic;
   
   signal rez_160x120 : std_logic;
   signal rez_320x240 : std_logic;
   signal size_select: std_logic_vector(1 downto 0);
   signal rd_addr,wr_addr  : std_logic_vector(16 downto 0);
begin
   vga_r <= red(7 downto 4);
   vga_g <= green(7 downto 4);
   vga_b <= blue(7 downto 4);
   
   rez_160x120 <= btnl;
   rez_320x240 <= btnr;
   your_instance_name : clocking
     port map
      (-- Clock in ports
       CLK_100 => CLK100,
       -- Clock out ports
       CLK_50 => CLK_camera,
       CLK_25 => CLK_vga);
       vga_vsync <= vsync;
   
 Inst_VGA: VGA PORT MAP(
  CLK25      => clk_vga,
                rez_160x120 => rez_160x120,
                rez_320x240 => rez_320x240,
  clkout     => open,
  Hsync      => vga_hsync,
  Vsync      => vsync,
  Nblank     => nBlank,
  Nsync      => nsync,
                activeArea => activeArea
 );
 Inst_debounce: debounce PORT MAP(
  clk => clk_vga,
  i   => btnc,
  o   => resend
 );
 Inst_ov7670_controller: ov7670_controller PORT MAP(
  clk             => clk_camera,
  resend          => resend,
  config_finished => config_finished,
  sioc            => ov7670_sioc,
  siod            => ov7670_siod,
  reset           => ov7670_reset,
  pwdn            => ov7670_pwdn,
  xclk            => ov7670_xclk
 );
 size_select <= btnl&btnr;

    with size_select select 
    rd_addr <= rdaddress(18 downto 2) when "00",
        rdaddress(16 downto 0) when "01",
        rdaddress(16 downto 0) when "10",
        rdaddress(16 downto 0) when "11";

   with size_select select 
    wr_addr <= wraddress(18 downto 2) when "00",
            wraddress(16 downto 0) when "01",
            wraddress(16 downto 0) when "10",
            wraddress(16 downto 0) when "11";
 Inst_frame_buffer: frame_buffer PORT MAP(
  addrb => rd_addr,
  clkb   => clk_vga,
  doutb        => rddata,
      
  clka   => ov7670_pclk,
  addra => wr_addr,
  dina      => wrdata,
  wea      => wren
 );
 Inst_ov7670_capture: ov7670_capture PORT MAP(
  pclk  => ov7670_pclk,
                rez_160x120 => rez_160x120,
                rez_320x240 => rez_320x240,
  vsync => ov7670_vsync,
  href  => ov7670_href,
  d     => ov7670_data,
  addr  => wraddress,
  dout  => wrdata,
  we    => wren(0)
 );
 Inst_RGB: RGB PORT MAP(
  Din => rddata,
  Nblank => activeArea,
  R => red,
  G => green,
  B => blue
 );
 Inst_Address_Generator: Address_Generator PORT MAP(
  CLK25 => clk_vga,
                rez_160x120 => rez_160x120,
                rez_320x240 => rez_320x240,
  enable => activeArea,
                vsync  => vsync,
  address => rdaddress
 );
end Behavioral;

The main code was collected from here.

Camera Connection to Cmod 7 board

image

image

  • OV7670.pdf
  • View
  • Hide