Summer of FPGA
  • Challenges & Projects
  • Design Challenges
  • Summer of FPGA
  • More
  • Cancel
Summer of FPGA
Blog Security Hardware Accelerator #2 Reinstall Vitis and Add board support
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fyaocn
  • Date Created: 1 Dec 2021 6:35 AM Date Created
  • Views 1697 views
  • Likes 5 likes
  • Comments 2 comments
Related
Recommended

Security Hardware Accelerator #2 Reinstall Vitis and Add board support

fyaocn
fyaocn
1 Dec 2021

1. Reinstall the Vitis With Vivado

I have use the vitis in Ubuntu 18.02, not board support for CMOS-S4 is proper installed. Then I reinstall the Vitis in Windows 10 and added the Board support. 

image

image

Then Installing Digilent Board Files, Download the most recent Master Branch ZIP Archive of Digilent's vivado-boards Github repository and extract it.I prefer to use git instead of SDKs.

Find the file “Vivado_init.tcl” in the “utility” subdirectory of the vivado-boards repo. Copy and paste it into the %APPDATA%/Xilinx/Vivado/ directory for Windows. This file is a script that will be run whenever Vivado is launched. It will load Digilent's board files for use in Vivado from the directory they were extracted into.

image

Open the copied init script in a text editor. Change the text <extracted path> in the script to the path to the extracted vivado-boards folder. Save and close the file. This script sets the board.repoPaths parameter to a fixed path. The script is run whenever any version of Vivado is launched, and the parameter for that version of Vivado will remain.

image

The board support is installed.

2. Create new project with board support.

Create new project with vivado.

image

set project name

image

select project type with RTL project, 

image

tick the choice Do not specifiy sources at this time, if use board support,

image

If it appears that mean the board support is installed.Then select board.

image

Complete the initiantion setup and press finish.

image

3. Design the project bareboard

The sample project used Vivado with guide can not be used well with Vitis, the new Norm by Xilinx. I shall use VItis after create the board template.

image

  • Sign in to reply
  • fyaocn
    fyaocn over 4 years ago

    better refer to https://digilent.com/reference/programmable-logic/guides/getting-started-with-ipi

    Vivado can be used indendantly. Vitis is new with more control in coding, I am studying how to use it and post blog later.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago

    When you install the board file in Vitis, can you please document the steps here?
    I was able to install my board file in Vivado, but not in Vitis yet.