Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe and Sound - MSP-EXP432P401 & Sharp LCD - blog 8
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
  • Author Author: dougw
  • Date Created: 12 Mar 2017 3:24 AM Date Created
  • Views 2438 views
  • Likes 6 likes
  • Comments 10 comments
  • safe and sound
  • safe and sound design challenge
  • hazardous_environmental_factors
  • invisible_hazards
  • safe & sound
  • wearable technology
  • Wearables
  • safe&sound
  • doug_wong
Related
Recommended

Safe and Sound - MSP-EXP432P401 & Sharp LCD - blog 8

dougw
dougw
12 Mar 2017

This update covers my first attempt to fire up the  MSP-EXP432P401RMSP-EXP432P401R I am using Energia at this point since they claim to support this platform and the Sharp display.

I modified the  430BOOST-SHARP96430BOOST-SHARP96 to be always enabled by unsoldering the R16 zero ohm resistor and soldering it at the R17 location. This is needed in my design to avoid a conflicting use of one of the GPIO pins. (It conflicts with the CC3100 Boosterpack)

image

Here is the corresponding schematic:

image

The Sharp Boosterpack LCD plugs directly on the  MSP-EXP432P401RMSP-EXP432P401R as shown below

image

You can see the results of my first code in the picture.

Here is the source code:

 

//  Hazardous Gas Sensor Module

//  MSP_EXP432P401R

  430BOOST-SHARP96430BOOST-SHARP96

  CC3100MODBOOSTCC3100MODBOOST

//  MQx_Sensor Boosterpack

//  Author :  Doug Wong

//  Date   :  Mar 11, 2017

//  Version:  1.00

//

//

 

 

// Include application, user and local libraries

#include "SPI.h"

#include "OneMsTaskTimer.h"

#include "LCD_SharpBoosterPack_SPI.h"

 

 

// Variables

LCD_SharpBoosterPack_SPI myScreen;

int AlcPin = A11;           //MQ3 - Alcohol

int COPin = A14;            //MQ7 - Carbo Monoxide

int AQPin = A13;            //MQ135 - Air Quality

int CO2Pin = A8;            //CO2

int UVPin = A9;             //Ultraviolet Light

int AlcValue = 0;           //MQ3 - Alcohol

int COValue = 0;            //MQ7 - Carbo Monoxide

int AQValue = 0;            //MQ135 - Air Quality

int CO2Value = 0;           //CO2

int UVValue = 0;            //Ultraviolet Light

String AlcStr;

String COStr;

String AQStr;

String CO2Str;

String UVStr;

 

 

// setup code

void setup() {

    Serial.begin(9600);

    myScreen.begin();

  

// setup LCD to display sensor data

    myScreen.clearBuffer();

  

    myScreen.setFont(1);

    myScreen.text(5, 1, "SENSORS");

    myScreen.setFont(0);

    myScreen.text(3, 22, "Alc         ppm");

    myScreen.text(3, 37, "CO          ppm");

    myScreen.text(3, 52, "AQ          ppm");

    myScreen.text(3, 67, "CO2         ppm");

    myScreen.text(3, 82, "UV          idx");

    myScreen.flush();

}

 

 

// loop to read and display sensor data

void loop()

{

  AlcValue = analogRead(AlcPin);    //read Alcohol sensor

  COValue = analogRead(COPin);      //read CO sensor

  AQValue = analogRead(AQPin);      //read Air Quality sensor

  CO2Value = analogRead(CO2Pin);    //read CO2 sensor

  UVValue = analogRead(UVPin);      //read UV sensor

 

 

  AlcStr = String(AlcValue);        //convert reading to ASCII

  COStr = String(COValue);          //convert reading to ASCII

  AQStr = String(AQValue);          //convert reading to ASCII

  CO2Str = String(CO2Value);        //convert reading to ASCII

  UVStr = String(UVValue);          //convert reading to ASCII

 

    myScreen.setFont(0);

    myScreen.text(33, 22, AlcStr + "   ");  //display alcohol

    myScreen.text(33, 37, COStr + "   ");   //display CO

    myScreen.text(33, 52, AQStr + "   ");   //display Air Quality

    myScreen.text(33, 67, CO2Str + "   ");  //display CO2

    myScreen.text(33, 82, UVStr + "   ");   //display UV

    myScreen.flush();

  

  delay(100);

}

 

One thing to note - the Energia selector for the target board did not show the MSP-EXP432P401RMSP-EXP432P401Rin its list it just showed Launchpad /w MSP432 EMT (48MHz)" - but it seems to work.

I do not have my sensor Boosterpack back from the PCB shop yet, so I connected 5 potentiometers to simulate the 5 sensors.

Here is a demo video of the system in action:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

My next blog is likely to be about ELF radiation or maybe I will cover all RF in one blog.

The Boosterpack PCB I designed has shipped but not arrived, so that is also a possibility.

 

All links to blogs related to this project can be found in the first blog here:

Safe and Sound - Invisible Hazardous Environmental Factors Monitoring System - blog 1

  • Sign in to reply

Top Comments

  • dwinhold
    dwinhold over 9 years ago +3
    Here is an update... It is ok to laugh... I just completed the change on my 430BOOST-SHARP96 of moving the R16 0 ohm resistor to R17.... But not without issues.... De-soldering went without a hitch, picked…
  • mcb1
    mcb1 over 9 years ago in reply to dwinhold +3
    Product Link Product Link Same thing happened when we were fixing my Intel Edison breakout board. The regulator chip went flying .... luckily I ordered two. To help remedy this I brought one of these for…
  • dougw
    dougw over 9 years ago in reply to dwinhold +2
    All I know is when it happens to me, it is the opposite of a laughing matter. The expletives can be significantly more vehement that you would expect from loss of a 1 cent part. A piece of wire can be…
Parents
  • dwinhold
    dwinhold over 9 years ago

    Here is an update... It is ok to laugh...

     

    I just completed the change on my 430BOOST-SHARP96 of moving the R16 0 ohm resistor to R17.... But not without issues.... De-soldering went without a hitch, picked up the resistor with tweezers and proceeded to set in place. This is where the issue occurred, the resistor popped out of my tweezers grip and landed...... Who knows where... Lets look for it, it is either on the cluttered work table with 5000 other lost items or on the carpet floor... Hmmmm, I couldn't see it without a magnifying glass already, not much hope finding it. Lets start looking for another resistor to use, luckily I found one on another board I saved. Works great now.

     

    Dale

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to dwinhold

    Product LinkProduct Link

    Same thing happened when we were fixing my Intel Edison breakout board.

    The regulator chip went flying .... luckily I ordered two.

     

     

    To help remedy this I brought one of these for $20

    image

    Product LinkProduct Link

     

    Not sure how it will go, but worth a try.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dwinhold
    dwinhold over 9 years ago in reply to mcb1

    I did solve the problem but I like the pickup tool. I will be ordering it very soon.

     

    Thank you for the tip and Link!!

     

    Dale

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to dwinhold

    You're welcome.

    It's a weird device where the handle where the fingers touch is a flexible tube.

    You squeeze it and place it over the part then let go. The vacuum should hold it.

     

    I wouldn't recommend going for long walks, but it should (I hope) hold it long enough to get it over the board.

     

    Most vacuum tools have a constant suction, so leakage within reason will still hold the part.

    This has none of that, and having seen the surface of the regulator chip, I'm wondering if it will seal.

     

     

    Regardless it was low cost and looks like it can be adapted if required.

     

    shabaz has been building his own device

    Building a SMT Pick-and-Place Buddy

     

    rachaelp has also been building one

    Lab Equipment Projects - Vacuum Pick and Place Assistant Part 1 - Overview

    Lab Equipment Projects - Vacuum Pick and Place Assistant Part 2 - Prototype Design

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 9 years ago in reply to dwinhold

    You're welcome.

    It's a weird device where the handle where the fingers touch is a flexible tube.

    You squeeze it and place it over the part then let go. The vacuum should hold it.

     

    I wouldn't recommend going for long walks, but it should (I hope) hold it long enough to get it over the board.

     

    Most vacuum tools have a constant suction, so leakage within reason will still hold the part.

    This has none of that, and having seen the surface of the regulator chip, I'm wondering if it will seal.

     

     

    Regardless it was low cost and looks like it can be adapted if required.

     

    shabaz has been building his own device

    Building a SMT Pick-and-Place Buddy

     

    rachaelp has also been building one

    Lab Equipment Projects - Vacuum Pick and Place Assistant Part 1 - Overview

    Lab Equipment Projects - Vacuum Pick and Place Assistant Part 2 - Prototype Design

     

    Mark