Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe and Sound Wearables- Hearing Guard System #10: Creating Graphics
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
  • Author Author: jomoenginer
  • Date Created: 1 May 2017 12:14 AM Date Created
  • Views 2135 views
  • Likes 6 likes
  • Comments 11 comments
  • 430boost-sharp96
  • msp430 image reformer*
  • msp430 image reforme*
  • msp432
Related
Recommended

Safe and Sound Wearables- Hearing Guard System #10: Creating Graphics

jomoenginer
jomoenginer
1 May 2017

Creating Graphics for the Sharp LCD

 

Hardware:

SimpleLinkTm MSP432P401R LaunchPad

430BOOST-SHARP96

 

Software:

MSP Graphics Library

Image Reformer Tool

Microsoft Paint

 

From the inception of my project I had an idea of a graphic image that I wanted to represent the project but I was not sure how to get this created and added to the MSP432 to display on the the Sharp 96x96 LCD booster.  I had taken the Valvano Embedded MOOCs on edX and tried to use the example that was used in the courses, but these did not work with the grlib and LCD code I have with TI-RTOS.  After some searching, I found that TI provided a nifty tool that can take an image and convert to a '.c' file which can be added to the exist code to display the image on a LCD such as the Sharp LCD Booster pack.

 

The tool is the MSP430 Image Reformer Tool which is found in the MSP GRLIB Graphics Library download

.

http://www.ti.com/tool/msp-grlib

 

The code produced from this tool is compatible with the MSP430 and MSP432 line of Launchpads and devices and the Grlib calls from TI.

 

As an example, I downloaded the Element14 Safe & Sound log, and using MS Paint, I made some minor changes and then created a .bmp. file to be used with Image Reformer.

 

First, open the file in Paint (Or an equivalent tool to create bitmaps with).

 

image

 

Resize the image to fit n the Sharp LCD 96x96 pixel screen:

 

image

 

If needed, you can zoom in or out to work on the image or add Gridlines to edit each pixel. I changed the '&' symbol color to black so it would stand out in the black and white image from Image Reformer.

image

 

Then, save the image as a 24-bit bitmap with a ".bmp" extension for use with the Image Reformer Tool.

 

image

 

Then launch the MSP430 Graphics Library Image Reformer tool.

On my system, after it was installed, the tool executable was found at:

     C:\ti\msp430\imagereformer_1_00_00_00\imagereformer.exe

 

Once the Image Reformer Tool is launched, you will get a blank page.

image

 

 

From the 'File-Open Image' menu option, find your bitmap file and open it.

The image should be shown on both the left and the right screens.

image

 

From here,you can set the Width, Height, Number of colors to use and whether Compression is on or off.

For the Sharp 96x96 LCD, I found  the following settings to work best:

 

  • Number of colors - 2 Color
  • Width                   - 96 Max
  • Height                  - 96 Max (76 in this case)
  • Compression       - Off

 

This will change the image on the right to a Black and White Image.

image

 

 

 

Once the settings are in place, just click on the Gear icon next to the folder icon in the menu bar to Generate the image 'C' code.

 

image

 

This will generate the '.c' file that will be used in the Code Composer Code to display the image on the LCD screen.

 

image

 

Data in the '.c' file

/* Copyright (c) 2012, Texas Instruments Incorporated
All rights reserved.


Redistribution and use in source and binary forms, with or without
modification, are permitted provided that the following conditions
are met:


*  Redistributions of source code must retain the above copyright
   notice, this list of conditions and the following disclaimer.


*  Redistributions in binary form must reproduce the above copyright
   notice, this list of conditions and the following disclaimer in the
   documentation and/or other materials provided with the distribution.


*  Neither the name of Texas Instruments Incorporated nor the names of
   its contributors may be used to endorse or promote products derived
   from this software without specific prior written permission.


THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.*/




#include "grlib.h"


static const unsigned char pixel_SafeAndSound1BPP_UNCOMP[] =
{
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0x81, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xf8, 0x18, 0x1f, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xf8, 0x38, 0x1e, 0x0f, 0xfc, 0x7f, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xf8, 0x3c, 0x1e, 0xe7, 0xfd, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xf8, 0x24, 0x1c, 0xf6, 0x10, 0xc3, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xf8, 0x66, 0x1e, 0x1d, 0xc9, 0x99, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xf8, 0x6e, 0x1f, 0x87, 0x0d, 0x81, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xfc, 0x66, 0x1d, 0xf4, 0xcd, 0xbf, 0xff, 0x07, 0xff, 0xff, 0xff, 0xdf, 
0xfc, 0xfe, 0x3c, 0xf5, 0xcd, 0x9d, 0xfe, 0x73, 0xff, 0xff, 0xff, 0xdf, 
0xfc, 0x7e, 0x3e, 0x0c, 0x05, 0xc3, 0xfe, 0x7f, 0x0c, 0xe8, 0x18, 0x1f, 
0xfe, 0x3c, 0x7f, 0xff, 0xff, 0xff, 0xff, 0x0e, 0xe4, 0xe9, 0xdb, 0x9f, 
0xfe, 0x3c, 0x7f, 0xff, 0xff, 0xff, 0xff, 0xc2, 0xf4, 0xe9, 0xd3, 0xdf, 
0xff, 0x3c, 0xff, 0xff, 0xff, 0xff, 0xfe, 0xf8, 0xf4, 0xe9, 0xd3, 0xdf, 
0xff, 0xbd, 0xff, 0xff, 0xff, 0xff, 0xfe, 0x72, 0xe4, 0xc9, 0xdb, 0x9f, 
0xff, 0xc3, 0xff, 0xff, 0xff, 0xff, 0xff, 0x07, 0x0e, 0x09, 0xdc, 0x1f, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 
0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff
};


static const unsigned long palette_SafeAndSound1BPP_UNCOMP[]=
{
  0x000000, 0xffffff
};


const tImage  SafeAndSound1BPP_UNCOMP=
{
  IMAGE_FMT_1BPP_UNCOMP,
  96,
  76,
  2,
  palette_SafeAndSound1BPP_UNCOMP,
  pixel_SafeAndSound1BPP_UNCOMP,
};

 

This file can be added to a CCS project such as the MSP432 Sharp LCD example that Jan Cumps outlines:

 

image

 

I added a 'images.h' file to add an interface to the image so I can just include this where I wish to use the image code.

For the Safe & Sound image, the '.h' file looks like this.

/*
 * images.h
 *
 *  Created on: Apr 20, 2017
 *      Author: Jon Morss
 */


#ifndef HGSIMAGES_IMAGES_H_
#define HGSIMAGES_IMAGES_H_




extern const Graphics_Image  SafeAndSound1BPP_UNCOMP;
//extern const Graphics_Image  TI_Logo_69x64_1BPP_UNCOMP;




#endif /* HGSIMAGES_IMAGES_H_ */

 

 

To use the image, just include the header file for the image where the image will be displayed.

Example:

 

#include <lcddriver/sharp96x96.h>


#include "SASImages/images.h"


Graphics_Context g_sContext;

 

To display the image, just replace the "Hello World" string output, or as in my case, just added a function to display the image before the Task runs in the main.

    System_flush();


    drawLogo();
    Delay(10);

 

Function drawLogo:

void drawLogo(void)
{
    Graphics_clearDisplay(&g_sContext);
    Graphics_drawImage(&g_sContext, &SafeAndSound1BPP_UNCOMP, 5, 48);
    Graphics_flushBuffer(&g_sContext);
}

 

I created a simple Delay call that I use to control the how long the image will be on screen.

void Delay(volatile int d_Time)
{
    volatile int i;
    volatile int j;
    for (i=0;i < d_Time; i ++) {
        for (j=0;j < 1700000 ; j ++);
    }
}

 

As a result, the image should look like what is seen in the following vid.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • jomoenginer
    jomoenginer over 9 years ago in reply to Jan Cumps +4
    Jan, Here is a Compressed RLE4 image that was Generated by Image Reformer and displayed on the Sharp96 LCD with a MSP432.
  • jomoenginer
    jomoenginer over 9 years ago in reply to Jan Cumps +3
    Jan, I wonder if the issue is that the CC1310 has a Cortex-M3 vs a Cortex-M4-F as does the MSP432. However, here is the same image running on the CC1310 using the 'display' example from the SimpleLink…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jomoenginer +2
    I haven't tried uncompressed yet. I'm on a business trip (Barcelona, yay) and will try when home. The line is really a stray artifact, nothing in the original image (or in the right pane of the TI tool…
Parents
  • Jan Cumps
    Jan Cumps over 9 years ago

    When using the compress options of the tool, and setting the same compress setting in the tImage struct (happens automatic during code generation), I have a slightly skewed image on the display and a stray line in the left lower corner (at least with the CC1310 Launchpad image , haven't tried with the MSP432 yet)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 9 years ago in reply to Jan Cumps

    I haven't tried the compression option with the Sharp LCD.  The compression option might be best suited for something like the BOOSTXL-K350QVG-S1 LCD.  Have you tried it uncompressed?  

     

    if you are getting a stray line in the display, check the image to ensure there is nothing in that location that might be getting translated as a line or that you are not displaying a larger area than the image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jomoenginer

    I haven't tried uncompressed yet. I'm on a business trip (Barcelona, yay) and will try when home.

     

    The line is really a stray artifact, nothing in the original image (or in the right pane of the TI tool) indicates that something is off.

    ... and I have a line in each image I render, but it's not the same length each time.

     

    (I typically don't use the TI tool + API to convert and render photos. So I know it's a software thing, not something with the display).

     

    My todo-s are:

    - test unciompressed on CC1310

    - test compressed on an MSP432

     

    I'll report back, with photos.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jomoenginer

    I haven't tried uncompressed yet. I'm on a business trip (Barcelona, yay) and will try when home.

     

    The line is really a stray artifact, nothing in the original image (or in the right pane of the TI tool) indicates that something is off.

    ... and I have a line in each image I render, but it's not the same length each time.

     

    (I typically don't use the TI tool + API to convert and render photos. So I know it's a software thing, not something with the display).

     

    My todo-s are:

    - test unciompressed on CC1310

    - test compressed on an MSP432

     

    I'll report back, with photos.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jomoenginer
    jomoenginer over 9 years ago in reply to Jan Cumps

    I wonder if it has something to do with the Run Length Encoding (RLE) or the Bits Per Pixel (BPP) setting.  In the uncompressed version I show in the post, a 1BPP was used since the image was fairly simple.  I've used the same setting for another image and it seems to work as well.  I would have try it with a more complex image and test the compression option to see if I see the same results.

    You might want to reference section 4.4.5 Compression Types in the " Design Considerations When Using MSP430 Graphics Library" doc for some options to try:

    http://www.ti.com.cn/cn/lit/an/slaa548/slaa548.pdf

     

    However, since the tools seems to be a MSP430 (432) tool, I am not sure what support there is with a CC1310.  I'll see if I can give it a go with a CC1310 when I get a chance.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 9 years ago in reply to Jan Cumps

    Jan,

     

    Here is a Compressed RLE4 image that was Generated by Image Reformer and displayed on the Sharp96 LCD with a MSP432.

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jomoenginer

    Thanks Jon. I can see that you don't have the artifact on your display.

    The tool is MSP430 branded but the outputs are RTOS grlib compatible.  TI-RTOS grlib library supports the same drawing and compression algorithms across the product line.

    I'm using the same API calls as you.

     

    I'll give it a go this Friday.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 9 years ago in reply to Jan Cumps

    Jan,

     

    I wonder if the issue is that the CC1310 has a Cortex-M3 vs a Cortex-M4-F as does the MSP432. 

     

    However, here is the same image running on the CC1310 using the 'display' example from the SimpleLink CC13x0 SDK examples version 1.30.00.06.  In this particular instance with the CC1310 I do see some distortion midway in the word 'STAR' as well at the bottom right corner. 

    I'm not sure what to say outside of it might be something to bring up to TI and see if it is a known issue.

     

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to jomoenginer

    It's a TI-RTOS version issue.

    Works good in the last proper TI-RTOS for CC13XX and 26XX version 2.16.0.06

    In the current SimpleLink for CC1310 SDK 1.30.0.06 (everyone knows that I'm not a fan of this particular path TI has gone with RTOS) the odd artifacts and skewed images appear.