Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe&Sound:Wearable Tracking Device for Miners - 04: KIT review [430BOOST-SHARP96]
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
  • Author Author: sunnyiut
  • Date Created: 29 Mar 2017 7:58 PM Date Created
  • Views 1140 views
  • Likes 2 likes
  • Comments 2 comments
  • msp432_launchpad
  • safe and sound design challenge
  • msp432p401r
  • sharp96
  • sharp_lcd_booster_pack
Related
Recommended

Safe&Sound:Wearable Tracking Device for Miners - 04: KIT review [430BOOST-SHARP96]

sunnyiut
sunnyiut
29 Mar 2017

Title: Wearable Tracking Device for Miners                    

By: sunnyiut                                                                      

Previous Blogs
01: Introduction02: The Kit03: Review_MSP432P401R

 

Design Challenge: Safe and Sound Wearables

Blog number: 04

 

 

Intro:

imageimage

 

The KIT contains an LCD display booster pack. This blog post will present a review on this booster pack: 430BOOST-SHARP96.

LS013B4DN04 display from Sharp Electronics with capacitive touch sliders makes this Booster Pack an ultra low power display solution for small menu, sensor readings, time and for providing touch inputs to navigate.

 

 

 

Features:

 

  • Ultra low power LS013B4DN04 LCD consumes 10uW
  • 9216 pixels in 1.3 inch screen with 96x96 resolution
  • 50% reflectance for moving graphics
  • visibility at >0.5 LUX without light source
  • two capacitive touch sliders, each consists of three elements
  • on-board additional 5v DCDC converter for customized power
  • additional through hole terminals for Booster Pack headers provide customizable wiring

 

image

image taken from TI 430BOOST-SHARP96 User's Guide

 

 

Review Description:

 

This review contains two parts with example codes to demonstrate the functionalities of this plug in display module. The example codes are from TI support for this Booster Pack.

 

  • PART 01 - demonstrates the static graphic display capability for 'text', 'image', 'rectangle', 'round' etc
  • PART 02 - demonstrates the moving graphics display capability with capacitive touch inputs from sliders

 

     example codes:          1. 430boost_sharp96_grlibExample

                                     2. 430boost_sharp96_Cap Touch

 

     IDE:                          Code Composer Studio v7.1.0

     Resource:                  Resource Explorer [dev.ti.com/tirex]

     Launchpad:                MSP-EXP432P401R

 

 

PART 01:image

 

Example code - 01: 430boost_sharp96_grlibExample_msp432p401r

 

Description -

 

It demonstrates the use of Graphics Library with the Sharp display to show simple graphics primitives.

like -  Pixels, Lines, Circles, Rectangles, Text, Image etc.

It also utilizes functions for Initialization, for switching foreground and background color scheme, for inverting pixels / text / graphics color etc.

 

Includes - grlib.h and LcdDriver/Shar96x96.h

 

Display -

 

Intro Screen:

image

 

        Graphics_drawStringCentered(&g_sContext, (int8_t *)"MSP-EXP432P401R", GRAPHICS_AUTO_STRING_LENGTH, 48, 15, GRAPHICS_TRANSPARENT_TEXT);
        Graphics_drawStringCentered(&g_sContext, (int8_t *)"CCS v7.1.0", GRAPHICS_AUTO_STRING_LENGTH, 48, 35, GRAPHICS_TRANSPARENT_TEXT);
        Graphics_drawString(&g_sContext, (int8_t *)"SAFE & SOUND", GRAPHICS_AUTO_STRING_LENGTH, 10, 51, GRAPHICS_OPAQUE_TEXT);
        Graphics_drawStringCentered(&g_sContext, (int8_t *)"ELEMENT14", GRAPHICS_AUTO_STRING_LENGTH, 48, 75, GRAPHICS_TRANSPARENT_TEXT);
        Graphics_flushBuffer(&g_sContext);

 

 

 

Image of Rocket and TI logo:

image

image

 

        Graphics_drawImage(&g_sContext, &LPRocket_96x37_1BPP_UNCOMP, 3, 28);
        Graphics_flushBuffer(&g_sContext);
        Delay();
        Graphics_clearDisplay(&g_sContext);
        Graphics_drawImage(&g_sContext, &TI_Logo_69x64_1BPP_UNCOMP, 15, 15);

 

 

 

Pixels and Lines:

 

image

        Graphics_drawStringCentered(&g_sContext, (int8_t *)"Draw Pixels", GRAPHICS_AUTO_STRING_LENGTH, 48, 5, GRAPHICS_TRANSPARENT_TEXT);
        Graphics_drawStringCentered(&g_sContext, (int8_t *)"& Lines", GRAPHICS_AUTO_STRING_LENGTH, 48, 15, GRAPHICS_TRANSPARENT_TEXT);
        Graphics_drawPixel(&g_sContext, 30, 30);
        Graphics_drawPixel(&g_sContext, 30, 32);
        Graphics_drawPixel(&g_sContext, 32, 32);
        Graphics_drawPixel(&g_sContext, 32, 30);
        Graphics_drawLine(&g_sContext, 35, 35, 90, 90);
        Graphics_drawLine(&g_sContext, 5, 80, 80, 20);
        Graphics_drawLine(&g_sContext, 0, Graphics_getDisplayHeight(&g_sContext) - 1, Graphics_getDisplayWidth(&g_sContext) - 1, Graphics_getDisplayHeight(&g_sContext) - 1);

 

 

Circles:

image

 

        Graphics_drawString(&g_sContext, (int8_t *)"Draw Circles", GRAPHICS_AUTO_STRING_LENGTH, 10, 5, GRAPHICS_TRANSPARENT_TEXT);
        Graphics_drawCircle(&g_sContext, 30, 70, 20);
        Graphics_fillCircle(&g_sContext, 60, 50, 30);

 

 

Rectangles:

 

image

        Graphics_drawStringCentered(&g_sContext, (int8_t *)"Draw Rectangles", GRAPHICS_AUTO_STRING_LENGTH, 48, 5, GRAPHICS_TRANSPARENT_TEXT);
        Graphics_drawRectangle(&g_sContext, &myRectangle1);
        Graphics_fillRectangle(&g_sContext, &myRectangle2);
        // Text below won't be visible on screen due to transparency (foreground colors match)
        Graphics_drawStringCentered(&g_sContext, (int8_t *)"Normal Text", GRAPHICS_AUTO_STRING_LENGTH, 50, 50, GRAPHICS_TRANSPARENT_TEXT);
        // Text below draws foreground and background for opacity
        Graphics_drawStringCentered(&g_sContext, (int8_t *)"Opaque Text", GRAPHICS_AUTO_STRING_LENGTH, 50, 65, GRAPHICS_OPAQUE_TEXT);
        Graphics_setForegroundColor(&g_sContext, ClrWhite);
        Graphics_setBackgroundColor(&g_sContext, ClrBlack);
        Graphics_drawStringCentered(&g_sContext, (int8_t *)"Invert Text", GRAPHICS_AUTO_STRING_LENGTH, 50, 80, GRAPHICS_TRANSPARENT_TEXT);

 

 

Inverting Foreground and Background colors:

 

image

        Graphics_setForegroundColor(&g_sContext, ClrBlack);
        Graphics_setBackgroundColor(&g_sContext, ClrWhite);
        Graphics_fillRectangle(&g_sContext, &myRectangle3);
        Graphics_setForegroundColor(&g_sContext, ClrWhite);
        Graphics_setBackgroundColor(&g_sContext, ClrBlack);
        Graphics_drawStringCentered(&g_sContext, (int8_t *)"Invert Colors", GRAPHICS_AUTO_STRING_LENGTH, 48, 5, GRAPHICS_TRANSPARENT_TEXT);
        Graphics_drawRectangle(&g_sContext, &myRectangle1);
        Graphics_fillRectangle(&g_sContext, &myRectangle2);
        // Text below won't be visible on screen due to transparency (foreground colors match)
        Graphics_drawStringCentered(&g_sContext, (int8_t *)"Normal Text", GRAPHICS_AUTO_STRING_LENGTH, 50, 50, GRAPHICS_TRANSPARENT_TEXT);
        // Text below draws foreground and background for opacity
        Graphics_drawStringCentered(&g_sContext, (int8_t *)"Opaque Text", GRAPHICS_AUTO_STRING_LENGTH, 50, 65, GRAPHICS_OPAQUE_TEXT);
        // Text below draws with inverted foreground color to become visible
        Graphics_setForegroundColor(&g_sContext, ClrBlack);
        Graphics_setBackgroundColor(&g_sContext, ClrWhite);
        Graphics_drawStringCentered(&g_sContext, (int8_t *)"Invert Text", GRAPHICS_AUTO_STRING_LENGTH, 50, 80, GRAPHICS_TRANSPARENT_TEXT);

 

 

 

PART 02:image

 

Example code - 02: 430BOOST_SHARP96_CapTouch_MSP432P401R

 

Description -

 

This demonstration has three elements -

  • implementation of a simple menu with two objects and navigate using touch sliders
  • a digital timer clock, where the time, date and day can be set using Launchpad buttons and touch sliders
  • a slider ball game, which demonstrates moving graphics and multi touch control using touch sliders

 

Display -

 

Menu:

 

A simple menu which displays two objects to select -

  • Clock
  • Slider Ball Game

The left touch slider can be used to navigate and select any of the objects.

There is an 'enter' button at the bottom right corner, which reacts with the S2 button on the launchpad. So, the left touch slider will select whether the MCU will display a digital clock or run a Slider Ball game and the S2 button will execute the selected program.

 

imageimageimage

Display main menu                                             left touch slider downward: Slider Ball Game                           left touch slider upward: Clock

 

 

Digital Clock:

 

A digital clock starts with 12:00 am, 01/01/2015, monday.

There are two options at the bottom side of the screen - Exit and Set

By pressing S1 button on the launchpad, program exits the clock and goes back to main menu.

By pressing S2 button on the launchpad, program selects the time, date and day segments of the clock and the right touch slider can be used to increase or decrease the value.

 

imageimage

clock starts with 12:00 MONDAY 01/01/2015          S2 -> selects segments, right touch slider -> set different values

 

However, I set the time -> 07:13, day-> SUNDAY, date -> 03/26/2017

Time and day segments were updated and the clock started ticking. But the date became-> 03/26/2015. image

 

 

Slider Ball Game:

 

It demonstrates a nice, slim 'slider ball' game providing a good example of moving display. The ball starts moving from left to right and there are two bars at the left and right edges of the display. If the ball hits the bar it reflects back to the opposite direction. But if the ball misses the bar then it hits the wall and 'game over'.

These two bars can be moved up and down using the left and right touch sliders.

It's a nice example of multi touch sense and a moving graphics display.

 

imageimageimage

 

However,

In my opinion, the touch sliders are not so sensitive to be effectively used in this case. May be that's because it does not have any material overlay. As, the user's guide suggests that a material overlay will improve the performance, but in that case a re-calibration is required.

This LCD display has good visibility in room environment. But it does not have any backlight. In my project proposal, I may need to use an LCD which is bright enough to be viewed in low light or even dark. So, I may need to think about it ......

 

That's the end of my review on this 430BOOST_SHARP96 memory LCD booster pack. In my next blog, I'll post a review on the sensor booster pack.

  • Sign in to reply
  • sunnyiut
    sunnyiut over 9 years ago in reply to pl98

    hi,

    I have used example codes from the device web page of  TI for MSP4432P401R

    Example code : 430BOOST_SHARP96_CapTouch_MSP432P401R

     

    You can use this demo code to figure out the use of the capacitive touch of this Booster pack.

    here is the link of the example codes for MSP432P401R -

    MSP-EXP432P401R 3_00_00_03 - TI.com

     

    sorry for the late reply image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • pl98
    pl98 over 9 years ago

    Hello, I can't seem to get any display from the Capacitive Touch Library. Can you assist me?

    Thank You in Advance!:)