Twist, Turn and Move Design Challenge with TE Robotics
  • Challenges & Projects
  • Design Challenges
  • Twist, Turn and Move Design Challenge with TE Robotics
  • More
  • Cancel
Twist, Turn and Move Design Challenge with TE Robotics
Blog NEO Pixel Font Demo - (Blog 3)
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 17 Aug 2022 5:26 AM Date Created
  • Views 2461 views
  • Likes 12 likes
  • Comments 9 comments
  • doug wong
  • Sammy Semaphore
  • Twist Turn and Move Robotics Design Challenge
  • Neo pixels
Related
Recommended

NEO Pixel Font Demo - (Blog 3)

dougw
dougw
17 Aug 2022

The Twist, Turn, and Move Robotics Design Challenge with TE Connectivity

Intro
This project has a lot of moving parts (literally) and not all parts are here to be worked on so I will have to work on bits that I can while waiting for deliveries. This blog will cover the character display electronics and font that will be used on Sammy Semaphore's chest to display the character he is signaling with his flags. The LED display is an 8 x 8 matrix of addressable NEO pixels which is capable of all kinds of fancy visual effects. However for this project I will only be implementing a simple green character font. The blog will also cover assembly of a very cool TE Connectivity signal connector.

image

Display Description

The display is driven by one pin of an Arduino UNO that was included in the challenge kit. This demo simply cycles through the alphabet to have a look at the font and the colour. The display has a white diffuser inside an antistatic envelope to provide nice contrast. I hope to expand this program to allow remote entry of characters via a Bluetooth module.

Here is a quick video of the display showcasing its font:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I like the green colour - it is easy  on the eyes.

image

TE Connectivity M8 Signal Connector

This TE Connectivity M8 signal connector is really cool. Whoever designed this connector had his or her thinking cap on - it has an impressive list of features. This model has 4 pins capable of carrying 4 Amps each. The metal shell is waterproof, dustproof (IP67) and fully shielded. Both connectors can be field installed without soldering or crimping. The only tool needed is a small Allen key that comes with the connector. Here is a video showing how I assembled one of them - it also includes a demo of assembling another TE Connectivity connector from their MTA line. That assembly features my favorite AMP (another TE Connectivity brand) tool that is about the fastest way to make a connection:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I am very impressed with the high quality field installable signal connector.

Here is the demo firmware for the display above:

//Arduino UNO 8x8 NEO pixel display font demo
//by Doug Wong 2022

#include <FastLED.h>
#define NLEDS 64
#define LEDpin 2

CRGB leds[NLEDS];

byte AL[26][8] = {
{129, 129, 129, 255, 129, 129, 66, 60},     //A0
{127, 129, 129, 129, 127, 129, 129, 127},   //B1
{124,  130, 1, 1, 1, 1, 130, 124},          //C2
{63, 65, 129, 129, 129, 129, 65, 63},       //D3
{255, 1, 1, 1, 63, 1, 1, 255},              //E4
{1, 1, 1, 1, 63, 1, 1, 255},                //F5
{124, 130, 129, 225, 1, 1, 130, 124},       //G6
{129, 129, 129, 129, 255, 129, 129, 129},   //H7
{28, 8, 8, 8, 8, 8, 8, 28},                 //I8
{30, 33, 33, 32, 32, 32, 32, 248},          //J9
{129, 65, 33, 17, 31, 33, 65, 129},         //K10
{255, 129, 1, 1, 1, 1, 1, 1},               //L11
{129, 129, 129, 129, 153, 165, 195, 129},   //M12
{129, 193, 161, 145, 145, 137, 133, 131},   //N13
{126, 129, 129, 129, 129, 129, 129, 126},   //O14
{1, 1, 1, 1, 127, 129, 129, 127},           //P15
{190, 65, 161, 129, 129, 129, 129, 126},    //Q16
{129, 65, 33, 127, 129, 129, 129, 127},     //R17
{126, 129, 128, 64, 62, 1, 129, 126},       //S18
{8, 8, 8, 8, 8, 8, 8, 127},                 //T19
{126, 129, 129, 129, 129, 129, 129, 129},   //U20
{24, 36, 36, 66, 66, 129, 129, 129},        //V21
{129, 195, 165, 153, 129, 129, 129, 129},   //W22
{129, 66, 36, 24, 24, 36, 66, 129},         //X23
{16, 16, 16, 16, 24, 36, 66, 129},          //Y24
{255, 2, 4, 8, 16, 32, 64, 255}             //Z25
};

int abc, rc, cc;

void setup() {
  FastLED.addLeds<WS2812B, LEDpin, GRB>(leds, NLEDS);
  FastLED.setBrightness(50);
}

void loop()
{
  for (abc = 0; abc < 26; abc++)
  {
  for (rc = 0; rc < 8; rc++)
  {
    for (cc = 0; cc < 8; cc++)
    {
       if (bitRead(AL[abc][rc], cc) == 1)
       {
        leds[rc + cc * 8] = CRGB::Green;
       }
       else
       {
        leds[rc + cc * 8] = CRGB::Black;
       }
    }
  }
    FastLED.show();
    delay(600);
    for (int ac = 0; ac < 64; ac++)
    {
      leds[ac] = CRGB::Black;
    }
    FastLED.show();
  }
}

Discussion for Blog 3

I am very impressed with the high quality field installable signal connector from TE Connectivity, it has all the features I like to see in a high end connector. I can't think of a connector that has a better feature set.

The NEO pixel display font took quite a bit of fiddling around to use the 8x8 pixel format, but I like how it turned out. It should be readable from many meters away.

The fourth blog will likely cover design of Sammy Semaphore, and possibly the build.
The fifth blog will likely cover firmware for Sammy Semaphore.
The sixth blog will cover the Connector Tester build and operation.
A seventh blog may be needed to wrap up the project.

Relevant Links:

Twist, Turn and Move Design Challenge with TE Robotics
Sammy Semaphore - blog 1
Connector Tester - blog 2
NEO Pixel Display - blog 3
Sammy Semaphore Torso Demo - Blog 4
I Am Sam I Am - Blog 5
TE Connectivity Connector Tester Blog 6
Sammy Semaphore Fully Functional Blog 7

  • Sign in to reply
Parents
  • DAB
    DAB over 4 years ago

    Nice blog Douglas.

    One of my first jobs involved building cables for a power distribution system. Luckily, none are as small as these. My hands are just too big for such little components.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 4 years ago

    Nice blog Douglas.

    One of my first jobs involved building cables for a power distribution system. Luckily, none are as small as these. My hands are just too big for such little components.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 4 years ago in reply to DAB

    I think most of us have had to build cables at one time or another. It is nice when the manufacturer has made it easy.