Upcycle IoT Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Upcycle IoT Design Challenge
  • More
  • Cancel
Upcycle IoT Design Challenge
Blog Using (obsolete) home appliances to optimize energy consumption - blog 2, nature of the fridge
  • Blog
  • Forum
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Upcycle IoT Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: JWx
  • Date Created: 30 Jan 2024 4:49 PM Date Created
  • Views 2234 views
  • Likes 10 likes
  • Comments 9 comments
  • Upcycle IoT Design Challenge
Related
Recommended

Using (obsolete) home appliances to optimize energy consumption - blog 2, nature of the fridge

JWx
JWx
30 Jan 2024

Intro

As proposed in the previous blog post, I will investigate the possibility of turning home refrigerator into energy storage device, storing excess energy as cold, which hopefully will limit it's energy consumption during other parts of the day. To make things easier (and stick to this design challenge's theme) I will investigate using old (which usually means - simple)  construction, probably scheduled for replacement in many households. This way, if everything goes as planned, not only some energy consumption optimization will be obtained, but old appliance saved from recycling.

Let's start with refrigerator's construction analysis that will tell us how difficult will be implementation of external control mechanism.

Home refrigerator construction

Most common home refrigerator type is a compressor based one. It's working principle describes the following diagram and description (obtained from https://phys.libretexts.org with accordance to the CC BY 4.0 license)

image

A schematic diagram of a household refrigerator. A coolant with a boiling temperature below the freezing point of water is sent through the cycle (clockwise in this diagram). The coolant extracts heat from the refrigerator at the evaporator, causing coolant to vaporize. It is then compressed and sent through the condenser, where it exhausts heat to the outside.

One element omitted in this description is a thermostat that is controlling compressor operation - switching it on when temperature inside is too high and switching off when temperature lowers sufficiently.

Electrical connections

Ok - you can tell - it is not a HVAC forum, show us some electrical schematics! This part is easier to say than to do, mainly because electrical schematics seems very simple. For example, one random sticker from Sharp refrigerator (obtained from stackexchange and licensed with CC BY-SA) looks like this:

image

Omitting non-critical/not always present components, it looks like compressor is connected in series with thermostat, starter, overload protection device - and that's all...

Thermostat construction

Typical thermostat is purely mechanical one, with regulation based on mechanical means.

{gallery}Thermostat external view

image

image

The one analyzed in this paragraph was bought as (a cheap) universal replacement part. We can see that it is normally closed at the room temperature:

image

What is interesting that it stays closed in all the regulation range (that is inconsistent with observed behavior of most of the fridges, when appliance can be powered off simply by turning thermostat to the end of the regulation range) - maybe it is damaged or designed to be installed with appliances equipped with separate power switch.

Now it's time for checking what is inside our thermostat:

image

the main part of the thermostat it a pipe and a cylinder filled with gas that expands and contracts when temperature changes. Expanding cylinder keeps relay's contact closed, but is countered by the force regulated by the cam installed on the regulator's shaft, allowing for switching temperature regulation. Factory calibration is obtained by using regulation screw (both cam and screw pointed on the following picture using red lines)

image

As we can see, it seems that traditional refrigerator can be easily controlled by use of additional relay connected in parallel to the thermostat's contacts. When this relay stays open, fridge operates as normal, but can be forced ON simply by closing it. Now - some means of measuring the temperature inside in the independent and non-invasive way would be needed.

  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 2 years ago in reply to JWx +2
    PVT - photovoltaic thermal panels https://en.wikipedia.org/wiki/Photovoltaic_thermal_hybrid_solar_collector
Parents
  • kmikemoo
    kmikemoo over 2 years ago

    Very cool. Joy  It's the cold version of a masonry heater - which experiencing a re-birth of sorts these days.  If you need cool more than warm... this is a great plan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to kmikemoo

    I guess the overproduction event could be also be used to heat an existing hot water cylinder. You are probably likely to need and use hot water more than space heating in the summer months. However you may require anti-scold valves or a separate cylinder to avoid over temperature.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • JWx
    JWx over 2 years ago in reply to beacon_dave

    yes - this is AFAIK default reaction, people even configure their controllers to automatically start water heaters when energy production exceeds certain threshold... I personally don't like it very much - I think that heating water directly using heat pipes is far more effective, but preventing generation shutdown is a plus 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to JWx

    Using direct solar water heating would likely be more efficient but then you would likely lose prime roof space for PV panels.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 2 years ago in reply to JWx

    Using direct solar water heating would likely be more efficient but then you would likely lose prime roof space for PV panels.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • JWx
    JWx over 2 years ago in reply to beacon_dave

    I wonder if someone ever creates PV panel integrated with water heater - given that PV efficiency drops with temperature, integrated water cooler/heater would be of double use... 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to JWx

    PVT - photovoltaic thermal panels

    https://en.wikipedia.org/wiki/Photovoltaic_thermal_hybrid_solar_collector

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 2 years ago in reply to beacon_dave

    Did cursory check.  Those panels are crazy expensive.  No wonder the tech didn't take off.  That and if you can't extract the heat, it becomes it's own worst enemy for panel PV efficiency.  I agree that direct solar water heating is a better plan.

    In talking to a solar installer, he would prefer NOT to install on the roof.  Evidently, the retained heat of the roof can lower panel efficiency by up to 30% - from what he said.  Makes me wonder how high off the roof you need to go to mitigate that heating effect - which increases the installation price...  The installer really promoted ground installation - if you have the real estate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to kmikemoo

    You are paying for the cost of two panels basically.

    You perhaps have to cost in the increased lifespan of the PV component through reduced temperature of the panel, the increased power output, and also the savings you get from the solar water heating.

    But you have to then cost in the electricity to run the pump unless you have have a micro-hydro system to hand. 

    The Tech Ingredients channel managed to have some success with fan cooling a PV panel: 

    https://www.youtube.com/watch?v=Mt9qLRN7JvA 

    but then you have the expense of adding and maintaining fans in an outdoor environment. The gains always appear to turn out quite small, so it's perhaps dependent on scale.

    Ground level also helps with maintenance - regular cleaning which improves output. However in most cases it also increases shadow from trees/buildings which reduces output.