Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog Upcycle It - Funeka - The Skull #2 : Surprise!!!
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
  • Author Author: sakthi.1260
  • Date Created: 4 Apr 2017 8:22 AM Date Created
  • Views 823 views
  • Likes 5 likes
  • Comments 5 comments
  • upcycled_funeka
  • unboxing
  • intel edison
Related
Recommended

Upcycle It - Funeka - The Skull #2 : Surprise!!!

sakthi.1260
sakthi.1260
4 Apr 2017

Hi Guys,

 

Just came from home from Holiday. and someone was at the door already..... Yea the kits have arrived image

 

image

 

image

The gaiety of seeing new hardware  image

 

image

Couldn't Resist myself so started to work on it

 

image

 

You can find the drivers and Yocto images over Intel webpage https://software.intel.com/en-us/iot/hardware/edison/downloads

and Grove Library from seeedstudio GitHub depository https://github.com/Seeed-Studio/Sketchbook_Starter_Kit_V2.0

 

image Make sure the Slider is on the micro USB side image

image

 

I used the Arduino IDE to run a small program that shows temperature on the 16x2 and changes back-light when temperature exceeds a threshold.

 

const int pinTemp = A0;
const int B = 3975;
#include <Wire.h>
#include "rgb_lcd.h"

byte cel[8] = {
    0b11100,
    0b10100,
    0b11100,
    0b00000,
    0b00000,
    0b00000,
    0b00000,
    0b00000};
rgb_lcd lcd;

void setup()
{
    Serial.begin(115200);
lcd.begin(16,2);
lcd.createChar(0,cel);
}

void loop()
{
    int val = analogRead(pinTemp);

    // Determine the current resistance of the thermistor based on the sensor value.
    float resistance = (float)(1023-val)*10000/val;

    // Calculate the temperature based on the resistance value.
    float temperature = 1/(log(resistance/10000)/B+1/298.15)-273.15;

    // Print the temperature to the serial console.
    if(temperature>36)
    {lcd.setRGB(255, 20, 20);
      lcd.setCursor(4,0);
      lcd.print(temperature); lcd.write((unsigned char)0);lcd.print("C");
      }
else  {
   lcd.setRGB(20, 20, 255);
      lcd.setCursor(4,0);
      lcd.print(temperature); lcd.write((unsigned char)0);lcd.print("C");}    
    // Wait one second between measurements.
    delay(1000);

}

 

 

image

 

Heated the thermistor using Hair dryer. Yep it works

 

image

 

Cheers image

  • Sign in to reply

Top Comments

  • fvan
    fvan over 9 years ago in reply to mcb1 +4
    You'll finally be able to blame someone else for your purchases
  • mcb1
    mcb1 over 9 years ago +3
    I intially thought the RGB backlight was 'useful', but seeing the change when it exceeds a threshold is great. I might need to order some of these ... Mark
  • Workshopshed
    Workshopshed over 9 years ago +2
    I do like a board with nicely designed mounting holes. There's nothing worse than a screw hole but no room for the standoff or screws.
Parents
  • mcb1
    mcb1 over 9 years ago

    I intially thought the RGB backlight was 'useful', but seeing the change when it exceeds a threshold is great.

     

    I might need to order some of these ...

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 9 years ago in reply to mcb1

    You'll finally be able to blame someone else for your purchases image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to fvan

    I was going to mention you ...seems I didn't need to image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 9 years ago in reply to fvan

    I was going to mention you ...seems I didn't need to image