Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog Upcycle It - Funeka - The Skull #6 : Resplendent
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
  • Author Author: sakthi.1260
  • Date Created: 30 Apr 2017 5:57 PM Date Created
  • Views 688 views
  • Likes 3 likes
  • Comments 4 comments
  • lcd
  • upcycled_funeka
  • upcycle
  • intel edison
Related
Recommended

Upcycle It - Funeka - The Skull #6 : Resplendent

sakthi.1260
sakthi.1260
30 Apr 2017

Hey Guys,

 

Thought I would make the eye ball part for this week, but found out the Thermal sensor to be broken, have ordered a new one wondering how long its gonna take for delivery.

While walking around I found this monitor over the trash, I took it home.

image

 

After reading about it, I had a second thought of using this fellow. Its back light is CCFL which is supposed to have some mercury and the panel was broken, while the one salvaged from the Dell  was LED and also intact (probably I'd turn it into a Smart TV).

So just thought it would be better to re-purpose this than leaving it in the trash. Its from ViewSonic not sure for the model. Started to dismantle it image.

 

image

 

The power board was dead, and the control board was rusted....

 

image

But a lot of components could be salvaged and used again.

 

 

I found this Inverter capable of powering 4 CCFL's (fulfills our need), it costed around 500INR approx 8$

image

It has the(from left to Right) Vin,Vin, Enable, Brightness,Ground and Ground. Unfortunately the Brightness Pin was dummy.

 

image

All we need is the White Screen so removed the Panel.

 

Some connections.... Some soldering....

image

image

 

I removed the speaker connections which I did in the previous blog and turned them into wire to board connectors for convenience.

 

The code, well its actually simple..

void setup() {
  pinMode(2, OUTPUT);
  pinMode(4, INPUT);
}

void loop() {

  if (digitalRead(4) == HIGH)
  {
    digitalWrite(2, HIGH);
  } else  {
    digitalWrite(2, LOW);
  }
}

 

 

Lights ON... I placed to photo to see how it looks as a light panel. Well its WOW.

image

 

Well our actual purpose it to use it a under glow lamp, so I just flipped it...It's too bright so I've done some fancy work, which I'm gonna show only in the final post image.

image

 

Cheers image

  • Sign in to reply
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    Nice find, great upcycling

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 9 years ago

    Nice find, great upcycling