Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog Upcycle It - Washing Machine Hydroponic Grower - #3 Preparation II
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
  • Author Author: nandohila
  • Date Created: 10 Apr 2017 3:44 AM Date Created
  • Views 1548 views
  • Likes 5 likes
  • Comments 5 comments
  • upcycle_it
  • hydronics
  • upcycled_hydroponics
  • washing_machine
  • intel edison
Related
Recommended

Upcycle It - Washing Machine Hydroponic Grower - #3 Preparation II

nandohila
nandohila
10 Apr 2017

As I am still waiting for the kit, I will share some more updates about the washing machine preparation.

 

As we suspected, the original machine motor is too much for turning the drum at such low RPM (1-3 RPM). Maybe the new washing machine models will have those multiphase motors that could be hacked to operate as a step motor but this is not the case of the 1996 washing machine we have.

 

The solution will be using a stepper motor (also upcycled from an old printer). Using a stepper motor will be easy to integrate it with the Edison kit and we will be able to adjust precise rotation and also stop the drum at set positions, handy for loading the plant baskets and harvesting. But the big advantage will be the power savings, the small stepper is more than enough to turn the drum at low RPM, not requiring gear boxes or complex pulleys arrangements.

image

 

We also decided to remove most of the front panel exposing the whole drum. This will give an industrial apparency for our rotary grower and will help with the ventilation avoiding condensation.

 

  imageimage

 

In order to still resembling a washing machine, we will re-install the original control panel lower down so we can use some push buttons to actuate some of the new functions.

 

  imageimage

 

Next steps will be mounting the stepper, make a bracket for the light and install a water tank with a water pump.

  • Sign in to reply

Top Comments

  • COMPACT
    COMPACT over 9 years ago in reply to COMPACT +4
    Once it starts spinning you'll be the torque of the town.
  • DAB
    DAB over 9 years ago +3
    Things always get exciting when the hacksaw comes out. Make sure that the drum rollers are clean and move freely. You will also need to keep an eye on the current draw of the motor, so you might want to…
  • COMPACT
    COMPACT over 9 years ago +1
    The machine looks Australian.
Parents
  • COMPACT
    COMPACT over 9 years ago

    The machine looks Australian.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • nandohila
    nandohila over 9 years ago in reply to COMPACT

    Yeap, and it was a freebie from gumtree..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • nandohila
    nandohila over 9 years ago in reply to COMPACT

    Yeap, and it was a freebie from gumtree..