Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog Upcycle It - Washing Machine Hydroponic Grower - #8 Nutrient Solution System
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
  • Author Author: nandohila
  • Date Created: 29 May 2017 7:02 AM Date Created
  • Views 2285 views
  • Likes 5 likes
  • Comments 5 comments
  • hydroponics
  • upcycle_it
  • washing_machine
  • intel edison
Related
Recommended

Upcycle It - Washing Machine Hydroponic Grower - #8 Nutrient Solution System

nandohila
nandohila
29 May 2017

On hydroponic systems, the growing medium has the only function to secure the plant roots in place so it doesn't have any means to nourish the plants as the soil does. Therefore, the water caring a nutrient solution is the sole source of nutrients to the plant.

 

Conventional hydroponic systems consist in a reservoir for the nutrient solution and a pump that delivers this solution to the growing trays as required. For rotary systems, the solution normally doesn't need to be pumped as the growing bed will be partly submerged into the reservoir so every complete turn will deliver nutrient to all plants inside the drum.

 

In our case, we have a limited volume of water we can store on the bottom of the washing machine drum so we have to combine the 2 methods. We will have the drum partially submerged so the growing medium can absorb the nutrient when dipping into it but due to its low volume it wouldn't last long without refilling it.  So we need an auxiliary reservoir to store the nutrient and pump it into the drum when the drum level is low. The drum and the auxiliary tank will have a level switch. The one on the drum will trigger the pump to refill it and the one on the auxiliary reservoir will set an alarm to be manually filled.

 

Below is the nutrient solution system schematic.

 

image

 

Details of the items

 

Reservoir - Made using a plastic container. I drilled a hole and installed a threaded fitting with 2 "O" rings to seal the water. I also made a frame on the bottom of the washing machine using 20x20 mm aluminium equal angle so the plastic container is secured in place. 

 

imageimageimageimage

 

 

Water Pump - Original water pump connected to the reservoir

image

Water Level Adjustment - Made of 25 mm PVC Pipe, 2 x 90º Elbows and 1 x "T". Connected to the original flex joint that originally was connected to the water pump. I secured the pipe using a wingnut so we can change the water level adjusting the pipe height. Note that the top part of the pipe assembly is open; otherwise, it would become a siphon draining all drum water.

imageimage

Water Level Sensor - The original drum water level switch is an interesting piece of equipment, it is a mechanical device that uses air pressure, created by the water weight on the bottom of the drum, to actuate a contact switch. I couldn't imagine but this mechanical sensor can be adjusted to the level we want turning the plastic screws on the back. It took a while to adjust it but I managed to have it switching off when the water inside the drum lowers below the accepted level. This sensor will be used to give a signal to turn the water pump on.

 

imageimageimage

 

Besides the pump being started once the level inside the tumbler is low. it will also turn on in cycles for 10 seconds every hour to ensure the nutrient solution is refreshed.

 

Below is a short video of the water pump cycle testing.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 9 years ago +2
    As much as you progress in this project as much I see it a concrete reality. This is a very good "translation" of an idea to practical application. I have a curiosity as I am almost 100% ignorant on hydroponic…
  • DAB
    DAB over 9 years ago +1
    Nice update. After reading the post, I realized that you could also use a small spray system to mist the plants at the top. This last idea could be useful as some plants better absorb nutrients through…
  • nandohila
    nandohila over 9 years ago in reply to balearicdynamics +1
    Hi Enrico, I am not an expert in hydroponics but I've been reading a lot about this subject lately. So yes, plants will be upside down at one stage. The concept of having the plants turning in a drum is…
Parents
  • balearicdynamics
    balearicdynamics over 9 years ago

    As much as you progress in this project as much I see it a concrete reality. This is a very good "translation" of an idea to practical application. I have a curiosity as I am almost 100% ignorant on hydroponic plant growing; when the drum rotates the top plants are top down?

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 9 years ago

    As much as you progress in this project as much I see it a concrete reality. This is a very good "translation" of an idea to practical application. I have a curiosity as I am almost 100% ignorant on hydroponic plant growing; when the drum rotates the top plants are top down?

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • nandohila
    nandohila over 9 years ago in reply to balearicdynamics

    Hi Enrico,

     

    I am not an expert in hydroponics but I've been reading a lot about this subject lately. So yes, plants will be upside down at one stage. The concept of having the plants turning in a drum is to have a more efficient use of the artificial light and to apply gravity in different positions of the plant. The light being in the centre there is no need of reflectors as it will be plants all around it.  People who have being using such rotary growing systems claim that plants grows faster and stronger due this change of gravity effect. While my project is not up and running you can watch a time lapse video of a commercial unit on this link below.

     

    https://www.youtube.com/watch?v=84zh7XL15n8&t=140s

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to nandohila

    Thank you Fernando, very helpful answer. I was very curious and my level of ignorance in this field (ha) is a sort of abyss. I am following with great attention your posts are are very clear as the project if growing (ha).

     

    Enrico