Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Interactive Race Car Driver - Indicators - Offline testing with node and mraaStub
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
  • Author Author: Workshopshed
  • Date Created: 16 May 2017 5:22 PM Date Created
  • Views 682 views
  • Likes 6 likes
  • Comments 2 comments
  • upcycled_interactiveracecardriver
Related
Recommended

[Upcycle It] Interactive Race Car Driver - Indicators - Offline testing with node and mraaStub

Workshopshed
Workshopshed
16 May 2017

For my indicators, I wanted a simple function that would blink them 5 times then stop. I found a suitable piece of code on Stack Overflow which did the same thing for some flashing text and ported it across to node. However, I did not have the Edison to hand so pondered how I would test it. A quick google found mraaStub  a mock version of mraa that you can use on platforms that don't have mraa hardware. I installed this and discovered that it needs a logging package called "winston" which I also installed. I also had to tweak the mraaStub library so that it would log by default. My version can be found at https://github.com/Workshopshed/UpcyclingDesignChallenge/tree/master/mraaStub

 

//Simple function to test the indicator

var platform = require('os').platform();
var m;

if (platform === 'win32') {
    m = require('mraaStub'); //also needs winston
} else {
    m = require('mraa');
}

var myLed = new m.Gpio(13); //LED hooked up to digital pin 13 (or built in pin on Galileo Gen1 & Gen2)
myLed.dir(m.DIR_OUT); //set the gpio direction to output

function indicate() {
    var count = 1;
    var ledState = true;
    var intervalId = setInterval(function() {
        myLed.write(ledState?1:0);
        ledState = !ledState;
                if (count++ >= 10) {
                clearInterval(intervalId);
            }
    }, 500);
};

indicate();

 

Here's how it looks in Visual Studio Code when it is running.

image

 

Reference

javascript - Making text blink a certain number of times? - Stack Overflow

https://www.npmjs.com/package/winston

https://www.npmjs.com/package/mraaStub

https://github.com/Workshopshed/UpcyclingDesignChallenge/blob/master/Tests/test6.js

https://github.com/Workshopshed/UpcyclingDesignChallenge/tree/master/mraaStub

 

Previous Posts

Upcycle It Blogs tagged with upcycled_interactiveracecardriver

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 9 years ago +1
    One simplification of this approach is to rename the "node_modules\mraaStub" folder on the Windows development machine to be "node_modules\mraa" then code can be simplified to be: var m; m = require(…
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    One simplification of this approach is to rename the "node_modules\mraaStub" folder on the Windows development machine to be "node_modules\mraa" then code can be simplified to be:

     

    var m;  
    m = require('mraa');

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 9 years ago

    One simplification of this approach is to rename the "node_modules\mraaStub" folder on the Windows development machine to be "node_modules\mraa" then code can be simplified to be:

     

    var m;  
    m = require('mraa');