Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] Nixie Display #2 - Investigations
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
  • Author Author: gpolder
  • Date Created: 3 Apr 2017 8:17 PM Date Created
  • Views 2256 views
  • Likes 5 likes
  • Comments 6 comments
  • upcycle_it
  • voltage_measurement
  • pcb layout
  • nixie
  • counter
  • power_measurement
  • nixie_tube
  • upcycled_nixie
Related
Recommended

[Upcycle It] Nixie Display #2 - Investigations

gpolder
gpolder
3 Apr 2017
<< PreviousBlog IndexNext >>

 

In my first blog post I  described the idea and plan of converting my old nixie pulse counter to a versatile number display.

My plan was based only on visual investigation of the hardware. In this post I will describe some test and measurements in order to get a solid plan for the conversion.

 

Nixie power

Member mads391i asked for the power rating of the nixie tubes. Although not completely necessary to know for the purpose of the project, it is always good to have a good feeling of how the circuit works. Here is a picture of the bottom side of the PCB. As you can see a very clean and comprehensible design from which the circuit easily can be derived.

image

image

Here is the circuit I deduced from the PCB:

image

Then I measured the Vcc voltage, which drives the TTL logic:

image

The Vdd voltage, which drives the nixie tubes:

image

And the voltage across the 39k resistor, which appeared to be 85V. 85V over the 39k resistor is 2.2 mA current trough the resistor and nixie tubes. Total power consumed by the nixie tube, resistor and 74141 per digit is 225 x 2.2 = 495 mW, so almost half a Watt. And for all six digits 3 Watt in total excluding the rest of the logic.

image

 

 

BCD Decoder

Now some words about the coding of the numbers. The 7490 counters outputs BCD code to the 74141 BCD-DECIMAL decoder/driver IC. BCD takes advantage of the fact that any one decimal numeral can be represented by a four bit pattern, where each decimal digit is represented by its corresponding four-bit binary value, as shown in the following table, copied from the 74141 datasheet.

imageimage

As can be seen from the picture of the backside of the PCB the BCD outputs of the 7490 counters are connected to separate connections on the PCB where eventually pin headers or wires can be soldered.

In order to test the BCD inputs on the 74141 drivers I removed one of the 7490 counters. Since an open input in TTL logic counts as a logical H, according to the table we expect to have no output.

Unfortunately due to parasitic effects all the digits light up a bit.

This means that with the current circuit I'm not able to turn a digit completely off.

imageimage

Then I connected the GND (7490 pin 10) to output D (7490 pin 11). And bingo, a nice 7 appears on the display, as expected from the above  function table.

imageimage

So by providing proper BCD codes to the 7490 sockets I can easily select the different numbers.

Member jasonwier92 suggested to let the SN 7490 in place and control the digits with pulses. I like the idea, but drawback is that each time you change a digit you will have some counting effect on it. Furthermore I expect by replacing the 7490's with a small circuit board with an I/O extender will give a more clean and solid solution.

 

  • Sign in to reply

Top Comments

  • gpolder
    gpolder over 9 years ago in reply to mcb1 +1
    I do like the GerritCAD drawing. A vintage device needs vintage tools
  • COMPACT
    COMPACT over 9 years ago +1
    If you're stripping out the 7490's why not replace it with a PSoC4 or 5LP to drive the 74141 BCD inputs. The PSoCs make a really easy way to create a parallel, serial, USB, SPI, or I2C device to display…
  • gpolder
    gpolder over 9 years ago in reply to COMPACT +1
    Hi COMPACT I appreciate your suggestion for using a PSoC. I did a nice project already on a 5LP ( The specified item was not found. ) Although I think PSoC is a good candidate, I decided to solve it the…
Parents
  • COMPACT
    COMPACT over 9 years ago

    If you're stripping out the 7490's why not replace it with a PSoC4 or 5LP to drive the 74141 BCD inputs.

     

    The PSoCs make a really easy way to create a parallel, serial, USB, SPI, or I2C device to display a few nixie numeric digits with minimal fuss and effort.

     

    Just a thought (as DAB would say).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gpolder
    gpolder over 9 years ago in reply to COMPACT

    Hi COMPACT I appreciate your suggestion for using a PSoC. I did a nice project already on a 5LP (The specified item was not found.)

    Although I think PSoC is a good candidate, I decided to solve it the easy way, with an I2C I/O extender. I will blog about this soon.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • gpolder
    gpolder over 9 years ago in reply to COMPACT

    Hi COMPACT I appreciate your suggestion for using a PSoC. I did a nice project already on a 5LP (The specified item was not found.)

    Although I think PSoC is a good candidate, I decided to solve it the easy way, with an I2C I/O extender. I will blog about this soon.