Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Blog [Upcycle It] WiFi Connected Smoke Detector #9: WannaCry and IoT security
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
  • Author Author: vlasov01
  • Date Created: 22 May 2017 3:05 AM Date Created
  • Views 2862 views
  • Likes 2 likes
  • Comments 12 comments
  • wannacry
  • ransomware
  • cyber security
  • network isolation
Related
Recommended

[Upcycle It] WiFi Connected Smoke Detector #9: WannaCry and IoT security

vlasov01
vlasov01
22 May 2017
<< Previous

Project Index

Next>>

Sonoff POW order arrived

 

This week started pretty good as I received my order of Sonoff POW WiFi Switch with Power Consumption Measurement. It was the last piece I wanted to use in my system to demonstrate that I can improve home safety by acting on an alert from a smoke detector by shutting down connected appliances.

The out of box firmware doesn't provide MQTT connection and creates a lot of Internet network connections as discovered in the following blog post "How to hack free your Sonoff RF without soldering". I've turned down this option.

I've start reading about Sonoff ESP8266 programming options. TASMOTA project seems the most straightforward one for Sonoff devices. This Arduino sketch is an Open Source project. It has a lot of recent activity, documentation, videos and it comes with MQTT support,

I've installed required software and packages. I've updated user_config.h with mt WiFi parameters and other settings. Arduino IDE verify and build failed initially, but after some debugging and files movement the compilation was successful. Unfortunately my USB-to-TTL sopped functioning without any warning signs.I'll try to use my Arduino UNO as USB-to-TTL adapter as described in this 1 minute video.

 

Thoughts after WannaCry

 

WannaCry impacted significant number unpatched Windows PC worldwide.

The number of IoT internet connected devices will be significantly higher then the number of PCs.

 

There is a lot of questions in relation to IoT security. The negative impact of breaches in IoT may be comparable or even bigger then from WannaCry. Recently these IoT devices have been exploited for DDoS attacks.Once these devices become more widespread with a common core they may be exploited much more frequently.

  1. Who is managing patches for IoT devices? Based on my previous blog even Intel is not necessary keeps supplied Intel Edison packages up-to-date.
  2. How long they will be supported? Windows XP been released 16 years ago, but still requires patches.Do you think TASMOTA project will be supported in 5 years? It has only one contributor at this point.
  3. How can I validate chain of trust of libraries, firmware and toolchain used to build it? What kind of secure software development practices were followed in the process of building them? TASMOTA relies on ESP SDK which is partially closed.
  4. What I can do to minimize risks of increasing secure attack vector on my IoT infrastructure in my home, which I'd like to make safer by introducing WiFi Connected Smoke Detector? Does it still make sense?

 

Many questions but one answer

 

I have very little power to control the top three points. But I may be able to control the last one. And the answer came from CBC Radio program Spark. One of the guests recommended to connect to the Internet only what needs to be connected. it can be achieved by applying network isolation, where the network gets split in several zones as described in the following paper.

I start looking if I can introduce this notion of network zones on my Intel Edison IoT gateway. I was thinking about using it as an edge gateway, where on one side it plays a role of Access Point (AP mode) for IoT devices like Sonoff and WiFi smoke detector, And on other side it is a WiFi client (STAtion mode) so it can communicate with Slack and Cronitor. But it is not possible now as Edison radio "Broadcom  module does not support STA/AP concurrently" as described in Intel Edison WiFi Guide.

At this point I can use a separate router (or create a separate net on my router) for IoT devices and Intel Edison gateway, where only the gateway has access my home network and internet. Another option is to add WiFi USB module to Intel Edison, so it will get two network interfaces one for each network.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +3
    Nice update. Security has been my main objection to this rush to IOT. Unless control is in place from the start then there is a huge systemic risk. I currently do not own any IOT enabled devices and I…
  • Workshopshed
    Workshopshed over 9 years ago in reply to mcb1 +2
    It is possible to put an opensource firmware onto a selection of routers. I have thought about that to turn an old one into a bridge
  • vlasov01
    vlasov01 over 9 years ago in reply to mcb1 +1
    My WiFi router allows creation of an isolated guest network. Not sure if I can set rules and ports for this network. If it is possible, then I'll set it for my IoT devices, where only the gateway will…
Parents
  • mcb1
    mcb1 over 9 years ago

    Peter Oakes has put together a lengthy video on reprograming ESP 8266 devices (which are the heart of the Sonoff)

    Peter Scargill is the mastermind behind it but they collaborated to bring it all together.

    http://tech.scargill.net/itead-slampher-and-sonoff/

     

     

    I always like to create a seperate network and then link that to the internet via the normal router.

    It allows you to set rules, ports and such like to hopefully prevent unwanted access.

     

    It is good that you're looking at security, far too many manufacturers aren't IMO.

    Mark.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vlasov01
    vlasov01 over 9 years ago in reply to mcb1

    My WiFi router allows creation of an isolated guest network. Not sure if I can set rules and ports for this network. If it is possible, then I'll set it for my IoT devices, where only the gateway will be able access internet..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vlasov01
    vlasov01 over 9 years ago in reply to mcb1

    My WiFi router allows creation of an isolated guest network. Not sure if I can set rules and ports for this network. If it is possible, then I'll set it for my IoT devices, where only the gateway will be able access internet..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 9 years ago in reply to vlasov01

    Not sure if I can set rules and ports for this network

    It might depend on your particular router.

     

    I have used a couple of different ones in the past, and the standard wireless one delivered by my broadband supplier is next to useless.

    I use this simply as a modem and let my own router do all the access, rules, etc.

     

    For these projects I usually connect a second wireless router into the main router, with it's own network address system and rules.

    Here is where you would limit things and try to lock down as much as you can.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to mcb1

    It is possible to put an opensource firmware onto a selection of routers. I have thought about that to turn an old one into a bridge

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to Workshopshed

    It is possible to put an opensource firmware onto a selection of routers. I have thought about that to turn an old one into a bridge

    I've started using the TPLINK Portable routers.

     

    http://www.pcadvisor.co.uk/review/wifi-routers/tp-link-tl-mr3020-review-3343107/

     

    If you are shopping at the right time, one of our large stores carries them for NZ$20-$40.

     

     

    Surprisingly these have a lot of features and allow a very high degree of locking, without resorting to opensource.

    I understand that there is OS for them.

     

    Mark