Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Forum Node and global vs local?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 2 subscribers
  • Views 1103 views
  • Users 0 members are here
  • node.js
Related

Node and global vs local?

Workshopshed
Workshopshed over 9 years ago

Something I spotted today on booting a node script on the Edison (if not using XDK)

 

Run a Script on Edison Boot | Shawn Hymel

 

The point of interest for me is the line:

 

Environment="NODE_PATH=/usr/lib/node_modules/"

 

I'm guessing that this stores the node modules in the lib folders as previously when I've used NPM to install node packages I've spotted it has been putting them under /home.

 

It looks like we can set this using:

 

 

export NODE_PATH=/usr/lib/node_modules:$NODE_PATH

 

 

There also seems to be an "npm -g" option but others seem to recommend against this.

 

No Need for npm -g | Peter Lyons

 

Any thoughts or recommendations on best practice for the Edison?

  • Sign in to reply
  • Cancel
  • jasonwier92
    0 jasonwier92 over 9 years ago

    I do not install global unless it is required or if it is something that I would use globally.

     

    Items to install globally (some exclusions for a small single board computer like the Edison).

    • Express if this is on a server doing several web projects
      • Yes for the Express CLI
      • Assuming they are all using the same version of Express
      • Not for the Edison or Raspberry Pi
      • Not for development, unless you are forcing express in each project to be the same
    • Node-red-admin - has to be install globally, or so it says
    • pm2 - This would be needed globally

     

    Otherwise I am a big fan of installing local to a project.  Global installs are bad when I am running moduleA-1.2.3 globally and need to use moduleA-2.1.0 for a feature, so I update globally and it breaks three other projects.  Isolation is good for dependent modules.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer