Upcycle It
  • Challenges & Projects
  • Design Challenges
  • Upcycle It
  • More
  • Cancel
Upcycle It
Forum Accessing hardware on the Edison?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 5 subscribers
  • Views 3117 views
  • Users 0 members are here
Related

Accessing hardware on the Edison?

Workshopshed
Workshopshed over 9 years ago

I'm wondering about accessing the GPIO of the Edison in high-level languages such as Python or Node.

 

So far I've found MRAA but wondered if there are other options?

 

https://github.com/intel-iot-devkit/mraa

  • Sign in to reply
  • Cancel

Top Replies

  • jasonwier92
    jasonwier92 over 9 years ago +3
    MRAA should be the way to go. Looks like they have Python interface. Check out this link: Getting Started With Intel Edison - Python Programming - All I cannot wait to play with Python and Node on the…
  • e14 Contributor
    e14 Contributor over 9 years ago +2
    If you can access the gpio through the standard linux filesystem method it should be possible to write out the bash commands in Python using os.popen e.g. import os p = os.popen("echo 1 > /sys/class/gpio…
  • mcb1
    mcb1 over 9 years ago in reply to konstantinoskonstas +2
    I'm learning as I go. I've always said I'm more a hardware guy that pokes and prods at software. I was hoping to get a head start on you guys/gals ...
  • e14 Contributor
    e14 Contributor over 9 years ago

    If you can access the gpio through the standard linux filesystem method it should be possible to write out the bash commands in Python using os.popen

     

    e.g.

     

    import os
    p = os.popen("echo 1 > /sys/class/gpio/export")
    p.close()

     

    would export pin 1 of the gpio for use in the file system.

     

    so once the pin is exported to the filesystem you would do

     

    p = os.popen("echo out > /sys/class/gpio/gpio1/direction")

     

    to set gpio pin 1 to be an output pin and then

     

    p = os.popen("echo 1 > /sys/class/gpio/gpio1/value")

     

    to set gpio pin 1 high

     

    and

     

    p = os.popen("echo 0 > /sys/class/gpio/gpio1/value")

     

    to set that pin low.

     

    This method should work for all devices that can access the gpio through the linux filesystem.

     

    --------------------------

     

    I should mention that you probably need to run the Python script with sudo or as root  for this to work. If this is a problem for your project you can get around it by adding the user account to the gpio group

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • jasonwier92
    jasonwier92 over 9 years ago

    MRAA should be the way to go.  Looks like they have Python interface.

     

    Check out this link:

    Getting Started With Intel Edison - Python Programming - All

     

    I cannot wait to play with Python and Node on the Edison. Plans are to make that an early write up.

     

    I was wondering if Firmata would work or how does the Arduino and Atom systems communicate?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to e14 Contributor

    Cheers Lucie, yes using the filesystem is always my fallback approach when I can't get something working.

    According to the hardware guide you can even control PWM that way.

    http://www.intel.com/content/dam/support/us/en/documents/edison/sb/edison-arduino-hardware-guide.pdf

     

    I really hate the whole needing to run as root thing for GPIO access. It seems a common problem across different platforms, would be nice to see if it's solved on the Edison.

     

    For my BeagleBone project I've resolved the problem with a C Daemon that listens on NamedPipes. That can run as root but the client apps can run as the user.

    https://github.com/Workshopshed/musicController/blob/master/servoDaemon/servoDaemon.c

     

    MRAA does seem like the natural choice given that it was provided by one of the competition sponsors. Libsoc could also be a possibility https://github.com/jackmitch/libsoc

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to jasonwier92

    Firmata does seem to be a possibilityhttps://github.com/rwaldron/galileo-io

     

    I believe that in the Edison the Atom communicates to the hardware at the chip level so there's NO serial communication like in the Yún.

    Arduinobreakout.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to Workshopshed

    try using

     

    useradd -G {group-name} username

     

    in a terminal to add the user account to the gpio group, doing this will allow the user account to work with gpio without needing sudo etc.. it took me a while to work it out but its obvious when the group is there ready and waiting to add users to it. There's usually groups for i2c spi etc..

     

    just type "groups" into a terminal to see which groups are available

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to e14 Contributor

    mcb1 can you test this on your Edison?

     

    You'd need to be root for the following:

     

    echo 1 > /sys/class/gpio/export

    echo out > /sys/class/gpio/gpio1/direction

     

    But can you run the following as a regular user?

     

    echo 1 > /sys/class/gpio/gpio1/value

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to jasonwier92

    This article suggests you'd need to be root to run things that access MRAA

     

    https://communities.intel.com/thread/60492

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to Workshopshed

    if you add the user account to the gpio group you can do export, direction, value and anything else available as a regular user. I add the www-data user to the group to allow webserver software to interact with gpio for control over network.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to Workshopshed

    Andy

    Your request worked right up until doing it as a normal user ...I'm going to need to do soem searching for that.

     

    So I picked GPIO 48, as it wasn't PWM and already set by the Arduino sketch that was trying to run.

    root@MyEdison:/sys/class/gpio# echo 48 > export
    root@MyEdison:/sys/class/gpio# cd gpio48
    root@MyEdison:/sys/class/gpio/gpio48# ls
    active_low  device  direction  edge  power  subsystem  uevent  value
    root@MyEdison:/sys/class/gpio/gpio48# echo out > direction
    root@MyEdison:/sys/class/gpio/gpio48# cat direction
    out
    root@MyEdison:/sys/class/gpio/gpio48# echo 1 > value
    root@MyEdison:/sys/class/gpio/gpio48# echo 0 > value
    root@MyEdison:/sys/class/gpio/gpio48#

     

    I followed the Sparkfun guide (to try to understand what your were trying to achieve image )

    https://learn.sparkfun.com/tutorials/sparkfun-blocks-for-intel-edison---gpio-block

     

    I found a few other references.

    https://communities.intel.com/thread/57506

    they are linking to this document

    https://emutex.com/emutexlabs/76-intel-edison-gpio-pin-multiplexing-guide

     

     

    https://communities.intel.com/thread/81616

    https://communities.intel.com/thread/53340

     

    Sounds like you should be our technical assistant image

    Perhaps jwatson can send you one so you can help with the difficult queries.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to Workshopshed

    There's an article here that is worth reading (the second part) if you want to detect pin changes.

    https://www.linux.com/learn/intro-to-Linux/2017/3/intel-edison-linux-maker-machine-matchbox

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>