Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green House Blog:10.1 - Update Code For Three Dollar EC PPM Meter for MCU
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
  • Author Author: m.ratcliffe
  • Date Created: 19 Sep 2015 7:14 PM Date Created
  • Views 11743 views
  • Likes 6 likes
  • Comments 71 comments
  • hydroponics
  • adapted_greenhouse
  • ppm
  • ec
  • arduino
Related
Recommended

Automated Green House Blog:10.1 - Update Code For Three Dollar EC PPM Meter for MCU

m.ratcliffe
m.ratcliffe
19 Sep 2015

This code is a slight update of the last one, updated:

>Better Uptime Counter

>LCD Shield

>New Pin out Diagram

>Restart Protected Calibration Details

>EU and US Plug Calibrated Probe

 

Also a quick update to the code so the calibration value will survive a power cut, we are storing the cell constant K [a float] in EEPROM as a scaled int, so there may be a slight change in the value following a reboot [but that small it wont make much difference].

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Cell Constants

I Recommend Calibrating your probe but if that is not an option at this time the following cell constants [K] will give a good estimated readout:

EU plug: K= 1.76

US Plug K= 2.88

 

Calibration

If it needs instructions to be operated someone engineered it wrong, the lcd should explain itself to you at start up. If you are still stuck watch the youtube video to see how I calibrate it.

Calibrate with an EC of about 50% your maximum expected reading for best results.

 

 

 

The NEW Pinout:

 

 

image

Save some wire and solder the divider onto a pin header

 

image

 

 

 

 

 

 

 

 

The new Code:

 

Header 1

 

 

/*

   ElCheapo Arduino EC-PPM measurments

 

   This scrip uses a common USA two prong plug and a 47Kohm Resistor to measure the EC/PPM of a Aquaponics/Hydroponics Sytem.

   You could modift this code to Measure other liquids if you change the resitor and values at the top of the code.

 

   This Program will give you a temperature based feed controller. See Read me in download file for more info.

 

   28/8/2015  Michael Ratcliffe  Mike@MichaelRatcliffe.com

   

   

          This program is free software: you can redistribute it and/or modify

    it under the terms of the GNU General Public License as published by

    the Free Software Foundation, either version 3 of the License, or

    (at your option) any later version.

 

 

    This program is distributed in the hope that it will be useful,

    but WITHOUT ANY WARRANTY; without even the implied warranty of

    MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the

    GNU General Public License for more details.

 

 

    You should have received a copy of the GNU General Public License

    along with this program.  If not, see <http://www.gnu.org/licenses/>.

  

    Parts:

    -Arduino - Uno/Mega

    -Standard American two prong plug

    -1 kohm resistor

    -DS18B20 Waterproof Temperature Sensor

  

    Limitations:

    -Cell Constant [K]  must be less than 5.0 or it will Mess with the way we save values in EEPROM

    -A reset will change your kell constant slightly, but not to a great extent

    -EEPROM seems to survive a reflash, so changing values in the code will not change them in the flashed software. you will need to do it via the LCD

  

    See www.MichaelRatcliffe.com/Projects for a Pinout and user guide or consult the Zip you got this code from

 

*/

 

 

//************************** Libraries Needed To Compile The Script [See Read me In Download] ***************//

// Both below Library are custom ones [ SEE READ ME In Downloaded Zip If You Dont Know how To install] Use them or add a pull up resistor to the temp probe

 

 

#include <OneWire.h>

#include <DallasTemperature.h>

#include <LiquidCrystal.h> //Standard LCD Lbrary

#include <EEPROM.h> //Standard EEPROM Library

 

 

 

 

//************************* User Defined Variables ********************************************************//

 

 

//##################################################################################

//-----------  Do not Replace R1 with a resistor lower than 300 ohms    ------------

//##################################################################################

 

 

int R1= 1000;

int Ra=25; //Resitance of Digital Pin, 25 ohms for mega/uno

int ECPin= A8;

int ECGround=A9;

int ECPower =A12;

 

 

//************************* User Defined Variables ********************************************************//

 

 

float CalibrationEC=1.38; //EC value of Calibration solution is s/cm

 

 

//*********** Converting to ppm [Learn to use EC it is much better**************//

// Hana      [USA]         PPMconverion:   0.5

// Eutech    [EU]          PPMconversion:  0.64

//Tranchen   [Australia]   PPMconversion:  0.7

// Why didnt anyone standardise this?

 

 

float PPMconversion=0.5;

 

 

//*************Compensating for temperature ************************************//

//The value below will change depending on what chemical solution we are measuring

//0.019 is generaly considered the standard for plant nutrients [google "Temperature compensation EC" for more info

float TemperatureCoef = 0.019; //this changes depending on what chemical we are measuring

 

 

 

 

//********************** Cell Constant For Ec Measurements *********************//

//Mine was around 2.9 with plugs being a standard size they should all be around the same

//But If you get bad readings you can use the calibration script and fluid to get a better estimate for K

//I Recommend Calibrating your probe but if that is not an option at this time the following cell constants [K] will give a good estimated readout:

//EU plug: K= 1.76

//US Plug K= 2.88

 

 

float K=2.88;

 

 

 

 

//************ Temp Probe Related *********************************************//

#define ONE_WIRE_BUS 26           // Data wire For Temp Probe is plugged into pin 10 on the Arduino

const int TempProbePossitive =22;  //Temp Probe power connected to pin 9

const int TempProbeNegative=24;    //Temp Probe Negative connected to pin 8

 

 

 

 

//***************************** END Of Recomended User Inputs *****************************************************************//

 

 

 

 

//********************************************************//

 

 

// select the pins used on the LCD panel

LiquidCrystal lcd(8, 9, 4, 5, 6, 7);

 

 

// define some values used by the panel and buttons

int lcd_key     = 0;

int adc_key_in  = 0;

int button =0;

#define btnRIGHT  1

#define btnUP     2

#define btnDOWN   3

#define btnLEFT   4

#define btnSELECT 5

#define btnNONE   6

 

 

int Screen =1;

 

 

OneWire oneWire(ONE_WIRE_BUS);// Setup a oneWire instance to communicate with any OneWire devices

DallasTemperature sensors(&oneWire);// Pass our oneWire reference to Dallas Temperature.

 

 

 

 

float Temperature=10;

float EC=0;

float EC25 =0;

int ppm =0;

 

 

float raw= 0;

float Vin= 5;

float Vdrop= 0;

float Rc= 0;

int Readings=0;

 

 

//********************** Some Variables For Loging Min/Max Values ********************************//

float MinEC=100;

float MaxEC=0;

float MinT=100;

float MaxT=0;

 

 

//************************** Just Some basic Definitions used for the Up Time LOgger ************//

long Day=0;

int Hour =0;

int Minute=0;

int Second=0;

int SecondStamp=0;

int Once=0;

 

//**************************Some Stuff For Calibration ******************************************//

float TemperatureFinish=0;

float TemperatureStart=0;

int i=0;

float buffer=0;

float Kt=0;

 

 

//*********************** EPROM Stuff [So SetPoint and Cal Survive a reboot] ******************//

int value;

int addresCalibration=0;

 

 

 

 

//**********************Some Stuff For Uptime **************************************************//

long Rollover=0;

int HighMillis=0;

 

 

//*********************************Setup - runs Once and sets pins etc ******************************************************//

void setup()

{

  Serial.begin(9600);

  pinMode(TempProbeNegative , OUTPUT ); //seting ground pin as output for tmp probe

  digitalWrite(TempProbeNegative , LOW );//Seting it to ground so it can sink current

  pinMode(TempProbePossitive , OUTPUT );//ditto but for positive

  digitalWrite(TempProbePossitive , HIGH );

  pinMode(ECPin,INPUT);

  pinMode(ECPower,OUTPUT);//Setting pin for sourcing current

  pinMode(ECGround,OUTPUT);//setting pin for sinking current

  digitalWrite(ECGround,LOW);//We can leave the ground connected permanantly

 

  delay(100);// gives sensor time to settle

  sensors.begin();  

  delay(100);

  //** Adding Digital Pin Resistance to [25 ohm] to the static Resistor *********//

  // Consult Read-Me for Why, or just accept it as true

  R1=(R1+Ra);

 

 

  //************** Restart Protection Stuff ********************//

   //Setpoint

     value = EEPROM.read(addresCalibration);

   if (value <=254) K=value*0.02;

 

 

  Serial.println("ElCheapo Arduino EC-PPM measurments");

  Serial.println("By: Michael Ratcliffe  Mike@MichaelRatcliffe.com");

  Serial.println("Free software: you can redistribute it and/or modify it under GNU ");

  Serial.println("");

  Serial.println("Make sure Probe and Temp Sensor are in Solution and solution is well mixed");

  Serial.println("");

  Serial.println("Measurments at 5's Second intervals [Dont read Ec morre than once every 5 seconds]:");

 

lcd.begin(16, 2);              // start the library

lcd.setCursor(0,0);

delay(1000);

lcd.print("Arduino EC-PPM");

lcd.setCursor(0,1);

delay(1000);

lcd.print("Mike Ratcliffe");

lcd.setCursor(0,1);

delay(1000);

lcd.setCursor(0,1);

lcd.print("Free Software   ");

delay(1000);

lcd.setCursor(0,1);

lcd.print("Mike Ratcliffe");

delay(1000);

lcd.setCursor(0,1);

lcd.print("Free Software   ");

delay(1000);

lcd.setCursor(0,0);

lcd.print("To Calibrate      ");

  lcd.setCursor(0,1);

lcd.print("Hold Select       ");

delay(3000);

  lcd.setCursor(0,0);

lcd.print("To Navigate         ");

  lcd.setCursor(0,1);

lcd.print("Use Up-Down     ");

delay(3000);

 

 

GetEC(); //gets first reading for LCD and then resets max/min

MinEC=100;

MaxEC=0;

MinT=100;

MaxT=0;

};

 

 

//******************************************* End of Setup **********************************************************************//

 

 

 

 

//************************************* Main Loop - Runs Forever ***************************************************************//

//Moved Heavy Work To subroutines so you can call them from main loop without cluttering the main loop

void loop()

{

 

if((millis()%10000)<=100){

GetEC();           //Calls Code to Go into GetEC() Loop [Below Main Loop] dont call this more that 1/5 hhz [once every five seconds] or you will polarise the water

};

LogEC();

read_LCD_buttons();

Calibration();

PrintReadings();   // Cals Print routine [below main loop]

delay(100); //Stops us entering the GETEC loop twice

 

 

}

//************************************** End Of Main Loop **********************************************************************//

 

 

 

 

//************ This Loop Is called From Main Loop************************//

void GetEC(){

Readings=1; //makes note of new readings avliable

//*********Reading Temperature Of Solution *******************//

 

 

 

 

sensors.requestTemperatures();// Send the command to get temperatures

Temperature=sensors.getTempCByIndex(0); //Stores Value in Variable

 

 

 

 

//************Estimates Resistance of Liquid ****************//

digitalWrite(ECPower,HIGH);

raw= analogRead(ECPin);

digitalWrite(ECPower,LOW);

 

 

 

 

//***************** Converts to EC **************************//

Vdrop= (Vin*raw)/1024.0;

Rc=(Vdrop*R1)/(Vin-Vdrop);

Rc=Rc-Ra;

EC = 1000/(Rc*K);

 

 

//*************Compensating For Temperaure********************//

EC25   =  EC/ (1+ TemperatureCoef*(Temperature-25.0));

ppm=(EC25)*(PPMconversion*1000);

 

 

;}

//************************** End OF EC Function ***************************//

 

 

 

 

//***This Loop Is called From Main Loop- Prints to serial usefull info ***//

void PrintReadings(){

Serial.print("Rc: ");

Serial.print(Rc);

Serial.print(" EC: "); 

Serial.print(EC25);

Serial.print(" Simens  "); 

Serial.print(ppm);

Serial.print(" ppm  "); 

Serial.print(Temperature);

Serial.println(" *C ");

 

 

 

 

if (button>=1||Readings==1) {

  Readings=0;

                    

                      if(Screen==1){

                      lcd.setCursor(0,0);

                      lcd.print("Arduino EC-PPM   ");

                      lcd.setCursor(0,1);

                      lcd.print("EC:               ");

                      lcd.setCursor(3,1);

                      lcd.print(EC25);

                      lcd.setCursor(9,1);

                      lcd.print(Temperature);

                      lcd.print("'C");

                      }

                    

                      else if(Screen==2){

                      lcd.setCursor(0,0);

                      lcd.print("Arduino EC-PPM   ");

                      lcd.setCursor(0,1);

                      lcd.print("PPM:         ");

                      lcd.setCursor(4,1);

                      lcd.print(ppm);

                      lcd.setCursor(9,1);

                      lcd.print(Temperature);

                      lcd.print("'C"); 

                        

                      }

                       else if(Screen==3){

                      lcd.setCursor(0,0);

                      lcd.print("Min:              ");

                       lcd.setCursor(4,0);

                       lcd.print(MinEC);

                       lcd.setCursor(9,0);

                      lcd.print(MinT);

                      lcd.print("'C");

                      lcd.setCursor(0,1);

                      lcd.print("Max:               ");

                      lcd.setCursor(4,1);

                      lcd.print(MaxEC);

                      lcd.setCursor(9,1);

                      lcd.print(MaxT);

                      lcd.print("'C");

                    

                       }

                        else if(Screen==4){

                   

                      lcd.setCursor(0,0);

                      lcd.print("Uptime Counter:              ");

                    

                      lcd.setCursor(0,1);

                      lcd.print("                                     ");//Clearing LCD

                      lcd.setCursor(0,1);

                      lcd.print(Day);

                      lcd.setCursor(3,1);

                      lcd.print("Day");

                      lcd.setCursor(8,1);

                      lcd.print(Hour);

                      lcd.setCursor(10,1);

                      lcd.print(":");

                      lcd.setCursor(11,1);

                      lcd.print(Minute);

                      lcd.setCursor(13,1);

                      lcd.print(":");

                      lcd.setCursor(14,1);

                      lcd.print(Second);

                    

                    

                       }

       

                    

                      else if(Screen==5){

                      

                      lcd.setCursor(0,0);

                      lcd.print("Factors          ");

                      lcd.setCursor(8,0);

                      lcd.print("PPMC:");

                      lcd.setCursor(13,0);

                      lcd.print(PPMconversion);

                    

                      lcd.setCursor(0,1);

                      lcd.print("K:               ");

                      lcd.setCursor(2,1);

                      lcd.print(K);

                      lcd.setCursor(9,1);

                      lcd.print("a:");

                      lcd.setCursor(11,1);

                      lcd.print(TemperatureCoef);

                      };

                      

                        

                  

  

  

};

 

 

/*

//********** Usued for Debugging ************

Serial.print("Vdrop: ");

Serial.println(Vdrop);

Serial.print("Rc: ");

Serial.println(Rc);

Serial.print(EC);

Serial.println("Siemens");

//********** end of Debugging Prints *********

*/

};

 

 

 

 

void read_LCD_buttons(){

  adc_key_in = analogRead(0);      // read the value from the sensor

// my buttons when read are centered at these valies: 0, 144, 329, 504, 741

// we add approx 50 to those values and check to see if we are close

if (adc_key_in > 1000)  button =0;

 

 

else if (adc_key_in < 50)   button =1;

else if (adc_key_in < 250)  button =2;

else  if (adc_key_in < 450)  button =3;

else if (adc_key_in < 650)  button =4;

else if (adc_key_in < 850)  button =5;

 

 

if(button==2){

Screen++;

 

 

}

else if (button==3){

Screen--;

};

 

 

if (Screen>=6) Screen=5;

if(Screen<=1) Screen=1;

};

 

 

//******************************* LOGS Min/MAX Values and Uptime Counter*******************************//

void LogEC(){

 

  if(EC25>=MaxEC)  MaxEC=EC25;

  if(EC25<=MinEC)  MinEC=EC25;

 

  if(Temperature>=MaxT) MaxT=Temperature;

  if(Temperature<=MinT) MinT=Temperature;

 

//** Checks For a Second Change *****//

if((millis()%1000)<=500&&Once==0){

SecondStamp=1;

Once=1;

};

//** Making Note of an expected rollover *****// 

                          if(millis()>=3000000000){

                          HighMillis=1;

                        

                          }

                          //** Making note of actual rollover **//

                          if(millis()<=100000&&HighMillis==1){

                          Rollover++;

                          HighMillis=0;

                          }

                        

                          long secsUp = millis()/1000;

                        

                          Second = secsUp%60;

                        

                          Minute = (secsUp/60)%60;

                        

                          Hour = (secsUp/(60*60))%24;

                        

                          Day = (Rollover*50)+(secsUp/(60*60*24));  //First portion takes care of a rollover [around 50 days]

                                                               

                      

                      

};

 

//******************************* Checks if Select button is held down and enters Calibration routine if it is ************************************//

void Calibration(){

 

 

 

 

 

if(button!=5) return;

else delay(1000);

read_LCD_buttons();

if(button!=5) return;

 

 

 

 

 

while(1){

read_LCD_buttons();

lcd.setCursor(0,0);

lcd.print("Set Calibration EC  ");

lcd.setCursor(0,1);

lcd.print("EC:                 ");

lcd.setCursor(3,1);

lcd.print(CalibrationEC); 

 

 

if (button==2) CalibrationEC=CalibrationEC+0.01 ;

if(button==3)  CalibrationEC=CalibrationEC-0.01;

if(button==1) break;

delay(100);

       };

 

 

lcd.setCursor(0,0);

lcd.print("Calibrating         ");

lcd.setCursor(0,1);

lcd.print("EC:                 ");

lcd.setCursor(3,1);

lcd.print(CalibrationEC); 

 

 

i=1;

buffer=0;

sensors.requestTemperatures();// Send the command to get temperatures

TemperatureStart=sensors.getTempCByIndex(0); //Stores Value in Variable

 

 

//************Estimates Resistance of Liquid ****************//

            while(i<=10){

          

              

            digitalWrite(ECPower,HIGH);

            raw= analogRead(ECPin);

          

            digitalWrite(ECPower,LOW);

            buffer=buffer+raw;

            i++;

            delay(5000);

            };

          

          

raw=(buffer/10);

sensors.requestTemperatures();// Send the command to get temperatures

TemperatureFinish=sensors.getTempCByIndex(0); //Stores Value in Variable

 

 

//*************Compensating For Temperaure********************//

EC =CalibrationEC*(1+(TemperatureCoef*(TemperatureFinish-25.0))) ;

 

//***************** Calculates R relating to Calibration fluid **************************//

Vdrop= (((Vin)*(raw))/1024.0);

Rc=(Vdrop*R1)/(Vin-Vdrop);

Rc=Rc-Ra; //Taking into account pin resistance

Kt= 1000/(Rc*EC);

 

 

 

 

 

 

 

 

                    if (TemperatureStart==TemperatureFinish){

                      Serial.println("   Results are Trustworthy");

                      Serial.print("Calibration Fluid EC: "); 

                      Serial.print(CalibrationEC);

                      Serial.print(" S  ");  //add units here

                      Serial.print("Cell Constant K");

                      Serial.print(K);

                    

                    

                      lcd.setCursor(0,0);

                      lcd.print("GoodResults         ");

                    

                    

                      lcd.setCursor(0,1);

                      lcd.print("EC:                    ");

                      lcd.setCursor(3,1);

                      lcd.print(CalibrationEC);

                      lcd.setCursor(9,1);

                      lcd.print("K:");

                      lcd.setCursor(11,1);

                      lcd.print(Kt);

                    

                              while (1) { // wee need to keep this function running until user opts out with return function

                            

                              read_LCD_buttons();

                              if(button==4) return; //exits the loop without saving becauser user asked so

                              if (button==5){

                              

                              

                              K=Kt; //saving the new cell constant

                            

                           //********Saving the new value to EEprom**********//  

                            value=K/0.02;

                            EEPROM.write(addresCalibration, value);

 

 

                            

                              lcd.setCursor(0,0);

                              lcd.print("Saved Calibration        ");

                                                          

                              lcd.setCursor(0,1);

                              lcd.print("K:                        ");

                              lcd.setCursor(3,1);

                              lcd.print(Kt);

                              delay(2000);

                              return;

                              }

                            

                              if(millis()%4000>=2000){

                              lcd.setCursor(0,0);

                              lcd.print("GoodResults         ");

                            

                            

                              lcd.setCursor(0,1);

                              lcd.print("EC:                  ");

                              lcd.setCursor(2,1);

                              lcd.print(CalibrationEC);

                              lcd.setCursor(9,1);

                              lcd.print("K:");

                              lcd.setCursor(11,1);

                              lcd.print(Kt);

                            

                              }

                              else{

                             

                              lcd.setCursor(0,0);

                              lcd.print("Select To Save       ");

                            

                              lcd.setCursor(0,1);

                              lcd.print("Down to Exit           ");

                              };

                            

                              

                              }

                    

                    

                      }

                      

                              else{

                               Serial.println("   Error Wait For Temperature To settle");

                             

                                        while (1) {

                                        read_LCD_buttons();

                                        if(button==2) Calibration();

                                        if(button==3) return;

                                      

                                        lcd.setCursor(0,0);

                                        lcd.print("Bad Results         ");

                                         lcd.setCursor(0,1);

                                        lcd.print("Press Up Exit           ");

                                                                     

                                                                      

                                  }

                    

                            }

 

 

 

 

};

 

 

Alternative download it at:  www.MichaelRatcliffe.com/projects

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 10 years ago +2
    I appreciate also your determination continuing and sure completing this project. It is really good; these detailed descriptions become historical reference for the future. It is just following the last…
  • m.ratcliffe
    m.ratcliffe over 10 years ago +1
    I got an email regarding this project " Hi I'm new Hydro trying to setup a monitor system to a friend. I am with EC sensor now I bought one from Web not sure it's reading well, and I have one more coming…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor +1
    So far it is working like a charm Actually I will take your approach to other sensors as well Instead of supplying 5V from the 5V pin I will switch analog pin to high make all my readings and switch o…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to m.ratcliffe

    I save all my code on Dropbox

    https://www.dropbox.com/s/6u6tuudywygh4h8/UK_CALIBRTE.ino?dl=0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to e14 Contributor

    No we are calibrating for the new plug.

     

    Link me to the calibration code you are running please. [the exact one you are using]

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to m.ratcliffe

    k should be 1.64

    when I put it i main code ec is 1.43

    the solution is 3.05

    Could it because I use different socket?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to e14 Contributor

    You cannot expect to get good results without calibrating the probe.

    Run the calibration Code and you will get a calibrated K value fed into the serial monitor. take this new K value and use it in the code you sent over.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to m.ratcliffe

    changed, it is the same as I hard coded it after, but I changed

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>