Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green House Blog:13.2 - PH Control: Measurement Portion
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
  • Author Author: m.ratcliffe
  • Date Created: 19 Nov 2015 2:48 PM Date Created
  • Views 1521 views
  • Likes 2 likes
  • Comments 2 comments
  • adapted_greenhouse
  • ph
Related
Recommended

Automated Green House Blog:13.2 - PH Control: Measurement Portion

m.ratcliffe
m.ratcliffe
19 Nov 2015

This Blog will cover how to measure pH in your aquaponics/hydroponics system, later we will be using this reading to control the pH.

 

Take a look at the blog below to see why PH is an important factor and why we need to be controlling it.

 

Blog:20.2 - Toying with Chemical Analysis - pH

 

The pH Probe

DFRobot have been nice enough to send me one of their MCU pH sensors, it is the pro model with a longer life than the normal probes [hopefully I cant break this probe].

 

image

 

 

What else you will need:

>pH calibration fluid [4 and 7]

>Arduino mega/uno

 

Wiring diagram

image

 

Calibration

pH probes need to calibrated routinely [one a month is a good idea] so we better have a code that lets us easily calibrate the thing.

 

Wire the probe up like the diagram above, upload the code below and then:

 

1:Place Probe into pH7 calibration fluid, open serial

image

 

2:Take Recommended cell constant and change it in the top of code

image

 

 

 

3:Rinse Probe and place in pH4 calibration fluid

4:Adjust potentiometer on pH meter shield until ph reading in serial is 4

image

 

 

That's it, you are now calibrated and ready to use the pH reading from serial.

 

The Code

This reads the ph probes shield [its an analog value] averages ten readings to reduce any noise and converts the ADC reading into a ph value. outputting the reading to serial.

 

PH Measurement code

/*

   Script to print PH to serial

 

 

   28/8/2015  Michael Ratcliffe  Mike@MichaelRatcliffe.com

  

  

          This program is free software: you can redistribute it and/or modify

    it under the terms of the GNU General Public License as published by

    the Free Software Foundation, either version 3 of the License, or

    (at your option) any later version.

 

 

    This program is distributed in the hope that it will be useful,

    but WITHOUT ANY WARRANTY; without even the implied warranty of

    MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the

    GNU General Public License for more details.

 

 

    You should have received a copy of the GNU General Public License

    along with this program.  If not, see <http://www.gnu.org/licenses/>.

 

    Parts:

    -Arduino - Uno/Mega

   -df Robot Ph Probe Kit [SKU:SEN0169] This is a great PH sensor compared to the ones ive had in the past

 

 

 

    See www.MichaelRatcliffe.com/Projects for a Pinout and user guide or consult the Zip you got this code from

 

*/

 

 

//*********************** User defined variables ****************************//

//pH meter Analog output to Arduino Analog Input 0

int PHPin =A15; 

//The calibration constant for the PH probe

float K=3.64;         

//The Ph we will be calibrating in

int Cal_pH=7;

 

 

//********************** End Of Recomended User Variables ******************//

 

 

//************** Some values for working out the ph*****************//

float Kn=0;

float phValue=0;

int i=0;

long reading=0;

long sum=0;

float average=0;

 

 

 

 

//******************** Setup Loop Runs Once ******************************//

void setup()

{

  Serial.begin(9600);

  startupinfo();

}

 

 

//******************** Main Loops runs Forver **************************//

void loop()

{

ReadPH();

PrintSerial();

Calabrate();

delay(1000);

}

 

 

//*************************Print Some useful startup info **************************//

void startupinfo(){

Serial.println("pH Probe Script for arduino");

Serial.println("Released under GNU by Michael Ratcliffe");

Serial.println("www.MichaelRatcliffe.com");

Serial.println("Element14 'Adapted_Greenhouse'");

Serial.println("Using DFRobot PH Probe Pro ");

Serial.println("How to Use:");

Serial.println("1:Place Probe into pH7 calibration fluid, open serial ");

Serial.println("2:Take Recomened cell constand and change it in the top of code");

Serial.println("3:Rinse Probe and place in pH4 calibration fluid");

Serial.println("4:Adjust potentiometer on pH meter shield until ph reading in serial is 4");

Serial.println("    ");

Serial.println("Thats it your calibrated and your readings are accurate!");

 

}

 

 

 

 

//*************************Take Ten Readings And Average ****************************//

void ReadPH(){

  i=1;

  sum=0;

  while(i<=10){

  reading=analogRead(PHPin);

  sum=sum+reading;

    delay(20);

    i++;

  }

average=sum/10.0;

//converting the average to PH 3.5 part convers mv to ph

phValue=average*K*5/1024; 

 

}

 

 

//*************************** Print useful data to moniter ****************************//

void PrintSerial(){

 

 

Serial.print("    pH:");

Serial.print(phValue);

Serial.println(" ");

 

}

 

 

 

 

//****************** Calculate a K value *********************************************//

void Calabrate(){

 

 

Kn=((Cal_pH*1024)/(average*5));

Serial.print("If pH 7, Cell Konstant=  :");

Serial.println(Kn);

 

 

};

 

 

Temperature Compensation:

For the time being we will not be implementing temperature correcting, because it is not a major effect. We may correct for it later if it proves to be a bigger problem than we anticipated. Here is a example of how measured PH will change with temperature [pH 4 potassium biphthalate buffer standard ] [1]

Temperature [C]             pH
104.00
154.00
204.00
254.01
304.02
354.02
404.04
454.05
504.06
554.08
60

4.09

 

 

Reference:

[1 ]pH Temperature Compensation: PASCO

  • Sign in to reply
Parents
  • DAB
    DAB over 10 years ago

    I am curious, how stable is the probe over time?

     

    You get the data you need for the calibration test, but have you looked at the values over time?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to DAB

    I got good readings over a hour, its a bit awkward to have the data over serial when working on the laptop. The next blog will be with a LCD and logs min/max PH, so I will leave it in some water overnight for a little longer of a test.


    It certainly feels a lot sturdier than the ones ive used in the past and the spec sheet says it is for "long term use" but I dont have enough data to confirm this at the moment. I hope it does live upto its claims, pH is what ive always struggled with the most. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to DAB

    I got good readings over a hour, its a bit awkward to have the data over serial when working on the laptop. The next blog will be with a LCD and logs min/max PH, so I will leave it in some water overnight for a little longer of a test.


    It certainly feels a lot sturdier than the ones ive used in the past and the spec sheet says it is for "long term use" but I dont have enough data to confirm this at the moment. I hope it does live upto its claims, pH is what ive always struggled with the most.