Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green House Blog:13.3 - PH Control: PH Probe LCD Readout + Gui
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
  • Author Author: m.ratcliffe
  • Date Created: 24 Nov 2015 10:30 PM Date Created
  • Views 2372 views
  • Likes 2 likes
  • Comments 2 comments
  • adapted_greenhouse
  • vertical_farming
  • ph
  • aquaponics
  • arduino
Related
Recommended

Automated Green House Blog:13.3 - PH Control: PH Probe LCD Readout + Gui

m.ratcliffe
m.ratcliffe
24 Nov 2015


DFRobot were nice enough to send me one of their pH pro MCU probes [Longer lasting] but this tutorial and code will work for any analog pH MCU meter [ebay special etc] these are coming down in price rapidly but I recommend calibrating often. I'm hoping the pro model can go longer between calibrations and still hold true. I put the probe in some pH4 buffer solution over night and the LCD printout gave a   min:3.92   max:4.02   this was probably caused by a temperature change. But it is good enough for our application without compensating for temperature.


You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image



This is the style of PH  probe we will be building the PH controller in the next blog, it has been built and in action now. Once it has passed [or is it if] its month of problem free use the code will be uploaded here, under gnu as always. 



Pin-out

image

 

The Code

 

We have writen the code mainly by calling functions [blocks of code] from the main loop. It can be helpful to write codes in this way because many projects will require similar blocks of code [uptime, max ram , temperature etc] and we can quickly make a new script using these blocks of code.

 

Header 1

/*

  Script to print PH to serial

 

 

  28/8/2015  Michael Ratcliffe  Mike@MichaelRatcliffe.com

 

 

          This program is free software: you can redistribute it and/or modify

    it under the terms of the GNU General Public License as published by

    the Free Software Foundation, either version 3 of the License, or

    (at your option) any later version.

 

 

    This program is distributed in the hope that it will be useful,

    but WITHOUT ANY WARRANTY; without even the implied warranty of

    MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the

    GNU General Public License for more details.

 

 

    You should have received a copy of the GNU General Public License

    along with this program.  If not, see <http://www.gnu.org/licenses/>.

 

    Parts:

    -Arduino - Uno/Mega

  -df Robot Ph Probe Kit [SKU:SEN0169] This is a great PH sensor compared to the ones ive had in the past

 

 

 

    See www.MichaelRatcliffe.com/Projects for a Pinout and user guide or consult the Zip you got this code from

 

*/

 

 

//************************** Libraries Needed To Compile The Script [See Read me In Download] ***************//

// Both below Library are custom ones [ SEE READ ME In Downloaded Zip If You Dont Know how To install] Use them or add a pull up resistor to the temp probe

 

 

#include <OneWire.h>

#include <DallasTemperature.h>

#include <LiquidCrystal.h> //Standard LCD Lbrary

#include <EEPROM.h> //Standard EEPROM Library

 

 

//*********************** User defined variables ****************************//

//pH meter Analog output to Arduino Analog Input 0

int PHPin =A15;

//The calibration constant for the PH probe

float K_PH=3.64;       

//used for min/max logs

float MinPH=10;

float MaxPH=0;

 

 

 

 

//************ Temp Probe Related *********************************************//

#define ONE_WIRE_BUS 26          // Data wire For Temp Probe is plugged into pin 10 on the Arduino

const int TempProbePossitive =22;  //Temp Probe power connected to pin 9

const int TempProbeNegative=24;    //Temp Probe Negative connected to pin 8

float Temperature=0.0;

float MinT=100;

float MaxT=0;

 

 

 

 

//********************** End Of Recomended User Variables ******************//

 

 

 

 

//************** Some values for working out the ph*****************//

float Kn=0;

float phValue=0;

int i=0;

long reading=0;

unsigned long sum=0;

float average=0;

 

 

// select the pins used on the LCD panel

LiquidCrystal lcd(8, 9, 4, 5, 6, 7);

 

 

// define some values used by the panel and buttons

int lcd_key    = 0;

int adc_key_in  = 0;

int button =0;

#define btnRIGHT  1

#define btnUP    2

#define btnDOWN  3

#define btnLEFT  4

#define btnSELECT 5

#define btnNONE  6

 

 

int Screen =1;

//Max number of screens on lcd

const int Last_Screen_no =4;

//used to debounce input button

int buttonLast=0;

 

 

OneWire oneWire(ONE_WIRE_BUS);// Setup a oneWire instance to communicate with any OneWire devices

DallasTemperature sensors(&oneWire);// Pass our oneWire reference to Dallas Temperature.

 

 

//************************** Just Some basic Definitions used for the Up Time LOgger ************//

long Day=0;

int Hour =0;

int Minute=0;

int Second=0;

int HighMillis=0;

int Rollover=0;

 

 

//***************** Specifying where to sotre the calibration value [non volatile memory **//

int value; //we use this to check if memory has been writen or not

int addresCalibrationPH=50;

 

 

//************************************** Setup Loop Runs Once ****************//

void setup()

{

  Serial.begin(9600);

  pinMode(TempProbeNegative , OUTPUT ); //seting ground pin as output for tmp probe

  digitalWrite(TempProbeNegative , LOW );//Seting it to ground so it can sink current

  pinMode(TempProbePossitive , OUTPUT );//ditto but for positive

  digitalWrite(TempProbePossitive , HIGH );

  read_Temp();// getting rid of the first bad reading

  Read_Eprom();

  Splash_Screen();

 

 

}

//******************************** End Of Setup **********************************//

 

 

//******************** Main Loops runs Forver ************************************//

void loop()

{

 

 

//All these functions are put below the main loop, keeps the loop logic easy to see

read_LCD_buttons();

read_Temp();

Log_Min_MaxTemp();

ReadPH();

Log_Min_MaxPH();

uptime();

CalibratePH();

PrintReadings();

delay(100);

};

 

 

//************************** End Of Main Loop ***********************************//

 

 

 

 

//*************************Print Some useful startup info **************************//

void startupinfo(){

Serial.println("pH Probe Script for arduino");

Serial.println("Released under GNU by Michael Ratcliffe");

Serial.println("www.MichaelRatcliffe.com");

Serial.println("Element14 'Adapted_Greenhouse'");

Serial.println("Using DFRobot PH Probe Pro ");

Serial.println("How to Use:");

Serial.println("1:Place Probe into pH7 calibration fluid, open serial ");

Serial.println("2:Take Recomened cell constand and change it in the top of code");

Serial.println("3:Rinse Probe and place in pH4 calibration fluid");

Serial.println("4:Adjust potentiometer on pH meter shield until ph reading in serial is 4");

Serial.println("    ");

Serial.println("Thats it your calibrated and your readings are accurate!");

 

}

 

 

//***************************** Function to read temperature ********************************//

void read_Temp(){

sensors.requestTemperatures();// Send the command to get temperatures

Temperature=sensors.getTempCByIndex(0); //Stores Value in Variable

 

 

 

 

}

 

 

 

 

 

 

//*************************Take Ten Readings And Average ****************************//

void ReadPH(){

  i=1;

  sum=0;

  while(i<=100){

  reading=analogRead(PHPin);

  sum=sum+reading;

    delay(20);

    i++;

  }

average=sum/i;

//converting the average to PH 3.5 part convers mv to ph

phValue=average*K_PH*5/1024;

 

}

 

 

 

 

 

 

 

 

 

 

//****************************** Reading LCd Buttons ****************************//

void read_LCD_buttons(){

  adc_key_in = analogRead(0);      // read the value from the sensor

// my buttons when read are centered at these valies: 0, 144, 329, 504, 741

// we add approx 50 to those values and check to see if we are close

if (adc_key_in > 1000)  button =0;

 

 

else if (adc_key_in < 50)  button =1;

else if (adc_key_in < 250)  button =2;

else  if (adc_key_in < 450)  button =3;

else if (adc_key_in < 650)  button =4;

else if (adc_key_in < 850)  button =5;

 

 

 

 

//Second bit stops us changing screen multiple times per input

if(button==2&&buttonLast!=button){

Screen++;

 

 

}

else if (button==3&&buttonLast!=button){

Screen--;

};

 

 

if (Screen>=Last_Screen_no) Screen=Last_Screen_no;

if(Screen<=1) Screen=1;

 

 

buttonLast=button;

};

 

 

 

 

 

 

//************************ Uptime Code - Makes a count of the total up time since last start ****************//

 

 

void uptime(){

//** Making Note of an expected rollover *****//

if(millis()>=3000000000){

HighMillis=1;

 

 

}

//** Making note of actual rollover **//

if(millis()<=100000&&HighMillis==1){

Rollover++;

HighMillis=0;

}

 

 

long secsUp = millis()/1000;

 

 

Second = secsUp%60;

 

 

Minute = (secsUp/60)%60;

 

 

Hour = (secsUp/(60*60))%24;

 

 

Day = (Rollover*50)+(secsUp/(60*60*24));  //First portion takes care of a rollover [around 50 days]

                 

};

 

 

 

 

//************************** Printing somthing useful to LCd on start up **************************//

void Splash_Screen(){

 

 

lcd.begin(16, 2);              // start the library

lcd.setCursor(0,0);

delay(1000);

lcd.print("PH meter      ");

lcd.setCursor(0,1);

delay(1000);

lcd.print("Mike Ratcliffe");

lcd.setCursor(0,1);

delay(1000);

lcd.setCursor(0,1);

lcd.print("Free Software  ");

delay(1000);

lcd.setCursor(0,1);

lcd.print("Mike Ratcliffe");

delay(1000);

lcd.setCursor(0,1);

lcd.print("Free Software  ");

delay(1000);

  lcd.setCursor(0,0);

lcd.print("To Navigate        ");

  lcd.setCursor(0,1);

lcd.print("Use Up-Down    ");

delay(3000);

  lcd.setCursor(0,0);

lcd.print("To Calibrate      ");

  lcd.setCursor(0,1);

lcd.print("Hold Select      ");

delay(3000);

 

 

 

 

};

 

 

void Read_Eprom(){

 

 

//************** Restart Protection Stuff ********************//

  //the 254 bit checks that the adress has something stored to read [we dont want noise do we?]

  value = EEPROM.read(addresCalibrationPH);

  if (value <=254) K_PH=value*0.02;

 

 

};

 

 

//******************************* Checks if Select button is held down and enters Calibration routine if it is ************************************//

void CalibratePH(){

 

 

 

//we check if we are on ph screen and the select button is held

if(Screen!=4) return;

if(button!=5) return;

else delay(1000);

read_LCD_buttons();

if(button!=5) return;

 

 

//we need to stop in this loop while the user calibrates

while(1){

read_LCD_buttons();

lcd.setCursor(0,0);

lcd.print("Ph Probe in pH7  ");

lcd.setCursor(0,1);

lcd.print("Press Right            ");

//user pressed right?

if(button==1) break;

delay(100);

      };

 

lcd.setCursor(0,0);

lcd.print("Calibrating              ");

lcd.setCursor(0,1);

lcd.print("pH Probe                ");

 

 

//let probe settle

delay(2000);

 

 

//read the ph probe

ReadPH();

Kn=((7*1024)/(average*5));

 

 

 

 

while (1) { // wee need to keep this function running until user opts out with return function

                         

  read_LCD_buttons();

  if(button==4) return; //exits the loop without saving becauser user asked so

  if (button==5){

                           

                           

  K_PH=Kn; //saving the new cell constant

                         

                         

  //*******Saving the new value to EEprom**********//

  value=Kn/0.02;

  EEPROM.write(addresCalibrationPH, value);

  lcd.setCursor(0,0);

  lcd.print("Saved Calibration        ");

                                                       

  lcd.setCursor(0,1);

  lcd.print("K:                        ");

  lcd.setCursor(3,1);

  lcd.print(Kn);

  delay(2000);

 

  lcd.setCursor(0,0);

  lcd.print("Now pH4 and          ");

                                                       

  lcd.setCursor(0,1);

  lcd.print("Adjust Pot                      ");

 

  delay(4000);

  //Put back to main screen and exit calibration

    Screen=1;

  return;

 

 

 

 

 

 

 

                              }

                         

if(millis()%4000>=2000){

      ReadPH();

    lcd.setCursor(0,0);

    lcd.print("Calibrated        ");

                         

                         

      lcd.setCursor(0,1);

      lcd.print("PH:                      ");

      lcd.setCursor(3,1);

      lcd.print(phValue);

      lcd.setCursor(8,1);

      lcd.print("K:");

      lcd.setCursor(11,1);

      lcd.print(Kn);

                         

                              }

else{

                         

      lcd.setCursor(0,0);

      lcd.print("Select To Save      ");                 

      lcd.setCursor(0,1);

      lcd.print("Down to Exit          ");

                              };

                         

                           

                              }

 

 

};

 

 

//******************************* LOGS Min/MAX Values*******************************//

                          void Log_Min_MaxTemp(){

                       

                     

                            if(Temperature>=MaxT) MaxT=Temperature;

                            if(Temperature<=MinT) MinT=Temperature;

                                           

                                             

                          };

 

 

//******************************* LOGS Min/MAX Values*******************************//

                          void Log_Min_MaxPH(){

                       

                     

                            if(phValue>=MaxPH) MaxPH=phValue;

                            if(phValue<=MinPH) MinPH=phValue;

                                           

                                             

                          };

 

 

 

 

 

 

void PrintReadings(){

           

                Serial.print("pH: ");

                Serial.print(phValue);

                Serial.print(Temperature);

                Serial.print(" *C  ");

 

                                      //** First Screen Shows Temp and EC **//

                                      if(Screen==1){

                                      lcd.setCursor(0,0);

                                      lcd.print("Arduino pH  ");

                                      lcd.setCursor(0,1);

                                      lcd.print("pH:              ");

                                      lcd.setCursor(3,1);

                                      lcd.print(phValue);

                                      lcd.setCursor(9,1);

                                      lcd.print(Temperature);

                                      lcd.print("'C");

                                      }

                                 

                                 

                                      //**Third Screen Shows Min and Max **//

                                      else if(Screen==2){

                                      lcd.setCursor(0,0);

                                      lcd.print("Min:              ");

                                      lcd.setCursor(4,0);

                                      lcd.print(MinPH);

                                      lcd.setCursor(9,0);

                                      lcd.print(MinT);

                                      lcd.print("'C");

                                      lcd.setCursor(0,1);

                                      lcd.print("Max:              ");

                                      lcd.setCursor(4,1);

                                      lcd.print(MaxPH);

                                      lcd.setCursor(9,1);

                                      lcd.print(MaxT);

                                      lcd.print("'C");

                                      }

                                 

                                 

                                      else if(Screen==3){

                               

                                      lcd.setCursor(0,0);

                                      lcd.print("Uptime Counter:              ");

                                 

                                      lcd.setCursor(0,1);

                                      lcd.print("                                    ");//Clearing LCD

                                      lcd.setCursor(0,1);

                                      lcd.print(Day);

                                      lcd.setCursor(3,1);

                                      lcd.print("Day");

                                      lcd.setCursor(8,1);

                                      lcd.print(Hour);

                                      lcd.setCursor(10,1);

                                      lcd.print(":");

                                      lcd.setCursor(11,1);

                                      lcd.print(Minute);

                                      lcd.setCursor(13,1);

                                      lcd.print(":");

                                      lcd.setCursor(14,1);

                                      lcd.print(Second);

                                 

                                 

                                      }

                   

                                      else if(Screen==4){

                                   

                                      lcd.setCursor(0,0);

                                      lcd.print("Calibrate pH          ");

                                 

                                 

                                      lcd.setCursor(0,1);

                                      lcd.print("Hold Select            ");

                               

                                      }

       

 

 

};

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Great post. I am getting curious about the materials in your PH sensor. If I can find some time I might investigate the chemistry and physics happening to degrade the sensor. DAB
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to DAB +1
    Hey DAB, I dont know what they are made from [usually dont get much info with the cheap ebay ones] But I dont think im the only person with the problem, I'm at a friends aquaponics set-up today and he…
Parents
  • DAB
    DAB over 10 years ago

    Great post.

     

    I am getting curious about the materials in your PH sensor.

     

    If I can find some time I might investigate the chemistry and physics happening to degrade the sensor.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to DAB

    Hey DAB, I dont know what they are made from [usually dont get much info with the cheap ebay ones] But I dont think im the only person with the problem, I'm at a friends aquaponics set-up today and he has had a similar problem.

    [Here is a picture of the new long life probe we are testing alongside some of the failed ones]

    image

     

     

    The probes usually, look clean when they fail but maybe the membrane is blocking up and would last longer if we put them in a shielded/filtered cage. Me and a few collaborators are going to start some testing of filter tips for the PH probes, hopefully we can 3d print a cap that incorporates a cleanable filter membrain, but again this is a long term test, its going to be a busy 2016.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to DAB

    Hey DAB, I dont know what they are made from [usually dont get much info with the cheap ebay ones] But I dont think im the only person with the problem, I'm at a friends aquaponics set-up today and he has had a similar problem.

    [Here is a picture of the new long life probe we are testing alongside some of the failed ones]

    image

     

     

    The probes usually, look clean when they fail but maybe the membrane is blocking up and would last longer if we put them in a shielded/filtered cage. Me and a few collaborators are going to start some testing of filter tips for the PH probes, hopefully we can 3d print a cap that incorporates a cleanable filter membrain, but again this is a long term test, its going to be a busy 2016.