Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Automated Green House Blog:8.1 -  Water Usage [LCD and Uno]
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
  • Author Author: m.ratcliffe
  • Date Created: 15 Oct 2015 5:10 PM Date Created
  • Views 2018 views
  • Likes 3 likes
  • Comments 6 comments
  • greenhouse_supplier
  • arduino
Related
Recommended

Automated Green House Blog:8.1 -  Water Usage [LCD and Uno]

m.ratcliffe
m.ratcliffe
15 Oct 2015

A updated Flow meter monitor to incorporate a LCD shield, log min and max flow rates.

 

If you want to incorporate some error logging [water loss or burst pipe] see the last blog for setting error flags.

 

LCD Shiled that it will work with:

 

image

 

Pinout [Solder onto LCD shiled is preferred ] :

 

image

 

Ignore external pull up, we are doing that in software instead

 

 

Header 1

 

/* This script is used to make sense of the output from a hall effect water flow meter and make a note of any problems

 

 

Michael Ratcliffe  Mike@MichaelRatcliffe.com

  

    This program is free software: you can redistribute it and/or modify

    it under the terms of the GNU General Public License as published by

    the Free Software Foundation, either version 3 of the License, or

    (at your option) any later version.

 

 

    This program is distributed in the hope that it will be useful,

    but WITHOUT ANY WARRANTY; without even the implied warranty of

    MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the

    GNU General Public License for more details.

 

 

    You should have received a copy of the GNU General Public License

    along with this program.  If not, see <http://www.gnu.org/licenses/>.

  

  

  

  

    Components:

    See main folder for sensor data sheets, required liabaries and extra information: [can be downloaded via www.michaelratcliffe.com]

  

    All power systems should be powerd of DC voltage of below 48v for safter [water is around] 12v is prefferable and cheapest. As always this is a DIY project and done at your own risk.

  

  

    >Arduino Uno

    >Hall Effect Water Flow Meter 5v

    >LCD button Shield [Hobby tronix]

 

 

  

*/

// including some libraries for interfacing with harware

#include <LiquidCrystal.h> //Standard LCD Lbrary

 

 

 

 

 

 

//******************************** User Defined Variables *******************************************************//

 

 

#define Water_pin 2

 

 

/*/####### Meter Specs ####//

Most meters are shipped with a forumla to work out flow rate

F=X*Q

Q=Flow rate in L/min [make sure its in L/min and not L/hr]

F=Frequency

X= variable

To work out click per L  Clicks = 60*X

*/

 

 

float Click_Per_L = 450; // this depends on your flow meter

 

 

 

 

//*********************8* Setting up LCD ************************//

// select the pins used on the LCD panel

LiquidCrystal lcd(8, 9, 4, 5, 6, 7);

 

 

// define some values used by the panel and buttons

int lcd_key     = 0;

int adc_key_in  = 0;

int button =0;

#define btnRIGHT  1

#define btnUP     2

#define btnDOWN   3

#define btnLEFT   4

#define btnSELECT 5

#define btnNONE   6

 

 

int Screen =1;

 

 

//used to debounce input button

int buttonLast=0;

 

 

//********************** Some Variables For Loging Min/Max Values ********************************//

float MinFLOW=100;

float MaxFLOW=0;

 

 

 

 

//************************** Just Some basic Definitions used for the Up Time LOgger ************//

long Day=0;

int Hour =0;

int Minute=0;

int Second=0;

int HighMillis=0;

int Rollover=0;

 

 

 

 

//***************************** End Of User Defined Variables **************************************************//

 

 

unsigned long PulseCount=0;  //counter for water meter pulses

unsigned long Current_PulseCount=0; // the one we will be doing maths on

int Last_Reading=0;

int Readings=0;

float Water_Used=0;

float Flow_Rate= 0;

unsigned long Last_Count =0;

 

 

 

 

//**************************** Setup Routine , Runs Once and Sets used pins to correct value *******************//

void setup() {

Serial.begin(9600); // starting Serial Com's

 

//Stoping noise from being a problem, pin is high untill hall sensor pulls it low

pinMode(Water_pin, INPUT);

digitalWrite(Water_pin, HIGH);// saves having an external pullup

    

//External Interrupts: This is what the watr meter pulse count is collected from     

attachInterrupt(0, WaterCounter, FALLING);  //watermeter pulse output connected to pin3

 

//************* Splash Screen *******************//

// Maybe change this to your details to add that finishing touch [max of 16 charictors per line]

 

 

lcd.begin(16, 2);              // start the library

lcd.setCursor(0,0);

delay(1000);

lcd.print("Water Meter          ");

lcd.setCursor(0,1);

delay(1000);

lcd.print("Mike Ratcliffe");

lcd.setCursor(0,1);

delay(1000);

lcd.setCursor(0,1);

lcd.print("Free Software   ");

delay(1000);

lcd.setCursor(0,1);

lcd.print("Mike Ratcliffe");

delay(1000);

lcd.setCursor(0,1);

lcd.print("Free Software   ");

delay(3000);

  lcd.setCursor(0,0);

lcd.print("To Navigate         ");

  lcd.setCursor(0,1);

lcd.print("Use Up-Down     ");

delay(3000);

 

 

 

 

//Clearing LCD SCREEN

lcd.setCursor(0,0);

lcd.print("                                   ");

lcd.setCursor(0,1);

delay(1000);

lcd.print("                                    ");

 

 

 

 

};

 

 

 

//************************************** Main Loop that will continualy run ******************************************//

void loop(){

 

 

//calls uptime function below main loop

uptime();

 

 

 

 

//************** If Statment that will run every second ******************//

            if (Last_Reading!=Second) {

            Last_Reading=Second; //Makes note of the last second

            Readings=1;          //Tell serial there is data to transmit

 

 

            //Turn off interupt while we take a quick note of it and then turn it back on

            detachInterrupt(0); //

            Current_PulseCount=PulseCount; // making note of pulse count

            attachInterrupt(0, WaterCounter, FALLING);  //watermeter pulse output connected to pin3

          

            Flow_Rate=((Current_PulseCount-Last_Count)/Click_Per_L); 

            Water_Used=(1/(Click_Per_L/Current_PulseCount)); //cant recall why I did it this way, maybe to retain float capabilities

          

            Last_Count=Current_PulseCount;                   // Makes a note of the last reading

 

 

                                    };

 

 

 

 

read_LCD_buttons();

LogFlow();

PrintReadings();

 

 

 

 

    

delay(10);

};

//*************************************************END OF LOOP ******************************************************//

 

 

 

 

//******************* Uptime Counter **************************************************//

//WE need an uptime counter to verify our total flow readout is valid

 

 

void uptime(){

//** Making Note of an expected rollover *****//

if(millis()>=3000000000){

HighMillis=1;

 

}

//** Making note of actual rollover **//

if(millis()<=100000&&HighMillis==1){

Rollover++;

HighMillis=0;

}

long secsUp = millis()/1000;

Second = secsUp%60;

Minute = (secsUp/60)%60;

Hour = (secsUp/(60*60))%24;

Day = (Rollover*50)+(secsUp/(60*60*24));  //First portion takes care of a rollover [around 50 days]                 

};

 

 

 

 

//******************************* LOGS Min/MAX Values and Uptime Counter*******************************//

void LogFlow(){

 

  if(Flow_Rate>=MaxFLOW)  MaxFLOW=Flow_Rate;

  if(Flow_Rate<=MinFLOW)  MinFLOW=Flow_Rate;

};

 

 

 

 

 

 

 

 

 

 

 

 

//****************************** Reading LCd Buttons ****************************//

void read_LCD_buttons(){

  adc_key_in = analogRead(0);      // read the value from the sensor

// my buttons when read are centered at these valies: 0, 144, 329, 504, 741

// we add approx 50 to those values and check to see if we are close

if (adc_key_in > 1000)  button =0;

 

 

else if (adc_key_in < 50)   button =1;

else if (adc_key_in < 250)  button =2;

else  if (adc_key_in < 450)  button =3;

else if (adc_key_in < 650)  button =4;

else if (adc_key_in < 850)  button =5;

 

 

 

 

//Second bit stops us changing screen multiple times per input

if(button==2&&buttonLast!=button){

Screen++;

 

 

}

else if (button==3&&buttonLast!=button){

Screen--;

};

 

 

if (Screen>=3) Screen=3;

if(Screen<=1) Screen=1;

 

 

buttonLast=button;

};

 

 

 

 

 

 

 

 

 

 

//**************This Loop Is called From Main Loop- Prints to serial usefull info and updates LCD *************//

void PrintReadings(){

 

 

//No Point updating if there is no new data

if (button>=1||Readings==1) {

  Readings=0;

 

 

//Printing Some Uptime Values

  Serial.print(F("Uptime: ")); // The "F" Portion saves your SRam Space

  Serial.print(Day);

  Serial.print(F("  Days  "));

  Serial.print(Hour);

  Serial.print(F("  Hours  "));

  Serial.print(Minute);

  Serial.print(F("  Minutes  "));

  Serial.print(Second);

  Serial.println(F("  Seconds"));

 

 

//Printing Some Water Flow info

  Serial.print(F("Total Water Used"));

Serial.print(Water_Used);

Serial.println(F(" L"));

Serial.print(F("Current Flow Rate: "));

Serial.print(Flow_Rate);

  Serial.println(F(" L/s"));

 

 

 

                     //First Screen is Total Flow and flowrate

                      if(Screen==1){

                      lcd.setCursor(0,0);

                      lcd.print("Volume:                ");

                      lcd.setCursor(7,0);

                      lcd.print(Water_Used);

                      lcd.setCursor(13,0);

                      lcd.print("L");

                    

                      lcd.setCursor(0,1);

                      lcd.print("FlRate:             ");

                      lcd.setCursor(7,1);

                      lcd.print(Flow_Rate);

                      lcd.setCursor(13,1);

                      lcd.print("L/s");

                      }

 

 

                   

                                           

                      }

                      //Min and Max flowrates

                       else if(Screen==2){

                      lcd.setCursor(0,0);

                      lcd.print("Min:              ");

                       lcd.setCursor(4,0);

                       lcd.print(MinFLOW);

                       lcd.setCursor(13,0);

                       lcd.print("L/s");

                      lcd.setCursor(0,1);

                      lcd.print("Max:               ");

                      lcd.setCursor(4,1);

                      lcd.print(MaxFLOW);

                      lcd.setCursor(13,1);

                      lcd.print("L/s");

                  

                       }

 

 

                       //Printing uptime

                        else if(Screen==3){

                 

                      lcd.setCursor(0,0);

                      lcd.print("Uptime Counter:              ");

                  

                      lcd.setCursor(0,1);

                      lcd.print("                                     ");//Clearing LCD

                      lcd.setCursor(0,1);

                      lcd.print(Day);

                      lcd.setCursor(3,1);

                      lcd.print("Day");

                      lcd.setCursor(8,1);

                      lcd.print(Hour);

                      lcd.setCursor(10,1);

                      lcd.print(":");

                      lcd.setCursor(11,1);

                      lcd.print(Minute);

                      lcd.setCursor(13,1);

                      lcd.print(":");

                      lcd.setCursor(14,1);

                      lcd.print(Second);

                  

                  

                       }

     

 

 

 

};

 

 

 

 

//*************Interupt routine for water meter readings - Runs everytime sensor has a pulse *************//

 

 

void WaterCounter() {

 

   // Increment the pulse counter

  PulseCount++;

 

};

  • Sign in to reply

Top Comments

  • gadget.iom
    gadget.iom over 11 years ago in reply to m.ratcliffe +1
    Your post is informative and progressive. Entirely what the design challenges are all about. Just out of curiosity, is this the Flow Meter you are using? http://www.seeedstudio.com/depot/G12-Water-Flow…
  • neilk
    neilk over 11 years ago +1
    very informative post Thanks for sharing. Neil
Parents
  • gadget.iom
    gadget.iom over 11 years ago

    Nice work! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • gadget.iom
    gadget.iom over 11 years ago

    Nice work! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to gadget.iom

    Thanks Paul,

    It is not high end stuff but some people might find it useful.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to m.ratcliffe

    Your post is informative and progressive. Entirely what the design challenges are all about. image

    Just out of curiosity, is this the Flow Meter you are using?

    http://www.seeedstudio.com/depot/G12-Water-Flow-Sensor-p-635.html

     

    Keep up the good work!

    Paul

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to gadget.iom

    Im using an ancient Flow meter that I found in the barn, that I had to replace the hall sensor in.

    But this should work with the one you linked to, or any 5v based hall effect meter for that matter. Got a project in mind?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago in reply to m.ratcliffe

    Not yet. But I keep an open mind. :)