• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Look What Came today!!!
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
  • Author Author: e14 Contributor
  • Date Created: 12 Aug 2015 7:29 PM Date Created
  • Views 699 views
  • Likes 1 like
  • Comments 4 comments
  • solar_farm
Related
Recommended

Look What Came today!!!

e14 Contributor
e14 Contributor
12 Aug 2015

So, I am working on finishing up a new blog about how my plant choice will affect the design and finishing my design, which will be posted as soon as I find out what plant I can use. Right now, I am hoping to choose peas, pak choi, or leafy greens. As a sidenote, I did not find any letter in the package about plant choice. I will give a brief description of my top picks. Number one being they all grow well in aquaponic systems and number two they all do not require too much sunlight.(A big plus because this project is indoors and I don't want to buy a sun lamp because that would kind of cheat the purpose of being solar-powered. So indoor lighting is truly a last resort.) I am thinking about using the top floor of the house(to maximize my houses' sunlight) for the vertical farm, so I might have to come up with a cooling system to deal with the scorching heat. I kind of want to try a vegetable that is compact, but also has a lot of problems in the outside world(especially pests) as an indoor vertical farm would be able to avoid these problem and stand out more. Right now, I am leaning towards lettuce because it has a larger market of the three. (http://supplementsos.com/nutrition-stats/most-consumed-foods/most-eaten-vegetables-usa/)

Also, lettuce requires less sunlight and when crowded outside attracts weeds and pests. (Not a problem with my farm because there is no soil) Unfourtunately, I will have to worry about the temperature of the top floor, which I checked with the new Puck sensor to be about 90-100 degrees, so I will put my solution for this problem later, but I will most likely have to have a mini-AC unit in each level unless I get something else planned. Luckily, the flip side is I can get a reliable 25k lux when the sun hit the window. (The window faces east so that's half a day of full light) The pump logistics will take me a whole day to figure out though and at least some sunlight will be lost as the light passes through the glass. Today going to work a bit on the other blog, and then experiment with Simplicity Studios.(SS sounds to spy-like)

Attachments:
image
  • Sign in to reply

Top Comments

  • element14Dave
    element14Dave over 11 years ago in reply to e14 Contributor +1
    You can expect to see an update on the plant requirements later this week.
Parents
  • element14Dave
    element14Dave over 11 years ago

    Hey nightdrakon l

     

    I have moved this over the Vertical Farming area.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • element14Dave
    element14Dave over 11 years ago

    Hey nightdrakon l

     

    I have moved this over the Vertical Farming area.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to element14Dave

    Thanks. Just wondering could you explain the plants we are supposed to use? Is the interpretation of any edible plant correct?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • element14Dave
    element14Dave over 11 years ago in reply to e14 Contributor

    You can expect to see an update on the plant requirements later this week.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to element14Dave

    cool