Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Modular Farm Blog: Post 11 - Automatic Nutrient Dispenser Part III
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
  • Author Author: jmbranco76
  • Date Created: 15 Oct 2015 10:47 PM Date Created
  • Views 1894 views
  • Likes 5 likes
  • Comments 6 comments
  • modular_farm
  • hydroponic
  • net_zero_energy_farming
  • growsharp
  • magnetic_level_sensor
Related
Recommended

Modular Farm Blog: Post 11 - Automatic Nutrient Dispenser Part III

jmbranco76
jmbranco76
15 Oct 2015

Hi vertical farmers,

 

In the previous post we discussed our power source and energy storage system and how we intend to supply our Modular Farm taking the most energy out of a solar panel while keeping the battery charge under control.

 

We will go back in time now to complete our Automatic Nutrient Dispenser topic (discussed on post 3 and post 4). Just to recapitulate, we discussed different possible implementations for our nutrient doser and decided to use a magnetic based implementation to reach a high resolution level detector. We also simulated its operation while waiting the delivery of solenoid valves. In this post we will show our nutrient doser functional prototype, and show how we can programmatically control it.

 

The Implementation

As you may remember we will use 4 reservoirs containing 2 concentrated nutrient components, water and a pH corrector (typically an acid). Sequentially the buffer reservoir, a tube, is filled with each of the 4 liquids while its volume is controlled via the magnetic sensors. The sensors (Hall sensors connected to the eight channels of EZR32WG ADC) were placed linearly to have a resolution of 2 milliliters of liquid in the tube.

 

The Automatic Nutrient Dispenser starts its operation pouring water into the tube to avoid contamination. It proceeds pouring the nutrient into the tube and deploying the solution into the reservoir. Next, it fills the tube with water and pours into the reservoir, cleaning the tube.

 

The system works using solenoid valves for filling and emptying the tube.

 

On the following video we show the operation of our Automatic Nutrient Dispenser with only one reservoir and simulating the measurement of water and one nutrient.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Inside the tube there is a floating container filled with air and a neodymium magnet.

 

The module receives commands and executes them according to the following program:

 

image

Figure 1. Automatic Nutrient Dispenser operation flowchart.

 

Also pH readings and control needs to be implemented. We will come back to this topic later.

 

Feel free to put any questions or share your thoughts and suggestions on our design and methodologies.

 

Keep in touch!

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 11 years ago +1
    Very interesting implementation. Always fine to see things coming real ! Enrico
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    Nice to see that all the work done a few weeks ago was worth it. I hope that the next step will be putting all the system working together, not only with the doser but also with the water pump and the…
  • DAB
    DAB over 11 years ago +1
    Nice test, when are you going to setup your first grow cycle? DAB
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Nice to see that all the work done a few weeks ago was worth it.

    I hope that the next step will be putting all the system working together, not only with the doser but also with the water pump and the other sensors.

     

    Great job José

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jmbranco76
    jmbranco76 over 11 years ago in reply to e14 Contributor

    Thanks João image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jmbranco76
    jmbranco76 over 11 years ago in reply to e14 Contributor

    Thanks João image