• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog New growing surface
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
  • Author Author: ochikov
  • Date Created: 4 Sep 2015 2:17 PM Date Created
  • Views 1388 views
  • Likes 6 likes
  • Comments 9 comments
Related
Recommended

New growing surface

ochikov
ochikov
4 Sep 2015

Hello Everybody,

Yesterday I just finished my conception for new growing surface. I'm not very good carpenter and I live in a city that is hard to find wooden material. That's why I use my imagination. You can see the pictures bellow. This is just the first phase of my project. The difficult phases are to make the whole process of growing plants - automated. More information will be provided soon!

 

imageimageimageimage

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 11 years ago in reply to ochikov +2
    About this problem, I have almost all the walls of my home the same, so I was worrying about how it was possible that the entire kitchen and the 70litres hot water tank was on the wall. Then a friend that…
  • ochikov
    ochikov over 11 years ago in reply to RWReynolds +1
    Hello! Thank you! First I want to try it without mounting on the wall. The reason is that my light source is from another direction. This week I will mount LED light emitted about 6000K. Then I will try…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hey Ognyan, cool way of doing the system. I do have a question though: what's the water cycle? Do you re-use the water or where does the water go?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hey Ognyan, cool way of doing the system. I do have a question though: what's the water cycle? Do you re-use the water or where does the water go?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ochikov
    ochikov over 11 years ago in reply to e14 Contributor

    Hello, I have holes and double "floor" equiped with another layer of naylon that takes care about the used water. I make a tube that drain this water in another big bottle. It has a lot of stuff inside it (like pieces of ground). I then use it to water the farm again.