• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Nutrients, nutrients everywhere
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
  • Author Author: sftwrngnr
  • Date Created: 7 Aug 2015 7:43 AM Date Created
  • Views 838 views
  • Likes 1 like
  • Comments 5 comments
  • ambient_growth
Related
Recommended

Nutrients, nutrients everywhere

sftwrngnr
sftwrngnr
7 Aug 2015

So I've noticed that several of the challengers already have experience with hydroponics, aquaponics and aeroponics. I... do not. So, I've done some due diligence, and decided that I'm going to go with General Hydroponics "Flora Series" of hydroponic nutrients.  The obvious issue, is that it's a three part solution, so my system will need to measure PH/TDS prior to anything being added, then add the appropriate quantity of each nutrient, mix the solution, and then things are good to go.  To that end, design wise, I was initially thinking peristaltic pumps, but I'm considering the possibility of using a valve based system with a measuring system.  The reason being that such a system should in theory, require less power than the peristaltic pumps.  I plan on purchasing both a peristaltic pump and a valve so that I can prototype that out at the end of the month.  I unfortunately have a work deadline that is likely going to consume the bulk of my weekends until the end of the month.

 

Has anyone used other brands of hydroponic nutrients, and if so, would you care to share your experiences?

  • Sign in to reply

Top Comments

  • sftwrngnr
    sftwrngnr over 11 years ago in reply to D_Hersey +1
    Wow Don! Thank you so much for your response and valuable information! OK then. Aeration system for the nutrients will be included in my build. So... I thought I may have been on the right track in terms…
Parents
  • D_Hersey
    D_Hersey over 11 years ago

    Most won't touch it because it is salty and it smells but I won't do without fish emulsion, because it is efficacious and cheap and I use systems that rinse well.  If I were to use chemical fertilizer I would use bulk NPK mixed with micronutrient salts inclucing Mo.  Mo is the only element in the micronutrient salt mix that is any expensive, therefore, usually, if it has molybdenum, you got the good stuff.  All as un-relabelled  commodity chemicals.

     

    The magic of nutrient uptake in green plants is due to complex mechanisms within the plant and between mycorrhizal allies and the roots.  A free ion is just that to this system, the plant doesn't know/care where it came from.  This system is tolerant and self-adjusting.

     

    Aerating the soln is important.  Good for the plant, bad for its enemies.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • D_Hersey
    D_Hersey over 11 years ago

    Most won't touch it because it is salty and it smells but I won't do without fish emulsion, because it is efficacious and cheap and I use systems that rinse well.  If I were to use chemical fertilizer I would use bulk NPK mixed with micronutrient salts inclucing Mo.  Mo is the only element in the micronutrient salt mix that is any expensive, therefore, usually, if it has molybdenum, you got the good stuff.  All as un-relabelled  commodity chemicals.

     

    The magic of nutrient uptake in green plants is due to complex mechanisms within the plant and between mycorrhizal allies and the roots.  A free ion is just that to this system, the plant doesn't know/care where it came from.  This system is tolerant and self-adjusting.

     

    Aerating the soln is important.  Good for the plant, bad for its enemies.