• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Nutrients, nutrients everywhere
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
  • Author Author: sftwrngnr
  • Date Created: 7 Aug 2015 7:43 AM Date Created
  • Views 837 views
  • Likes 1 like
  • Comments 5 comments
  • ambient_growth
Related
Recommended

Nutrients, nutrients everywhere

sftwrngnr
sftwrngnr
7 Aug 2015

So I've noticed that several of the challengers already have experience with hydroponics, aquaponics and aeroponics. I... do not. So, I've done some due diligence, and decided that I'm going to go with General Hydroponics "Flora Series" of hydroponic nutrients.  The obvious issue, is that it's a three part solution, so my system will need to measure PH/TDS prior to anything being added, then add the appropriate quantity of each nutrient, mix the solution, and then things are good to go.  To that end, design wise, I was initially thinking peristaltic pumps, but I'm considering the possibility of using a valve based system with a measuring system.  The reason being that such a system should in theory, require less power than the peristaltic pumps.  I plan on purchasing both a peristaltic pump and a valve so that I can prototype that out at the end of the month.  I unfortunately have a work deadline that is likely going to consume the bulk of my weekends until the end of the month.

 

Has anyone used other brands of hydroponic nutrients, and if so, would you care to share your experiences?

  • Sign in to reply

Top Comments

  • sftwrngnr
    sftwrngnr over 11 years ago in reply to D_Hersey +1
    Wow Don! Thank you so much for your response and valuable information! OK then. Aeration system for the nutrients will be included in my build. So... I thought I may have been on the right track in terms…
Parents
  • D_Hersey
    D_Hersey over 11 years ago

    I don't use any of that crap.  The reason I don't is because I am far too cheap to allow myself to be ripped off by the fertilizer racket.  I have a panoply of valid ancillary (buffering, for one) reasons, however.

     

    Peristaltic pumps require the user to move the pump down the tube occasionally as the tube looses its tendency to recover after awhile.  I find this unacceptable from an engineering standpoint.  Most other pump types cannot tolerate undissolved solids, this is unacceptable from a botany standpoint.

     

    I am not growing anything currently except out in the garden, there mostly wildflowers these days, I'm lazy.  If I were to try to use higher tech to grow green stuff, I would periodically lift a pot of aerated soln into my plants, which would be growing in mesh baskets upon clay pellets.  This system practically cannot clog.  With it, I can use compost tea as my nutrient.  I haven't done formal studies myself, but am convinced to a point of near existential certainty that compost tea is better for plants than mineral salts.  So much so that the analogy I commonly draw is between eating food versus eating food supplements solely.

     

    Plus, it costs a little better than free, as one ought to be composting anyway.

     

    Any system you use must be cyclically run with clear water.  This suppresses microbial growth.  It also is an anodyne for calcium build-up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • D_Hersey
    D_Hersey over 11 years ago

    I don't use any of that crap.  The reason I don't is because I am far too cheap to allow myself to be ripped off by the fertilizer racket.  I have a panoply of valid ancillary (buffering, for one) reasons, however.

     

    Peristaltic pumps require the user to move the pump down the tube occasionally as the tube looses its tendency to recover after awhile.  I find this unacceptable from an engineering standpoint.  Most other pump types cannot tolerate undissolved solids, this is unacceptable from a botany standpoint.

     

    I am not growing anything currently except out in the garden, there mostly wildflowers these days, I'm lazy.  If I were to try to use higher tech to grow green stuff, I would periodically lift a pot of aerated soln into my plants, which would be growing in mesh baskets upon clay pellets.  This system practically cannot clog.  With it, I can use compost tea as my nutrient.  I haven't done formal studies myself, but am convinced to a point of near existential certainty that compost tea is better for plants than mineral salts.  So much so that the analogy I commonly draw is between eating food versus eating food supplements solely.

     

    Plus, it costs a little better than free, as one ought to be composting anyway.

     

    Any system you use must be cyclically run with clear water.  This suppresses microbial growth.  It also is an anodyne for calcium build-up.