Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Overview of the project and work
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
  • Author Author: ochikov
  • Date Created: 10 Sep 2015 8:54 PM Date Created
  • Views 1381 views
  • Likes 5 likes
  • Comments 15 comments
Related
Recommended

Overview of the project and work

ochikov
ochikov
10 Sep 2015

Hello Everybody,

 

I will post my overview of the project. I managed to do a lot of work that is described there. I still wait RF modules and Ethernet Shield. Since then I managed to connect all the sensors to one Arduino Uno and start making tests with monitoring. As I receive the other stuff that I have purchased, i will start making tests with controlling the feeding system. I still have problems with calibration of Rain Sensor. But soon I will have success. Bellows are pictures:

 

This is the solution overview. As soon as I managed to understand and learn the kit's that we have, I will change the arduinos and use the kits to send/receive data and controlling the system.image

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Arduino:

image

LCD Measurements:

image

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 10 years ago +1
    Sounds very nice. The introductory architecture design seems to me very promising and the first experiments sounds good. Wait to see the further progress. Enrico
  • RWReynolds
    RWReynolds over 10 years ago +1
    Looks good Ognyan. I like the infographic of the system overview. Lots of easy to read information. I have to ask, what are you using to read the sensor-puck? I purchased a Plugable brand BLE and couldn…
  • ochikov
    ochikov over 10 years ago in reply to RWReynolds +1
    Hello Rick, Thank you for the good work. Now I use the Android app to read from Sensor-Puck. I try through the EFM32 ZERO GECKO Platform to program the Sensor-Puck, but with no success. Bellow is a picture…
Parents
  • balearicdynamics
    balearicdynamics over 10 years ago

    Sounds very nice. The introductory architecture design seems to me very promising and the first experiments sounds good. Wait to see the further progress.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 10 years ago

    Sounds very nice. The introductory architecture design seems to me very promising and the first experiments sounds good. Wait to see the further progress.

     

    Enrico