Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Project: ferris farm post 8
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
  • Author Author: shanesissons
  • Date Created: 14 Aug 2015 5:05 PM Date Created
  • Views 706 views
  • Likes 2 likes
  • Comments 5 comments
  • mechanical_farm
Related
Recommended

Project: ferris farm post 8

shanesissons
shanesissons
14 Aug 2015

Today is going to be an update on what i have been doing over the past 5 days


firstly i have been looking at the kit and what parts i am going to use for each task

The sensor puck

I will use this for realtime testing while programming the board


The wireless boards

I am hoping to use the boards to control all of the electronics i will have one board connected inside the unit and the second board either ontop of the unit or in a second unit that would sit on my desk or anywhere in the house that will have LEDs to tell me what the unit is doing (red yellow green LEDs for knowing if it is to high to low or just right for each sensor


The Zero gecko board

currently i am yet to implement this into my design it is possible that this board will be used as my motor controller keeping the unit turning at a set speed or at intervals


Motors

my plan now is to use a small geared stepper motor if on doesnt have enough power to turn the unit i have 4 more that i will add untill i have the required power but the low friction of the design should mean that one will be sufficient


Water & food

My water supply will be located in a small fishtank (because i had an empty tank that needed a use) that happens to be just about the right size with a small modification i will have 2 pumps located in the water and possibly a aerator pump aswell


secondly i have been working on the unit its self

the outside walls are nailed and glued into place

the rotisserie has been aligned and also glued

the planters have been water sealed from both ends

4 legs have been added to increase the height of the design for easier use and also so that any leaks can be observed if the occur


i should have parts ordered within the next week or so and then i can get on with finalising the build


sorry about no images today i havnt had time to compress my camera photos as they are to large for the site to allow but i will make it up with a video in the near future


Shane


 


  • Sign in to reply

Top Comments

  • shanesissons
    shanesissons over 11 years ago in reply to RWReynolds +1
    sounds like our base is quite similar just different rotations im going to be using skateboard bearings to hold the system in place and i believe im using the same stepper motor as you but i might need…
  • shanesissons
    shanesissons over 11 years ago in reply to RWReynolds +1
    I have heard of them also windows 10 has a built in 3d printing service but it's about pricy and uses a 3rd part website Yes it's a real thing but not just one we have poundland,pound world, 99p store…
  • RWReynolds
    RWReynolds over 11 years ago in reply to shanesissons +1
    LOL!! 99p Store. Sorry, that makes me chuckle. We have The Dollar Store and Dollar General where I am. Same thing, some good stuf and some rubbish. I live in South Mississippi, down on the Gulf Coast.…
Parents
  • RWReynolds
    RWReynolds over 11 years ago

    Sounds like you're making solid progress Shane.

     

    I am missing two parts needed to finish my rotator system. Hopefully, they will arrive today.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shanesissons
    shanesissons over 11 years ago in reply to RWReynolds

    sounds like our base is quite similar just different rotations

    im going to be using skateboard bearings to hold the system in place and i believe im using the same stepper motor as you but i might need to use a couple of them and then adapt a rubber rc wheel to the shaft to give me the friction to turn the system as i will be rotating it from the outside edge of the donut (circle with cutout sidewall of the planter this is where a 3d printer would be very handy but its surprising what you can find at the pound store/ dollar store that can be adapted to use instead

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to shanesissons

    Yes, sounds similar. Just different axis of rotation.

     

    Hey, check our ShapeWays.com. They do one off 3D printing that's fairly reasonable. I'm going to use them for my sprinkler head.

     

    Pound Store. lol... Is that a real thing?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shanesissons
    shanesissons over 11 years ago in reply to RWReynolds

    I have heard of them also windows 10 has a built in 3d printing service but it's about pricy and uses a 3rd part website

     

    Yes it's a real thing but not just one we have poundland,pound world, 99p store and many other none branded stores they basically get stuff that is mass produced and breaks after 5 minutes but they have also of good buys I use there superglue alot something like 20 tubes for 1 pound

     

    On a fun note they sell pregnancy tests in packs of 2 also for 1 pound ( where I live apparently has the highest teenage pregnancy rate in Europe) 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to shanesissons

    LOL!! 99p Store. Sorry, that makes me chuckle. We have The Dollar Store and Dollar General where I am. Same thing, some good stuf and some rubbish.

     

    I live in South Mississippi, down on the Gulf Coast. And we have several claims to fame as well. We are the fatest region in the fatest state in the fatest country in the world. Yep, we got some large folks around here. And my particualr area is one of the least educated and with a pretty high teen pregnanyc rate as well. So, we have that going for us.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • RWReynolds
    RWReynolds over 11 years ago in reply to shanesissons

    LOL!! 99p Store. Sorry, that makes me chuckle. We have The Dollar Store and Dollar General where I am. Same thing, some good stuf and some rubbish.

     

    I live in South Mississippi, down on the Gulf Coast. And we have several claims to fame as well. We are the fatest region in the fatest state in the fatest country in the world. Yep, we got some large folks around here. And my particualr area is one of the least educated and with a pretty high teen pregnanyc rate as well. So, we have that going for us.