• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Project: ferris farm post 9
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
  • Author Author: shanesissons
  • Date Created: 21 Aug 2015 1:52 AM Date Created
  • Views 994 views
  • Likes 1 like
  • Comments 6 comments
  • mechanical_farm
Related
Recommended

Project: ferris farm post 9

shanesissons
shanesissons
21 Aug 2015








{gallery} post 9

image

image

image

image

image

image

image

image

image

image

image

image

image

image

Parts have started to arrive !!

 

I have now started a dry run building the design so far i have

installed the PSU

installed the fans

1st coat of varnish on the wood

nailed and glued the sides and back

installed the legs

test fit the mounts for the dev boards

soldering and crimping wires and connectors

sizing up where the parts that have not arrived will go

 

PSU

 

the power for this unit will come from a pc power supply that has been adapted

i will be using the 3.3,5 and 12v lines from the PSU

 

Fans

 

I went with 2 5v fans that were repurposed from an old laptop cooling stand

in front of the fans are 3 layers of mesh this is to stop insects from entering the unit and also to restrict air flow to a lower amount

 

Varnish

 

After a long discussion with myself i decided to go with a varnish on the unit instead of a paint to keep the look of the OSB

the top of the unit also has a stain on as well this was a test to see what looked the best and decided just to keep the top stained

 

Board mount

 

i have used 3 pcb spacers to mount the board on a scrap piece of wood to test the idea and it worked out really well and this is how i will be mounting the board inside the unit

 

Cables

 

I have started to solder the connectors onto the cables ready for the boards to arrive that way i can solder them straight onto the boards and save some time as well

 

Lighting

 

for the lighting i am testing out using red green and blue LEDs i will be usign a total of 60 LEDs 20 of each colour i will have these mounted but connect them up so many at a time to get the best amount of light

 

still to be updated when parts arrive

rotation

moisture sensor and my crazy way of connecting them to the board through 2 axis of rotation

watering system

lighting

silver lining (mylar)

  • Sign in to reply

Top Comments

  • shanesissons
    shanesissons over 11 years ago in reply to balearicdynamics +1
    The legs of the unit are from a bed frame they are bolted through the wood and are very sturdy basically they are now one with the unit They will withstand alot of weight approx 10 stone per leg so I'm…
Parents
  • balearicdynamics
    balearicdynamics over 11 years ago

    Nice presentation. We already saw the scheme design and now there is a clear perception of what the size will be image

     

    Just a suggestion: the legs of the structure, as shown in the images maybe the weak point. A minimal horizontal oscillation can break one of them when there will be the water solution, plants and all the stuff installed. Why did you put them so long?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shanesissons
    shanesissons over 11 years ago in reply to balearicdynamics

    The legs of the unit are from a bed frame they are bolted through the wood and are very sturdy basically they are now one with the unit

     

    They will withstand alot of weight approx 10 stone per leg so I'm not worrying about the strength

     

    Reason for the size was firstly that's all I had and I wanted the unit off the ground and also I wasn't sure if my water tank would be inside or below so I accounted for both options and also it is now a similar size to a kitchen appliance so could even be used under the counter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shanesissons
    shanesissons over 11 years ago in reply to balearicdynamics

    The legs of the unit are from a bed frame they are bolted through the wood and are very sturdy basically they are now one with the unit

     

    They will withstand alot of weight approx 10 stone per leg so I'm not worrying about the strength

     

    Reason for the size was firstly that's all I had and I wanted the unit off the ground and also I wasn't sure if my water tank would be inside or below so I accounted for both options and also it is now a similar size to a kitchen appliance so could even be used under the counter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to shanesissons

    Clear ! Anyway, I suggest you don't try to make BBQ with this material image

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shanesissons
    shanesissons over 11 years ago in reply to balearicdynamics

    Funny you should say that I have actually used this material to repair my gas bbq's stands on either side

     

    Got an ancient bbq that needed some tlc