Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Stacked Container Hydroponics for Vertical Farming : Blog 7 - SCADA System Update
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
  • Author Author: RWReynolds
  • Date Created: 30 Sep 2015 2:25 AM Date Created
  • Views 1038 views
  • Likes 3 likes
  • Comments 2 comments
  • modular_hydroponics
Related
Recommended

Stacked Container Hydroponics for Vertical Farming : Blog 7 - SCADA System Update

RWReynolds
RWReynolds
30 Sep 2015

OK, so I received the EZR32WG starter kit last Friday. Thanks to element14Dave! image

 

This is not much of a blog post, but it's intended only as an update and the result of having recieved the EZR32WG starter kit last Firday.

 

I spent the weekend installing one of the EZR32WG MCUs and an RPi in an enclosure. This will be the cultivation area SCADA system.

 

The EZR32WG MCU will now replace the EFM32ZG MCU. I'm currently busy making a wiring harness for the enclosure and the code originally written for the EFM32ZG has been ported to the new MCU and is fully operational. Next, I'll write the communications code for the EZR32WG MCUs.

 

Please see the enclosure in the figures below. (Please excuse the mess. lol...)

image

Controller and power supply powered up and logging data.

 

image

Controller face with EZR32WG antenna installed.

 

image

Closeup of enclosure with EZR32WG, RPi and stepper motor controller installed, wired up and powered up. You can see here that the EZR32WG is actually being powered from an RPi USB port, although the RPi is a little difficult to see. The RPi is being powered through the GPIO header from a salvaged desktop PC power supply.

 

 

And here's another example of data being captured right now.

 

https://www.initialstate.com/app#/tiles/a9144f1f-a3b3-498e-9951-a523000c4154

 

More to come soon. I have the cultivator unit completely assembled and setup. This weekend I should have all the code completed and the entire system up and running.

 

Good luck to all the VF challengers, and happy vertical farming! image

 

Cheers,

Rick

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Looking good an neat. Hopefully you won't run into any EM interference with your combined cables. DAB
Parents
  • DAB
    DAB over 10 years ago

    Looking good an neat.

     

    Hopefully you won't run into any EM interference with your combined cables.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 10 years ago in reply to DAB

    Thanks DAB,

     

    No EMI issues so far. It's all running very smoothly. But I have considered it and it's the first thing I'll look for if I start getting any intermittent issues.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • RWReynolds
    RWReynolds over 10 years ago in reply to DAB

    Thanks DAB,

     

    No EMI issues so far. It's all running very smoothly. But I have considered it and it's the first thing I'll look for if I start getting any intermittent issues.