Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Start playing with the kits to build monitoring system
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
  • Author Author: ochikov
  • Date Created: 5 Sep 2015 10:18 AM Date Created
  • Views 1064 views
  • Likes 3 likes
  • Comments 11 comments
Related
Recommended

Start playing with the kits to build monitoring system

ochikov
ochikov
5 Sep 2015

Hello everybody,

Today I managed to start playing with all the stuff that I receive. My goal is now to start building the monitoring system. I suddenly found that some stuff is missing from my package and also in the invoice documents that I receive. Does anybody knows when we will receive:

 

  • Wurth capacitor kit (885 060)
  • Wurth switch kit (499 001)

 

Thanks.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to m.ratcliffe +2
    I've been asking around about this as well because I think it is pretty silly that I don't have the EZR32 microcontroller, since i'm required to use it. I also can't get simplicity studios to work....…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to RWReynolds +2
    Well, I am using a PC, but the Simplicity Studio does not recognize my EFM32 as being connected... Have yet to test with different computers, so I am just working on some arduino water based stuff right…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to RWReynolds +2
    I've tried reinstalling and exiting a bunch of times, but my computer anti-virus software sometiems says that SS contains a safety hazard, do you think I should just accept? Still can't get it to recognize…
Parents
  • m.ratcliffe
    m.ratcliffe over 11 years ago

    No one got the switch kit [Problem at the source, see Element14Dave's Second video about seeds] but I do have the capacitor kit.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to m.ratcliffe

    I've been asking around about this as well because I think it is pretty silly that I don't have the EZR32 microcontroller, since i'm required to use it. I also can't get simplicity studios to work.... going to try a different computer.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to e14 Contributor

    Maybe it is customs related that is causing your delay. I got the simplicity studio to work on a linux desktop [mint 17].

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to e14 Contributor

    What issues are you getting with SimplicityStudio Joshua? I amight be able to help, and SiLabs support has been very responsive to support tickets for me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to RWReynolds

    Well, I am using a PC, but the Simplicity Studio does not recognize my EFM32 as being connected... Have yet to test with different computers, so I am just working on some arduino water based stuff right now.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    The laptop which I am trying to run it on though is really crappy and I really junked it up, so maybe that's the reason....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to e14 Contributor

    I know a couple fo folks had issues with their machines not recognizing the MCU at frist. I think most everyone just removed and reinstalled SimplicityStudio to fix it.

     

    I had one issue where it was working fine and then quit recignizing the MCU. It had to do with trying to access the sensor-puck and changing the debug from MCU to OUT, I think that's right. But I eventually got it corrected.

     

    Cheers,

    Rick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • RWReynolds
    RWReynolds over 11 years ago in reply to e14 Contributor

    I know a couple fo folks had issues with their machines not recognizing the MCU at frist. I think most everyone just removed and reinstalled SimplicityStudio to fix it.

     

    I had one issue where it was working fine and then quit recignizing the MCU. It had to do with trying to access the sensor-puck and changing the debug from MCU to OUT, I think that's right. But I eventually got it corrected.

     

    Cheers,

    Rick

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to RWReynolds

    I've tried reinstalling and exiting a bunch of times, but my computer anti-virus software sometiems says that SS contains a safety hazard, do you think I should just accept? Still can't get it to recognize... But the computer lists the j-link on its USBs. Maybe it's because I did not install drivers correctly. Any suggestions?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to e14 Contributor

    Hmmmm....

     

    You are on a Windows machine, correct?

     

    Have you updated to Windows 10?

    Are you using only Windows Defender?

    Firewall on?

    Are you connected to the Internet while installing SS?

     

    It could be that some driver(s) or other required software is not being downloaded during install.

     

    I have SS running on both an Ubuntu 14.04 and Windows 10 VMs. I haven't had any issues except the one I described. And I caused that one.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to RWReynolds

    Well I have a mac book air runnin g OS X Yosemite and a Windows running widows 7 or 8....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to e14 Contributor

    I think Win 7 or 8 should be fine.

     

    One thing I've found that seems to make a difference is the order in which you run software and attach the device. Make sure that Simplicity studio is up and running and then connect the MCU. You should see a file open that lists several .html files. The switch back to SS. It may take a minute or so for the software to recognize the device. If the USB bus is seeing the J-Link debugger the software should detect the device and connect.