Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog The Plant Blog 6: Worst Case Scenario Fix
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
  • Author Author: e14 Contributor
  • Date Created: 25 Sep 2015 5:12 AM Date Created
  • Views 1031 views
  • Likes 1 like
  • Comments 2 comments
  • design_challenge
  • vertical_farming
  • challenge
  • farming
  • aquaponics
  • the_plant
Related
Recommended

The Plant Blog 6: Worst Case Scenario Fix

e14 Contributor
e14 Contributor
25 Sep 2015

Now we are moving along. I recently received all my aquaponics equipment like the Hydroton, new pump, electrical equipment etc. and have been able to continuously add to the Mini Plant 2. As I was adding more equipment to the system, I had to add in more water as well. The problem with this is that I live in an apartment, and if something goes wrong (aka overflow of water to my apartment (I live upstairs, too), I will have a lot to worry about. The solution to this anxiety-causing problem will be an automated overflow system.

We will be making our automated overflow system (AOS) run from the Raspberry Pi of course (UPS problems have denied us our kit still). The AOS will be based on a "Control Power Outlets Using Raspberry Pi" project we found online. Here is the link to that amazing tutorial if any of you want to use this as well:


https://www.samkear.com/hardware/control-power-outlets-wirelessly-raspberry-pi.


We have the material ready, and we are in the process of implementing it into our system. The only part left to do is to include the overflow switch: the switch that will turn off the pump if it detects an overflow occurring.

 

The overflow switch will be a simple open ended wiring that will complete the circuit when the two exposed conductors are submerged. The exposed conductors will be a screw of some sort. I am not sure if they sell copper screws, and if they don't I will get some copper tape and place it somewhere in the tank.

 

So far this is still in the works so if any of you have any questions or comments please let me know.

 

Quick update on everything else:
Our seeds are ready to be transferred over to a seedling tray, so I will be doing that tomorrow. This is my first time growing a plant from seed so much help would be appreciated. Here they are in my sandwich bags:
First Picture of the Seeds
The software is ready for temperature and pH. The lighting code is being completed as I type this. As soon as the lighting code is done, I will add the lights and the grow bed into the system. Tomorrow, I also plan on keeping the script running all day long as well to begin collecting data for us to play with.

This week is definitely looking busy for me, but not necessarily productive. Here's to a very productive week for all of us.

  • Sign in to reply
Parents
  • DAB
    DAB over 10 years ago

    Looks like a good start.

     

    Yes it always pays to take precautions with possible fluid leaks.

    It helps keep the neighbors happy if you don't drip fluids through their ceilings and onto their furniture.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 10 years ago

    Looks like a good start.

     

    Yes it always pays to take precautions with possible fluid leaks.

    It helps keep the neighbors happy if you don't drip fluids through their ceilings and onto their furniture.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to DAB

    Hey DAB,

     

    I haven't mentioned this in any of my blogs, but my last system had the pump's tube to the growbed detach itself from the fitting (the fitting was cracked). When the tube detached, it fell to the second level smaller container, where it overflowed. Luckily, my housemate came back to catch any more of the water from falling out, but we had a soaked kitchen floor. Just don't want that happening again. =)

     

    Besides that, experience has shown me always to have an emergency shutoff button for all my projects.

     

    Erik