Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Vertical Hydroponics: Blog 6 - EZR32WG Wireless Starter Kit: Part 1
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
  • Author Author: jamesod
  • Date Created: 28 Sep 2015 11:34 PM Date Created
  • Views 1744 views
  • Likes 2 likes
  • Comments 10 comments
  • vertical_hydroponics
  • vertical_farming
  • ezr32wg
  • wireless
Related
Recommended

Vertical Hydroponics: Blog 6 - EZR32WG Wireless Starter Kit: Part 1

jamesod
jamesod
28 Sep 2015

I have gotten a lot done since my last post, but I don't have time to write a detailed blog at the moment. I did want to give an update on my first chance to get started with what will be the controller for this project. More to come shortly.

 

This Friday I received the EZR32WG 915 MHz Wireless Starter Kit. Most of my time this weekend has revolved around getting to know the hardware and software that comes with this dev kit, and so far I am pretty impressed.

 

I began by installing Simplicity Studio. This was a fairly painless process. Then I started up the studio and connected one of the boards to my computer. After a few minor bumps, the board showed up in the Detected Hardware section. I moved the switch on the board to the AEM position, and went to the Kit Manager. There I updated the board firmware to the latest version. This gave me the “EZR32WG 915MHz Wireless Starter Kit (###)” as the detected Hardware instead of just “J-link Debugger.”


Next, I went to the software examples section. The appropriate Kit, Part, and SDK was automatically selected for me. I wanted to try out a program that would let me use the on-board display and push buttons first so I chose the SLWSTK6222A_clock program. I loaded this program into the IDE, and used the debug command to load it onto the board. It worked! I played with this to see how the buttons worked, and observed which libraries were used.

 

After this I tried out the ezradio_simple_trx example program. I loaded this onto both boards. When I pushed an button on one, the other received a number. This is a very simple example, but it shows how to implement bidirectional communication on these boards.

 

The last example program I looked at was SLWSTK6222A_humitemp. This program reads from the on board i2c temperature and humidity sensor and displays the data on the on board screen.

 

After looking through these examples I decided I had enough to hack together my first program on the board. I began with the ezradio_simple_trx program and added code from the humitemp program so that one board “Node1” sent the temperature to the other board “Gateway.” With this working successfully I now have a method for sending whatever data I want from the node to the Gateway.

 

With this working I can move on to getting data from the Gateway to the Beagle Bone Black Webserver. The I will write code to interface with all of the sensors and relays I am using, wire up the system in an enclosure, and start to write the main control code.

  • Sign in to reply

Top Comments

  • RWReynolds
    RWReynolds over 10 years ago +1
    Cool stuff James. Sounds like you've been busy. I also received the EZR32WG on Friday. Thanks element14Dave ! I've run the ezradio_simple_trx and a couple of other example applications. Works great. Busy…
  • jamesod
    jamesod over 10 years ago in reply to RWReynolds +1
    Are you having your system communicate with an external network? If so have you decided on a method yet? I've got communications between the radios working just fine, but I'm not sure how I'm going to…
  • RWReynolds
    RWReynolds over 10 years ago in reply to jamesod +1
    I'm doing the same on a Raspberry Pi James. Could have used a BBB, I have both available, but I've been playing with the RPi lately. lol... I actually have an RPi on both ends. On the cultivator end simply…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi James O'Donnell,

     

    I am trying to do the same with two EZR32. I get the temperature in one module and I want to send it to the other one.

     

    I began with the ezradio_simple_trx program too and added code from the humitemp program. I can read the temperature perfectly into the board "Node1" (like a char for example and print into the screen), however, to send it I have to convert int32_t (temData variable) to uint8_t (radioTxPkt, argument of ezradioStartTransmitDefault() function). I have tried several options but I don't know how to convert it. I am almost rookie so maybe I am really wrong. Could you please help me?

     

    Cheers

    Tini

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi James O'Donnell,

     

    I am trying to do the same with two EZR32. I get the temperature in one module and I want to send it to the other one.

     

    I began with the ezradio_simple_trx program too and added code from the humitemp program. I can read the temperature perfectly into the board "Node1" (like a char for example and print into the screen), however, to send it I have to convert int32_t (temData variable) to uint8_t (radioTxPkt, argument of ezradioStartTransmitDefault() function). I have tried several options but I don't know how to convert it. I am almost rookie so maybe I am really wrong. Could you please help me?

     

    Cheers

    Tini