Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Forum Question concerning the design challenge kit...
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 4 subscribers
  • Views 1612 views
  • Users 0 members are here
Related

Question concerning the design challenge kit...

RWReynolds
RWReynolds over 11 years ago

I have a question concerning the kit provided for this challenge.

 

On the kit description page, Vertical Farming Design Challenge - Kit List,  it lists two separate SL microcontroller devices.

The EFM32Tm Zero Gecko Starter Kit and the EZR32 Wonder Gecko Starter Kit.

However in the unboxing video, https://youtu.be/rPN4RmauEvE, David Finch references only the EZR32 Wonder Gecko Starter Kit.

And even though the box appears to contain two complete units he says the kit includes 1 each.

I'm assuming he means 1 each kit, and not unit, as he goes on to explain the mission critical nature of the comm link.

But he never mentions or shows the EFM32Tm Zero Gecko Starter Kit at all.

 

Just looking for clarification on what's included so I can move forward with design while waiting on delivery.

 

Thanks,

Rick Reynolds

  • Sign in to reply
  • Cancel

Top Replies

  • element14Dave
    element14Dave over 11 years ago in reply to shabaz +3 suggested
    Hi shabaz , actually the EFM32 Zero Gecko Starter Kit is included in the overall kit. It was a late entry into the materials supplied by Silicon Labs (after we shot the video) There terms and conditions…
  • RWReynolds
    RWReynolds over 11 years ago in reply to element14Dave +2
    Cool... So that's two BRD4001 motherboards, two EZR32 Wonder Geko radio/MCU boards and a separate EFM32 Zero Geko low power MCU. Plus pieces and parts. That's a lot to work with. Thanks for clearing that…
  • shabaz
    shabaz over 11 years ago in reply to element14Dave +1
    Hi Dave, Oh I see. Thanks for the clarification!
Parents
  • shabaz
    0 shabaz over 11 years ago

    Hi Rick,

     

    The EZR32 Wonder Gecko Starter Kit contains two base boards and two microcontroller/radio boards, see the EZR32 Wonder Gecko Starter Kit Silicon Labs page for more information. It assembles

    into two units, each unit being a base board and the microcontroller/radio board. As you say, this can then be used for communication between the two units. One kit containing the two units is supplied

    for the challenge.

    The EFM32 Zero Gecko Starter Kit is not part of the supplied materials for the challenge, I think that was a mistake on the page you mention, element14Dave can hopefully clarify.

     

    EDIT: My mistake, clarified by Dave below that it does include the EFM32 Zero Gecko Starter Kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 11 years ago

    Hi Rick,

     

    The EZR32 Wonder Gecko Starter Kit contains two base boards and two microcontroller/radio boards, see the EZR32 Wonder Gecko Starter Kit Silicon Labs page for more information. It assembles

    into two units, each unit being a base board and the microcontroller/radio board. As you say, this can then be used for communication between the two units. One kit containing the two units is supplied

    for the challenge.

    The EFM32 Zero Gecko Starter Kit is not part of the supplied materials for the challenge, I think that was a mistake on the page you mention, element14Dave can hopefully clarify.

     

    EDIT: My mistake, clarified by Dave below that it does include the EFM32 Zero Gecko Starter Kit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • RWReynolds
    0 RWReynolds over 11 years ago in reply to shabaz

    That's what I'm thinking as well Shabaz.

    Thanks for the quick reply!

     

    Dave, any further info on this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • element14Dave
    0 element14Dave over 11 years ago in reply to shabaz

    Hi shabaz, actually the EFM32 Zero Gecko Starter Kit is included in the overall kit. It was a late entry into the materials supplied by Silicon Labs (after we shot the video)

     

    There terms and conditions are up to date with the contents of the kit.

     

    Dave

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • RWReynolds
    0 RWReynolds over 11 years ago in reply to element14Dave

    Cool...

     

    So that's two BRD4001 motherboards, two EZR32 Wonder Geko radio/MCU boards and a separate EFM32 Zero Geko low power MCU. Plus pieces and parts. That's a lot to work with.

     

    Thanks for clearing that up Dave.

     

     

    A couple of other questions...

     

    I am considering adding an RPi to the system for greater control and easier IoT connectivity. Is it acceptable to use additional devices, in addition to the kit parts?

     

    IMPORTANT: Also will the US competitors receive the  SLWSTK6222ASLWSTK6222A 915MHz version of the EZ32 starter kit I found a blurb in the terms and conditions suggesting that we should specify in our applications if we needed other than the 868MHz version I'm not sure I did that but would like to make that request now As I believe the US assigns the 902MHz to 928MHz bands for sub gigahertz 802.15.4 use

     

    Thanks,

    RWReynolds

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 11 years ago in reply to element14Dave

    Hi Dave,

     

    Oh I see. Thanks for the clarification!