Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Forum windows 10 and silicon labs dev boards
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 25 replies
  • Answers 2 answers
  • Subscribers 6 subscribers
  • Views 5796 views
  • Users 0 members are here
Related

windows 10 and silicon labs dev boards

shanesissons
shanesissons over 11 years ago

im having issues connecting the dev boards to my pc I have recently upgraded to windows 10 (not the best idea in the middle of a project) has anybody else encountered this issue or have any suggestions?

 

on a side note im getting quite good at space invaders

  • Sign in to reply
  • Cancel

Top Replies

  • shanesissons
    shanesissons over 11 years ago in reply to clem57 +1
    no error messages windows makes sound to acknowledge usb item inserted then in simplicity I refresh detected hardware and says no hardware found not getting any errors just nothing when connected for any…
  • shanesissons
    shanesissons over 11 years ago in reply to RWReynolds +1
    thanks rick didn't see your message there if it doesn't work for you then I know its an issue with windows if it does work for you then I think I will get Linux running on another pc I have that has been…
  • shanesissons
    shanesissons over 11 years ago in reply to RWReynolds +1
    yea i have the wireless kit aswell it came with the rest of the kit might have been as i had the 868mhz (800 and something) kit
Parents
  • clem57
    0 clem57 over 11 years ago

    Can you tell messages and what leads up to issues?

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shanesissons
    0 shanesissons over 11 years ago in reply to clem57

    no error messages windows makes sound to acknowledge usb item inserted then in simplicity I refresh detected hardware and says no hardware found not getting any errors just nothing when connected for any of the 3 boards so im going to rule out a faulty board

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to shanesissons

    Another forum says you may need a separate driver for windows 10 http://community.silabs.com/t5/Interface/CP210x-USB-to-UART-Bridge-driver-for-Windows-10/td-p/146192

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shanesissons
    0 shanesissons over 11 years ago in reply to clem57

    yea says on that one that the drivers didn't work for windows 10 think I might just have to salvage a pc or laptop to make things easier

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to shanesissons

    Windows 10 although out in the wild is not really a production ready OS, even if M$ claims so. image

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shanesissons
    0 shanesissons over 11 years ago in reply to clem57

    yea I have noticed is has a few bugs still but I had to get away from windows 8 it was killing meimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shanesissons
    0 shanesissons over 11 years ago in reply to RWReynolds

    thanks rick didn't see your message there if it doesn't work for you then I know its an issue with windows if it does work for you then I think I will get Linux running on another pc I have that has been sat in a corner for a long time because I couldn't get an os to install but might have to try again

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWReynolds
    0 RWReynolds over 11 years ago in reply to shanesissons

    No problem...

    Ok, I am installing SS now with the EFM32ZG connected and it found it. But it's still in the middle of the install. I think it's going to take a bit. It may be hung up, seems like that happened when I installed on Ubuntu as well. I may have to stop it and do the updates manualy. But it did detect the SI board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWReynolds
    0 RWReynolds over 11 years ago in reply to shanesissons

    Hey, do you already have the EZR32WG starter kit? I saw you mentioned 3 boards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shanesissons
    0 shanesissons over 11 years ago in reply to RWReynolds

    yea i have the wireless kit aswell it came with the rest of the kit might have been as i had the 868mhz (800 and something) kit

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWReynolds
    0 RWReynolds over 11 years ago in reply to shanesissons

    Right, I'm assuming you're in the UK.

     

    Simplicity is still loading on my Win10 VM. I'll let ya know what I find out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWReynolds
    0 RWReynolds over 11 years ago in reply to shanesissons

    Hey Shane...

     

    I installed SS on Win10 VMand it found the EFM32ZG board no problem. I compiled and flashed one of the example programs and it ran fine.

     

    You're not getting any error messages or anything? Just not finding the board?

     

    When you plug the baord into the computer, there should be two leds lit. A green one blinking, maybe a couple times a second, just behind and to the inside of the USB connector. There's also a blue LED next to the USB connector. When the board is not connected it blinks rapidly. Once it finds the board it will change to solid. Are you seeing these LEDs lit at all?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • RWReynolds
    0 RWReynolds over 11 years ago in reply to shanesissons

    Hey Shane...

     

    I installed SS on Win10 VMand it found the EFM32ZG board no problem. I compiled and flashed one of the example programs and it ran fine.

     

    You're not getting any error messages or anything? Just not finding the board?

     

    When you plug the baord into the computer, there should be two leds lit. A green one blinking, maybe a couple times a second, just behind and to the inside of the USB connector. There's also a blue LED next to the USB connector. When the board is not connected it blinks rapidly. Once it finds the board it will change to solid. Are you seeing these LEDs lit at all?