Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Documents Vertical Farming Design Challenge
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 29 May 2015 11:07 AM Date Created
  • Last Updated Last Updated: 15 Jun 2015 3:50 PM
  • Views 9244 views
  • Likes 11 likes
  • Comments 51 comments
Related
Recommended

Vertical Farming Design Challenge

image
Vertical Farming Design Challenge

image  All About Vertical Farming

image  Overview Video

image  Prizes

image  Terms and Conditions

image  Kit List

 

Background

 

From Wikipedia

According to current projections of population growth, the world population of humans will continue to grow until at least 2050, with the estimated population, based on current growth trends, to reach 9 billion in 2040,and some predictions putting the population in 2050 as high as 11 billion. World population passed the 7 billion mark on October 31, 2011.

 

From the World Wildlife Organization

Soil is the earth’s fragile skin that anchors all life on Earth. It is comprised of countless species that create a dynamic and complex ecosystem and is among the most precious resources to humans. Increased demand for agriculture commodities generates incentives to convert forests and grasslands to farm fields and pastures. The transition to agriculture from natural vegetation often cannot hold onto the soil and many of these plants, such as coffee, cotton, palm oil, soybean and wheat, can actually increase soil erosion beyond the soil’s ability to maintain itself.

Half of the topsoil on the planet has been lost in the last 150 years. In addition to erosion, soil quality is affected by other aspects of agriculture. These impacts include compaction, loss of soil structure, nutrient degradation, and soil salinity. These are very real and at times severe issues.

 

From VerticalFarm.com

By the year 2050, nearly 80% of the earth’s population will reside in urban centers. Applying the most conservative estimates to current demographic trends, the human population will increase by about 3 billion people during the interim. An estimated 109 hectares of new land (about 20% more land than is represented by the country of Brazil) will be needed to grow enough food to feed them, if traditional farming practices continue as they are practiced today. At present, throughout the world, over 80% of the land that is suitable for raising crops is in use (sources: FAO and NASA). Historically, some 15% of that has been laid waste by poor management practices. What can be done to avoid this impending disaster?”

 

The confluence of these observations and forecasts points to the need to increase our ability to grow fresh food in urban areas – closer to the populations that will consume them.  This means shifting from traditional outdoor gardens to indoor systems for food production.  Electronic Engineers are uniquely suited to provide systems based on a technology infrastructure that can lessen required energy consumption in production and improve the output of a smaller space.

 

Vertical Farming is a developing industry growing to meet these demands.  The main areas for measuring their success – and focus for improvement - are the production output per square foot, monitoring and lessening the energy and water consumption, and efficiencies around harvesting.

  

The Challenge

We will select 15 challengers from all entries received to build indoor, vertical farms that are true IoT solutions. The projects should include:

  • Environmental monitoring (light, temperature and humidity)
  • A watering and feeding system
  • A greater growing surface than just the overall footprint of the build
  • Energy monitoring to collect data on the overall consumption of power and water by the system


Help Along the Way

In addition to the great Kit that Challengers will receive, we also have support for those of you without a green thumb.  We’re going to be recommending the types of seeds to buy, the types of fertilizer and ranges to be aware of when you’re monitoring moisture, light and humidity.  We’ll announce a point in time about six weeks out when all Challengers should start their seedlings.  After a 7-10 day germination period, your seedlings should be transferred to your Vertical Farm.  Then after about a month of growing we’ll ask you to harvest your crop.  Submitting information about the overall weight of the harvest and the average height of the plants will help the Judges determine the best developed solutions.

And if your seedlings start looking sickly, then post a question on the Design Challenge site and someone from the Vertical Farming Association will give you tips and suggestions to help you nurse your plants back to life.

 

More details coming soon.

  • vertical
  • vertical_farming
  • Design
  • challenge
  • farming
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +3
    Questions are a good thing! They inspire thought and conversation. Never be sorry you asked a question, and never feel stupid for asking a question that is considered 'basic'. I ask basic questions all…
  • jkutzsch
    jkutzsch over 10 years ago in reply to shabaz +3
    I will definitely have to check those groups out, I went through last night and just started following a variety of interesting groups but was noticing a bunch have not been updated in years. :-) The specifics…
  • mcb1
    mcb1 over 11 years ago in reply to clem57 +2
    clem57 Clem Yes it did strike me that in very hot climates it could be an issue with water transvapouration putting them at a disadvantage. Even her in summer we lose 4-5mm per day, which many won't realise…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Is there a specific plant that must be used?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kellyhensen
    kellyhensen over 11 years ago in reply to e14 Contributor

    nightdrakon

    Yes, we will be circulating information about what type of plants to grow as a part of the challenge to level the playing field.  The selected challengers will have to procure their own seeds locally (turns out seeds are harder to ship internationally than electronic components).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to kellyhensen

    Also, am I right to assume that if our watering system were to run out of water, we can fill it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kellyhensen
    kellyhensen over 11 years ago in reply to e14 Contributor

    Of course!  However, it would be good to have a method for monitoring the amount of water used throughout as data such as that will be a part of judging the winners at the end of the competition.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to kellyhensen

    Do we have to measure the water used with a machine like a weight, or just remember and write down how much we put in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Joshua,

     

    If you choose to do this automatically then there are some interesting electronic methods which are possible too - e.g. optical methods, electrical conductivity, foam float with magnetic sensor, and so on. Another option would be to alert when the water level is dangerously (for the plants etc) low - i.e. just a high/low indication possibly, rather than a more granular measurement.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    The point of these competitions, at least in part, is to inspire creative thinking. There is no correct answer to your question, only suggestions. You are posting in an electrical engineering related forum so I would assume an electronic solution would earn you a higher score vs simply writing it down. However, that does not neccasarly mean you have to automate the process. Manual data collection through a creative electronic version of 'pen & paper', in theory, would net you a higher score. You can build a simple data collection device, manual inputs via PB or a num-pad. Store the data on an EEPROM and export to excel/ or vice versa. Write down your measurements in excel and send the variables to the ucontroller, you can write a control system that responds to the stimulus.

     

    Alternatively you can measure and record water level in realtime if you use the right tech. You have options, from simple --> complex.

    examples: ( I can elaborate if requested)

     

    Water is conductive, so if you use two nails; one @ the top of the tank and one @ the bottom, a little electronic magic and poof! Cheap low water alert. I used this method to monitor mixing tanks/PLC

     

    But the nail method is not a great solution as you wont be collecting very much data beyond "low" "not low" For more advanced measure... you can use more contact points (more nails) or... smarter sensors!

     

    Before you 'figure-out' what sensor to use, define your objective.

    What are you trying to measure? 

    Are there material related restrictions?

    Precision?

    ....


    example:

    Objective:

    We want to measure the water level in a large tank with reasonable precision. The measurement should be in real time with multiple data samples over 1 min. Lets also assume we are farming fish, thus no metal in the water.

     

    SO..

     

    No metal = we cant use the nail trick... We could use a float, the float can have an internal magnet read by a hall effect sensor. A hall effect sensor is going to out-put an analog voltage that corresponds to magnetic field intensity. Although it's a valid method for measuring position, we can do better in the accuracy department.

     

    Another option is to use the float but instead of a hall effect sensor we can connect the float to an encoder. The encoder is has greater accuracy then the hall effect but who knows whats in the cheap plastic floats, don't want to hurt the fish.

     

    Yet another option... IR, simple IR diode circuit (reflector/emitter). Float a reflective disc and point the IR @ the disc. The IR method has good accuracy and a smaller footprint in the water, which reduces the risk of contamination, but the disc is still a source of contamination. So lets go with a non-contact Ultrasonic Sensor

     

    PING the water like a dolphin and never get wet! Score!

     

    Just remember to weigh the negatives of each option. Some designs may suffer from poor precision, limitations in relation to distance, drift, interface, speed, and don't forget to pay-attention to stuff like temperature/humidity degradation. After-all how much use is a sensor if you don't trust the values.

     

     

    Hope this helps, .. I'm trying to put together my project proposal as this contest is right up my alley. I married a biologist who works at the local college. I have done a lot of pond/greenhouse/habitat building and I already have a team of students and community support. (by the way, even if we compete against each-other, I will still offer assistance/advice.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Sorry about all the questions, but I was just finishing the specifications as I was looking through my design, and was wondering:

    How big does it have to be?

    Is it meant to be outside or inside?

    If inside should we use inside lamps or can we use solar energy?

    I would really appreciate it if someone could help explain these to me. Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Joshua,

     

    An indoors solution is a mandatory requirement because it is specifically mentioned in the blog post. The other things that you mentioned (i.e. size, lighting) are open to you to design and implement as you see fit. You also want to make best use of the hardware from the kit list.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Joshua,

     

    An indoors solution is a mandatory requirement because it is specifically mentioned in the blog post. The other things that you mentioned (i.e. size, lighting) are open to you to design and implement as you see fit. You also want to make best use of the hardware from the kit list.