Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Documents Vertical Farming Design Challenge
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 29 May 2015 11:07 AM Date Created
  • Last Updated Last Updated: 15 Jun 2015 3:50 PM
  • Views 9254 views
  • Likes 11 likes
  • Comments 51 comments
Related
Recommended

Vertical Farming Design Challenge

image
Vertical Farming Design Challenge

image  All About Vertical Farming

image  Overview Video

image  Prizes

image  Terms and Conditions

image  Kit List

 

Background

 

From Wikipedia

According to current projections of population growth, the world population of humans will continue to grow until at least 2050, with the estimated population, based on current growth trends, to reach 9 billion in 2040,and some predictions putting the population in 2050 as high as 11 billion. World population passed the 7 billion mark on October 31, 2011.

 

From the World Wildlife Organization

Soil is the earth’s fragile skin that anchors all life on Earth. It is comprised of countless species that create a dynamic and complex ecosystem and is among the most precious resources to humans. Increased demand for agriculture commodities generates incentives to convert forests and grasslands to farm fields and pastures. The transition to agriculture from natural vegetation often cannot hold onto the soil and many of these plants, such as coffee, cotton, palm oil, soybean and wheat, can actually increase soil erosion beyond the soil’s ability to maintain itself.

Half of the topsoil on the planet has been lost in the last 150 years. In addition to erosion, soil quality is affected by other aspects of agriculture. These impacts include compaction, loss of soil structure, nutrient degradation, and soil salinity. These are very real and at times severe issues.

 

From VerticalFarm.com

By the year 2050, nearly 80% of the earth’s population will reside in urban centers. Applying the most conservative estimates to current demographic trends, the human population will increase by about 3 billion people during the interim. An estimated 109 hectares of new land (about 20% more land than is represented by the country of Brazil) will be needed to grow enough food to feed them, if traditional farming practices continue as they are practiced today. At present, throughout the world, over 80% of the land that is suitable for raising crops is in use (sources: FAO and NASA). Historically, some 15% of that has been laid waste by poor management practices. What can be done to avoid this impending disaster?”

 

The confluence of these observations and forecasts points to the need to increase our ability to grow fresh food in urban areas – closer to the populations that will consume them.  This means shifting from traditional outdoor gardens to indoor systems for food production.  Electronic Engineers are uniquely suited to provide systems based on a technology infrastructure that can lessen required energy consumption in production and improve the output of a smaller space.

 

Vertical Farming is a developing industry growing to meet these demands.  The main areas for measuring their success – and focus for improvement - are the production output per square foot, monitoring and lessening the energy and water consumption, and efficiencies around harvesting.

  

The Challenge

We will select 15 challengers from all entries received to build indoor, vertical farms that are true IoT solutions. The projects should include:

  • Environmental monitoring (light, temperature and humidity)
  • A watering and feeding system
  • A greater growing surface than just the overall footprint of the build
  • Energy monitoring to collect data on the overall consumption of power and water by the system


Help Along the Way

In addition to the great Kit that Challengers will receive, we also have support for those of you without a green thumb.  We’re going to be recommending the types of seeds to buy, the types of fertilizer and ranges to be aware of when you’re monitoring moisture, light and humidity.  We’ll announce a point in time about six weeks out when all Challengers should start their seedlings.  After a 7-10 day germination period, your seedlings should be transferred to your Vertical Farm.  Then after about a month of growing we’ll ask you to harvest your crop.  Submitting information about the overall weight of the harvest and the average height of the plants will help the Judges determine the best developed solutions.

And if your seedlings start looking sickly, then post a question on the Design Challenge site and someone from the Vertical Farming Association will give you tips and suggestions to help you nurse your plants back to life.

 

More details coming soon.

  • vertical
  • vertical_farming
  • Design
  • challenge
  • farming
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +3
    Questions are a good thing! They inspire thought and conversation. Never be sorry you asked a question, and never feel stupid for asking a question that is considered 'basic'. I ask basic questions all…
  • jkutzsch
    jkutzsch over 10 years ago in reply to shabaz +3
    I will definitely have to check those groups out, I went through last night and just started following a variety of interesting groups but was noticing a bunch have not been updated in years. :-) The specifics…
  • mcb1
    mcb1 over 11 years ago in reply to clem57 +2
    clem57 Clem Yes it did strike me that in very hot climates it could be an issue with water transvapouration putting them at a disadvantage. Even her in summer we lose 4-5mm per day, which many won't realise…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    TRANSLATE TO PORTUGUESE PLEASE ..

     

    Penso que o futuro da nossa agricultura vai ser subterranea .. com abundancia de solo ... porem debaixo da terra .. terra muito ferteis e boa para o plantio, só vai faltar a melhorarmos na nossa condição de iluminação, em um futuro muito proximo vamos abrir tuneis e usar para fazer quintas subterraneas de cultivo,

     

    Wbarros.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 11 years ago

    TRANSLATE TO PORTUGUESE PLEASE ..

     

    Penso que o futuro da nossa agricultura vai ser subterranea .. com abundancia de solo ... porem debaixo da terra .. terra muito ferteis e boa para o plantio, só vai faltar a melhorarmos na nossa condição de iluminação, em um futuro muito proximo vamos abrir tuneis e usar para fazer quintas subterraneas de cultivo,

     

    Wbarros.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to e14 Contributor

    Wellington,

     

    todo lo que puedo hacer por ayudarte es una traducción muy sencilla de los conceptos mas importantes en español, pero no lo hablo muy bien. Si puede ayudarte pregunta lo que mas te necesita en este comentarios y como tengo un minutito te dire.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Hello!

     

    Do you want to translate to or from Portuguese?


    Here is from your text in PT to EN:

    I think the future of our agriculture will be underground, with soil abundance however underground, fertile soils, good for planting and farming. It will be missing the improvement on our lighting condition. In a close future we will open tunnels and use them to farm and cultivation.