Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Documents Vertical Farming Design Challenge
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 29 May 2015 11:07 AM Date Created
  • Last Updated Last Updated: 15 Jun 2015 3:50 PM
  • Views 9237 views
  • Likes 11 likes
  • Comments 51 comments
Related
Recommended

Vertical Farming Design Challenge

image
Vertical Farming Design Challenge

image  All About Vertical Farming

image  Overview Video

image  Prizes

image  Terms and Conditions

image  Kit List

 

Background

 

From Wikipedia

According to current projections of population growth, the world population of humans will continue to grow until at least 2050, with the estimated population, based on current growth trends, to reach 9 billion in 2040,and some predictions putting the population in 2050 as high as 11 billion. World population passed the 7 billion mark on October 31, 2011.

 

From the World Wildlife Organization

Soil is the earth’s fragile skin that anchors all life on Earth. It is comprised of countless species that create a dynamic and complex ecosystem and is among the most precious resources to humans. Increased demand for agriculture commodities generates incentives to convert forests and grasslands to farm fields and pastures. The transition to agriculture from natural vegetation often cannot hold onto the soil and many of these plants, such as coffee, cotton, palm oil, soybean and wheat, can actually increase soil erosion beyond the soil’s ability to maintain itself.

Half of the topsoil on the planet has been lost in the last 150 years. In addition to erosion, soil quality is affected by other aspects of agriculture. These impacts include compaction, loss of soil structure, nutrient degradation, and soil salinity. These are very real and at times severe issues.

 

From VerticalFarm.com

By the year 2050, nearly 80% of the earth’s population will reside in urban centers. Applying the most conservative estimates to current demographic trends, the human population will increase by about 3 billion people during the interim. An estimated 109 hectares of new land (about 20% more land than is represented by the country of Brazil) will be needed to grow enough food to feed them, if traditional farming practices continue as they are practiced today. At present, throughout the world, over 80% of the land that is suitable for raising crops is in use (sources: FAO and NASA). Historically, some 15% of that has been laid waste by poor management practices. What can be done to avoid this impending disaster?”

 

The confluence of these observations and forecasts points to the need to increase our ability to grow fresh food in urban areas – closer to the populations that will consume them.  This means shifting from traditional outdoor gardens to indoor systems for food production.  Electronic Engineers are uniquely suited to provide systems based on a technology infrastructure that can lessen required energy consumption in production and improve the output of a smaller space.

 

Vertical Farming is a developing industry growing to meet these demands.  The main areas for measuring their success – and focus for improvement - are the production output per square foot, monitoring and lessening the energy and water consumption, and efficiencies around harvesting.

  

The Challenge

We will select 15 challengers from all entries received to build indoor, vertical farms that are true IoT solutions. The projects should include:

  • Environmental monitoring (light, temperature and humidity)
  • A watering and feeding system
  • A greater growing surface than just the overall footprint of the build
  • Energy monitoring to collect data on the overall consumption of power and water by the system


Help Along the Way

In addition to the great Kit that Challengers will receive, we also have support for those of you without a green thumb.  We’re going to be recommending the types of seeds to buy, the types of fertilizer and ranges to be aware of when you’re monitoring moisture, light and humidity.  We’ll announce a point in time about six weeks out when all Challengers should start their seedlings.  After a 7-10 day germination period, your seedlings should be transferred to your Vertical Farm.  Then after about a month of growing we’ll ask you to harvest your crop.  Submitting information about the overall weight of the harvest and the average height of the plants will help the Judges determine the best developed solutions.

And if your seedlings start looking sickly, then post a question on the Design Challenge site and someone from the Vertical Farming Association will give you tips and suggestions to help you nurse your plants back to life.

 

More details coming soon.

  • vertical
  • vertical_farming
  • Design
  • challenge
  • farming
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor +3
    Questions are a good thing! They inspire thought and conversation. Never be sorry you asked a question, and never feel stupid for asking a question that is considered 'basic'. I ask basic questions all…
  • jkutzsch
    jkutzsch over 10 years ago in reply to shabaz +3
    I will definitely have to check those groups out, I went through last night and just started following a variety of interesting groups but was noticing a bunch have not been updated in years. :-) The specifics…
  • mcb1
    mcb1 over 11 years ago in reply to clem57 +2
    clem57 Clem Yes it did strike me that in very hot climates it could be an issue with water transvapouration putting them at a disadvantage. Even her in summer we lose 4-5mm per day, which many won't realise…
Parents
  • mcb1
    mcb1 over 11 years ago

    I think this challenge is a great idea but as an observer I have a few questions.

     

    1. These items aren't included in the Terms and Conditions.

            image

    2. element14 community is truly global, and the past challenges have contestants from Northern and Southern Hemispheres.

         Since the Nothern Hemisphere is entering summer, while the South is entering winter, the temperatures and sunlight have dropped by at least a magnitiude, so the growing conditions aren't exactly similar.

         The energy used to support this will be different. Will this impact on the contestants result?

     

    3. Soil productivity and sustainability is tied to proper PH and Essential minerals balance.

         While it is possible to add products, one of the key items on the first page Infografik suggest fertilizer is scarce. (or could be)

    Will there be any consideration/suggestions to using organic methods of ensuring the soil remains productive for years to come.?

    Is the association/sponsors providing any guidelines to help people do soil sampling so they can maximise the output, and help stop poor practices as stated here ? http://www.verticalfarm.com/

     

    I see from the map Vertical Farming , there is nothing in the Southern Hemisphere ...anywhere.

    Is there a reason.?

    image

     

    Thanks

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 11 years ago

    I think this challenge is a great idea but as an observer I have a few questions.

     

    1. These items aren't included in the Terms and Conditions.

            image

    2. element14 community is truly global, and the past challenges have contestants from Northern and Southern Hemispheres.

         Since the Nothern Hemisphere is entering summer, while the South is entering winter, the temperatures and sunlight have dropped by at least a magnitiude, so the growing conditions aren't exactly similar.

         The energy used to support this will be different. Will this impact on the contestants result?

     

    3. Soil productivity and sustainability is tied to proper PH and Essential minerals balance.

         While it is possible to add products, one of the key items on the first page Infografik suggest fertilizer is scarce. (or could be)

    Will there be any consideration/suggestions to using organic methods of ensuring the soil remains productive for years to come.?

    Is the association/sponsors providing any guidelines to help people do soil sampling so they can maximise the output, and help stop poor practices as stated here ? http://www.verticalfarm.com/

     

    I see from the map Vertical Farming , there is nothing in the Southern Hemisphere ...anywhere.

    Is there a reason.?

    image

     

    Thanks

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • clem57
    clem57 over 11 years ago in reply to mcb1

    mcb1 Some could grow with a minimum soil and I think this may go into the judging criteria. As to our southern cousins, you have a valid point, except here in Texas where the sun is brutal hot and can toast eggs on a car hood. You may be at the advantage. image

    Oh the fact of locations in the north is due to heavier concentrations of cities over the equator. image But they could be open to future expansion in the down under places. BTW, after some research  I discovered this field is very early stages and has a lot to explore which can may the challenge more interesting. Are you considering this one <<< Hope so.image

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to clem57

    clem57

    Clem

    Yes it did strike me that in very hot climates it could be an issue with water transvapouration putting them at a disadvantage.

    Even her in summer we lose 4-5mm per day, which many won't realise.

     

    The challenge will need careful balancing though, because those in a dense urban area of single level dwellings, may be more disadvantaged than those in a high rise.

    As I understand the amount of sunlight falling on the ground in some cities is very low due to pollution or weather.

     

    Each will have unique real world challenges to overcome, and hopefully apply to the greater mass.

     

    Are you considering this one <<< Hope so.

    Thanks but I'm already doing Teachers Pet, so no I'm not applying ...and besides I have LOT's of horizontal space for growing ...

     

    Cheers

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • element14Dave
    element14Dave over 11 years ago in reply to mcb1

    Hey mcb1, the criteria for this contest is that it be an indoor application to minimize the variables you have outlined above.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to element14Dave

    the criteria for this contest is that it be an indoor application to minimize the variables you have outlined above

    Dave thanks for clrifying.

     

    I was looking at this from a point of view that if replicated 100's of times over, you'd want it to be saving the resource, not replacing it each year with new soil, etc.

     

    Mark