Products
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
Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Blog Wireless charging - status update 2
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: hlipka
  • Date Created: 17 Jun 2014 8:00 PM Date Created
  • Views 2823 views
  • Likes 1 like
  • Comments 17 comments
  • beyond_the_phone
Related
Recommended

Wireless charging - status update 2

hlipka
hlipka
17 Jun 2014

I actually wanted to finish a blog post explaining the full schematic today, but since my PCB arrived today I thought it might be time for another status update (so no German version again - I will leave them for the informational posts...).

So what happened in the last two weeks? As already mentioned, I finalized the PCB and send it away. I did go with Würth in the end. They were not the cheapest of the lot, but provided the most bang for the buck. I got 5 day manufacturing time (and since they deliver with courier, probably even from Germany, delivery also takes only one day). Also, they did not charge extra for silkscreen or solder resist (as may happen with cheaper manufacturers). And last but not least I got Ni/Au plating for still the same price, which is not only better for long-term usage, but also better than HASL for SMD soldering. So I send the board files off to WEdirekt (no need to convert them to Gerbers), and thanks to Simon Leuz I even got a 10 percent rebate image

And lo and behold, the board arrived today. Opening the envelope reveals this:

image

Looks strange, I did not remember to order a white PCB... But further unwrapping reveals the real PCB, and it looks really nice:

imageimage

The silkscreen looks different - it seems to be color-less, and is matte finish. Given more time to look at the options of Eagle I should have made the vias tented. I do not need to solder on them (OK, maybe use them for probing signals), but there are many places where the silk screen runs over the vias (the board is populated rather dense). Also, I should have made the silk screen a little bit thicker (the font size is OK though), so it would be more readable.

While waiting for the PCB, I also made my Farnell order (finally...). I waited so long to be sure that I really could order anything I needed for the project. (And I really found some crucial part in the last week that I did not have available). Farnell was little bit faster than Würth, but they just had to package all the things up. This how a Farnell order worth 200 EUR (that made 60 items...) looks like:

image

It came actually in four different parcels, since parts of it came from UK (the rest from Belgium), and the etching chemicals I ordered are treated as dangerous goods and came in separate parcels.

About one third of the stuff I ordered went into this project, which means that my project box with all the stuff in it now looks pretty crowded:

image

Until now, I discovered two errors I made. First, I ordered two type of resistors in 0603 package where it should have been 0805 (as the footprint is on the PCB). Second, two resistor footprints on the PCB are 1206 where they should have been 0805. Both are fortunately not fatal (the affected resistors are not the same ones), and the resistors should fit nonetheless (though soldering 0603 components by hand will get tricky).

I also worked on the enclosure for the transmitter - after all it needs to be handled by my son. But since its now finished by now, I did not take any pictures (it just needs some final touches to be ready).

So I will try to finished the enclosure today, and then start populating the PCB. Since I did not prototype all of the parts of the circuit, I will start doing only parts of the PCB, and then test it to be sure it works as intended (and without destroying other parts, maybe). Oh, and there is another article to be written...

  • Sign in to reply
Parents
  • mcb1
    mcb1 over 12 years ago

    Nice work.

    We suggested several drinks before soldering the small smd parts ... to calm the nerves.

     

    When I used Hackvana for my boards he had a very good guide and it included sizing for Silkscreen, and yes the minimum size is legible but looks better a couple of mils larger.

     

    Once you gut your Groomer, we can trade pictures, as they have gutted one at the skifield and used it to power a Tow. image

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hlipka
    hlipka over 12 years ago in reply to mcb1

    The soldering itself is not the biggest problem - I tend to flip away such small parts with the tweezers and then needs too much time to find them again... And my rule with alcohol is to never drink when you get the feeling you need it. Maybe lost football world cup finals will be an exception, we will see... (thats another problem with my time frame right now, btw.)

    Regarding the silk screen: the font size itself is not the problem. As you can see on the pictures, its large enough. But the strokes should have been thicker. It might be that I forgot to activate vector fonts in the Eagle settings, though.

    I surely will post some pictures when the project is finished. But I think it will still loose any comparision with the real ones:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to hlipka

    I know what you mean about those small parts going somewhere, and then trying to find them.

    I think the idea was to drink before you needed it, and to steady the hands  ... well that was the theory.

     

    Mitch links to this http://mindbleach.com/words/eagle-text-silkscreen-width/ in his guide.

    basically the Height x stroke width should be a minimum of 4mils, but 6mils is better, so smaller size ---> wider stroke.

     

    That groomer is far too flash and looks fairly late model.

    The ones with a winch are really impressive.

     

    Good luck

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 12 years ago in reply to hlipka

    I know what you mean about those small parts going somewhere, and then trying to find them.

    I think the idea was to drink before you needed it, and to steady the hands  ... well that was the theory.

     

    Mitch links to this http://mindbleach.com/words/eagle-text-silkscreen-width/ in his guide.

    basically the Height x stroke width should be a minimum of 4mils, but 6mils is better, so smaller size ---> wider stroke.

     

    That groomer is far too flash and looks fairly late model.

    The ones with a winch are really impressive.

     

    Good luck

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • hlipka
    hlipka over 12 years ago in reply to mcb1

    Thanks for the links explaining the silk screen. I should have known that before - with my text size of 50 mil the ration should have been at least 10%, but its 8% only...

    The groomer looks so shiny because it did not got so much use last season (there was just not enough snow in our regular skiing area). And I think it has a winch, but its mounted on the back, so its not visible in this picture.