element14 presents
  • Challenges & Projects
  • More
element14 presents
e14 presents blogs Build Inside The Box - Sump Pump Alarm
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kmikemoo
  • Date Created: 5 May 2021 6:46 PM Date Created
  • Views 9295 views
  • Likes 17 likes
  • Comments 23 comments
  • buildinsidethebox
  • build inside the box
  • bitb
Related
Recommended

Build Inside The Box - Sump Pump Alarm

kmikemoo
kmikemoo
5 May 2021

Thank you Christopher Stanton and element14 for the opportunity to Build Inside The Box!  It was great fun.

 

Getting the box was a moment of great joy and great panic as the reality of "I've got to build something!" really hits home.  I retreat to my basement lair and begin to think.

  Think.  Think.  Think.  THUMP, Thump, thump.  Argh!  Silly sump pump.  I don't remember it being so loud.

  Think.  Think.  Think.  THUMP, Thump, thump. ARGH!!!  That's it!  I'm buying one of those silent check valves!

  What integrates temperature, a switch and something with an op amp?  What can I make with the op amp?  THUMP, Thump, thump.

So... I'm not quite sure how I came up with this as an idea.

 

As the title indicates, the plan was to use the components to make a monitoring system for my sump pump to alert me of abnormal conditions and to give an indication of how often the pump runs.  "All the time" and "I can't remember the last time" are not very accurate time measurements.

The write-up should be a shortened version of the video.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Vishay TCST1103TCST1103 Photo Interrupter

The photo interrupter as part of a high water level float switch just made sense.

  imageimageimage

 

Microchip MCP9701-E/TOMCP9701-E/TO Temperature Sensor IC

By living in a house with a sump pump, I've learned a few of the quirks of the system - like when the outlet freezes, the water doesn't go anywhere - so the pump just keeps on running.  In this scenario, the sump water acts as a heat sink for the long running pump.  This, of course, warms the water - quite a bit, from the two incidents that I can remember.  It wasn't until I did some experimenting for this build that I discovered how slow the water temperature rises - which is a good thing for the longevity of my sump pump.  0-1023 analog in.  It moves about 25 in 30 minutes, worst case (zero flow, almost no water added to the sump during the 30 minutes).  To get to the bath water temperature that I remember, my pump must have been running for hours.

 

Moving ahead, I just needed to place the temperature IC in the water near the pump and read the output.  I attached leads to the IC, put on some heat shrink to prevent shorting, stuffed it into a plastic tube and sealed the end with hot glue.

I will use the analog in value for processing as the actual temperature doesn't improve the functionality.  I do not plan to display it - because the system will sit in the corner of a basement, unattended, alone (most of the time).

imageimage

 

Microchip MCP604-I/PMCP604-I/P

My plan was to use this quad op amp as my non-contact voltage sensor.  I tried a number of circuits, but most did not function as advertised.  I decided to try a very simple circuit and it worked better than the rest.  It did not behave on the Arduino as it did on the test bench.  On the test bench, I got about a one volt swing between output with power on and output with power off.  On the Arduino, the readings cycled between 1023 and 0 on the analog input when power was ON, usually in sets of three.  The input remained at 1023 when power was OFF.  To detect this, I took 10 samples and looked for a 0.  Other than that adjustment in code, the circuit performed as expected.  I could detect loss of AC power.

  imageimageimage

 

ST Range/Gesture Sensor 53L0-SATEL-I1

This is a VL53L0x sensor and the board is an I2C device.  I chose to use the Adafruit library and the sensor worked reasonably well.  I say "reasonably well" because one must have realistic expectations when bouncing a laser off of water.  I wound up using the fluctuations in distance readings to my advantage in triggering the begin and end of a fill/drain cycle.  Average 6 readings.  If four of these average readings in a row are increasing, the pump must be draining the sump.  The time difference between cycles is divided up to display in weeks, days, hours or minutes.  I probably should have added seconds as well - in retrospect.

 

One of the two sensors in the kit seemed a little finicky - until it stopped working.  It won't initialize.  The other one is still performing as expected.

  imageimageimage

 

Midas MDOB128032EV-WS OLED Graphic Display

This display has an SPI interface even though the screen printing would lead someone to assume I2C.  The [Buy Now] button said the interface was SPI so that was what I ran with.  I connected SDA to MOSI (D8) and clock to clock and it worked.

  imageimageimage

    imageimageimage

.

Overall Project

Again, the vision was to use all of the above components in a sump pump monitoring system.  I chose to use a more graphic build plan.  You can see some of the notes and corrections (like adding the resistors on the photo interrupter circuit).

 

The "as built" isn't quite as neat.  Vcc is the upper string of WAGO connectors.  Ground is the WAGO in the white mount and a 3-pack just to the right of the Vcc buss.

 

The third picture is the completed project.  I'm still waiting for that inspirational moment around the "packaging".  The case is functional, but I want something cooler.

  imageimageimage

 

MULTICOMP PRO Portable USB High Capacity Power Bank - 10000mAh

Finally, the device that powers it all... the power bank.  In an ironic twist of fate... this one confounded me for a bit - and I was one of the folks that recommended putting it in the box.

I had completely forgotten about the Auto OFF feature of large power banks.     Serves me right.

image

I did a little experimenting to see how low a current draw I could get away with to keep the bank alive, but had to opt for a 100mA draw as a balance between enough draw and hearty enough on-hand components.

I do want to build a 555 controlled pulse draw device to decrease battery drain, but that is for another day.

 

Conclusion

This challenge was amazing!  It really helped me dust the cobwebs off of some skills that I thought I still had.  I made fewer mistakes in the coding as time went on.  I spent most of my bench time trying to get a decent AC detection circuit.  I spent most of my coding time trying to get a reasonably accurate cyclic timer system.  A current sensor would have been easier, but the time of flight sensor is cooler.  I really must figure out if I can recover the one that won't initialize.  With that, maybe I could add a detection circuit that only turned on the display when someone was within range.

 

Thank you again to element14 for allowing me to play along.

 

UPDATE May 8th, 2021:  As I read some of the other builds, I see some folks received a SD card.  I did not but I thought I addressed this in the blog.  I did not.  Must have been one of those fat-finger oops edits.  They happen.  If I needed to use the SD card, it would simply have been used as a data logger.  The next evolution would have been to play audio clips for an alarm instead of using the buzzer.  "Hey!  Hey!  I'm flooding here!"  - Mike

Attachments:
BITB_Main.txt.zip
  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 5 years ago +7
    Great project kmikemoo ! I think you came up with a clever use for the photo-interrupter. This display has an SPI interface even though the screen printing would lead someone to assume I2C. The [Buy Now…
  • kmikemoo
    kmikemoo over 5 years ago in reply to fmilburn +5
    fmilburn I found the post you mentioned just after publishing this - and now can't "re-find" it. I think it was from 2018. There's not much more effective for releasing a flood of information than pressing…
  • jw0752
    jw0752 over 5 years ago in reply to fmilburn +5
    Hi Frank, I think this is the post you were mentioning. https://www.element14.com/community/groups/test-and-measurement/blog/2018/10/15/on-using-a-usb-battery-for-a-portable-project-power-supply John
Parents
  • shabaz
    shabaz over 5 years ago

    Hi Mike,

     

    Great project & video! (& Scarface reference : ).

    The Range/Gesture sensors look quite versatile, if they had both worked, I was thinking maybe one of them could have been used for the float switch too, instead of the photo-interruptor. But it all worked out since you had the photo-interruptor to use anyway!

    It's really annoying that power banks have that auto-off feature : )

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 5 years ago in reply to shabaz

    Thanks, shabaz!  I was definitely amazed when the range sensor responded correctly to water level.

    There has to be some way to defeat the auto-off feature on a power bank that doesn't consume all those milliamp-hours.  Maybe there's someone in the Community that know that circuitry enough to help us crack the code.  That would really be handy.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 5 years ago in reply to fmilburn

    Hi Frank,

     

    I think this is the post you were mentioning.

     

    https://www.element14.com/community/groups/test-and-measurement/blog/2018/10/15/on-using-a-usb-battery-for-a-portable-project-power-supply

     

    John

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 5 years ago in reply to jw0752

    Hi John and thanks!  That was a good post with lots of great comments below it.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to kmikemoo

    If you wanted to experiment with something other than a 555 to keep the battery alive, you could

    maybe try something like this with one of your spare op amps

     

    image

     

    That's a traditional op-amp multivibrator circuit to generate a square wave, with the duty cycle

    modified [the diode gives a charge current much different to the discharge current]. You would

    probably need to experiment with the period and the time it loads the supply for to get it to work

    with your battery pack.

     

    I've tried it with a MCP6022 [I don't have an MCP604] and the basic circuit works ok. Your op amp has

    a more limited common-mode range, so I've biased the inputs so that they both remain below 2V on a

    3.3V supply: it should work on an MCP604, but you'd have to try it to find out. Here are the two

    inputs [blue is the capacitor at the inverting input and yellow is the comparator level at the non-

    inverting input]. This is the fast charging through the diode

     

    image

     

    This next is a longer term view of the same, showing the much slower discharging through the 270k resistor

     

    image

     

    The duty cycle is just below 1% with my circuit values. This next trace shows the gate drive to the MOSFET.

     

    image

     

    I've shown a BSS138 on the circuit, because the simulator says that a 2N7000 or BS170 won't sink

    100mA with only 3.3V gate drive, but in practice I found a real BS170 could almost floor a 33R

    resistor hanging from the 3.3V supply, so you'd probably do fine with one if that's all you had lying

    around [the simulator models must have very conservative parameters].

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 5 years ago in reply to jc2048

    jc2048  Very cool.  I really like the duty cycle.  I've copied the schematic and put it into the "Circuits to try" folder. 

    I actually have zero MOSFETs in my stash o' stuff.  I keep meaning to change that, but then I overthink things and it never winds up coming to pass.  So... if I was going to have a few laying about, what is your recommendation?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to kmikemoo

    what is your recommendation?

     

    Like any component, it depends on what you want to do with them.

     

    The 2N7000 and the BS170 are both TO-92, so work fine with a plug-in breadboard. The specs are very similar, so personally I wouldn't bother with both [I've got a dozen BS170s that I use for experimenting with]. They are cheap and cheerful: in quantity, they sell for a few cents each.

     

    The BSS138 has a lower threshold voltage and a lower on resistance but it's SMD (SOT23), so more appropriate for a pcb, though there's nothing to stop you soldering leads on and using them with a breadboard as though they were conventional parts.

     

    Those are all n-channel parts. Don't know if I've got any small p-channel parts.

     

    I actually have zero MOSFETs

    Doesn't have to be a MOSFET. Do you have any small NPN transistors? Maybe use a Darlington pair to reduce the loading on the op-amp output, rather than just a single transistor.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 5 years ago in reply to kmikemoo

    what is your recommendation?

     

    Like any component, it depends on what you want to do with them.

     

    The 2N7000 and the BS170 are both TO-92, so work fine with a plug-in breadboard. The specs are very similar, so personally I wouldn't bother with both [I've got a dozen BS170s that I use for experimenting with]. They are cheap and cheerful: in quantity, they sell for a few cents each.

     

    The BSS138 has a lower threshold voltage and a lower on resistance but it's SMD (SOT23), so more appropriate for a pcb, though there's nothing to stop you soldering leads on and using them with a breadboard as though they were conventional parts.

     

    Those are all n-channel parts. Don't know if I've got any small p-channel parts.

     

    I actually have zero MOSFETs

    Doesn't have to be a MOSFET. Do you have any small NPN transistors? Maybe use a Darlington pair to reduce the loading on the op-amp output, rather than just a single transistor.