element14 presents
  • Challenges & Projects
  • More
element14 presents
Off-Grid MakerShop Project - The Hydro-Electric System Design & Discussion
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: KalebTheMaker
  • Date Created: 22 Oct 2022 2:28 AM Date Created
  • Views 4184 views
  • Likes 14 likes
  • Comments 29 comments
  • micro-hydro
  • diy
  • power
  • off-grid
Related
Recommended

Project - The Hydro-Electric System Design & Discussion

KalebTheMaker
KalebTheMaker
22 Oct 2022

In addition to the main Solar generation system, I am going to build a backup Hydro-Electric system in the year-round stream. Currently, it is the dryest part of the year and there is still a good amount of water flowing in the stream. From the water lines I can see in the stream it's going to get *much* higher in the winter months which should be more than enough for the turbine. I should be able to generate enough electricity from a turbine to offset the lack of sun in the winter.

The coolest part of hydro is that it generates 24h a day rather than the 5-6 hours of sunlight one might expect on Solar Panels. It's much less wattage, but running all night and day makes up for that.

I am not starting this project just yet, there are a couple more that need to be done first (keep an eye out for those as well), I just wanted to get the topic open so we can discuss. 

This topic is open for discussion, I would love to hear your ideas and have you all involved. I will be documenting every step of the build here with descriptions, pictures and videos.

Why Hydro if I am installing Solar?

The solar array is going to be the main power generator. But during the winter months, it will generate much less than the summer months. I need a way to offset that. Many people run a generator for several hours every couple of days, or as needed. Since I am running a shop with CNC routers, welders, laser cutters, etc, I would need to run the generator quite often. And with gas prices around $6.70/gal right now, It's the most expensive way to generate electricity that I can think of. With the stream flowing all winter, It's a perfect opportunity to harness that potential energy to generate power. 

Setting the Stage

image      image

The stream runs through a large part of the property dropping in elevation. I walked the creek from the bottom to the top looking for good sites to collect water, and to place the turbine. The graph below shows the elevation & distance between these locations. Yes, it's in reverse, but I walked from bottom to top and did battle with google sheets and lost... Currently, it is October and the dryest part of the year in my area. There is still flow in the stream right now. Not much, but it is running. From observing (what I think are) the high water lines, it will have quite a bit of water flowing during the winter months. 

image

As you can see, we get about 16m of elevation drop over about 200 meters in distance. I think this qualifies as a "low head" system. I won't know a GPM or L/S rate until it the rain starts, and I get a capture system in place.

I will also need to run a conduit from the hydro generation site up to the solar site since that is where all of the batteries will be.  

The Current Plan

The current plan is to build some sort of intake system with filtration to filter out large debris and pipe that into a 50gal plastic barrel. The water will enter from the top of the barrel and exit about half way up the barrel in a 2" poly tube. The water will then run through approximately 500-700' of 2" poly tube to a motorized ball valve and then into the turbine distribution. The 2" pipe needs to be reduced to much smaller nozzles that shoot the water into the pelton wheel of the turbine. As beacon_dave suggested, I could also install motorized valves on each of the nozzles to control the amount of flow to the pelton wheel. 

The Intake

The intake will divert water from the natural streambed into (probably multiple) 2" poly tubes. It will have to be constructed at a place in the stream where there is a small but dramatic elevation change. It could be as simple as cutting a plastic barrel at a diagonal and fitting it with 2" fittings. It will also have to have a screen to filter out large debris. I have seen some pretty clever methods for intakes. One was a rotating screen drum with catchment on the bottom 1/3rd. The rotating screen let all the large debris fall off back into the flowing stream. 

The Barrel

Water flows into the barrel from the top, and exits in the center. This serves two purposes. First, it is another stage of filtration by having any heavy debris fall to the bottom of the barrel (I will have to have some sort of cleanout), and second, it removes any air in the line by having the water enter at the top, and exit at the center. 

The 2" Poly Tube

This may be the most critical part of the system. The 2" tube needs to be as long as possible, and drop in as much elevation as possible to build up enough "head" to run the turbine. "Head" is the height measurement from where the water enters the system down to where it exits the system at the turbine. Combined with the amount of water flowing through the 2" poly tube we can calculate how much pressure will be in the tube, and even calculate how much power could be generated. This is a very simplified description of how this works and there are formulas for all of this which I do not understand yet but have a general idea. 

The Turbine

I have looked into building my own, and that's not off the table, but there are off-the-shelf options available that are within the budget. If they are more efficient and can generate more power, that is going to be very attractive. Dont worry, there is plenty of other DIY in the rest of the system.

These systems typically use a Pelton wheel connected to a generator, with multiple reducer nozzles firing the water at the wheel from different angles. These are what I think of as a "side load" type of turbine. Another style which I have not investigated much yet, but supposedly works better for a "low head" are what I think of as a "top load" where the water falls down onto some sort of impeller to turn the generator. 

The turbine type is all up in the air still. I have not decided on which type to buy, use, or build.

That is about all the information I have on this project so far. Please feel free to discuss this, I will be monitoring this blog and will try to respond to everyone. 

-Kaleb

  • Sign in to reply
  • beacon_dave
    beacon_dave over 4 years ago in reply to KalebTheMaker

    "...When I walked the creek the other day, there was a lot of large debris wedged in rocks and sharp bends..."

    Natural first stage filtration Slight smile

    I guess you could aim to have a series of graded rock/gravel beds before the intake filter to try and remove most of the debris upstream of the final filter.

    The coanda box appears a bit inefficient in some ways as you waste a lot of water over the top just to provide the self-cleaning action. A submerged intake filter would avoid the floaty debris however I suspect is likely to silt up without regular cleaning, or at least a cunning plan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • KalebTheMaker
    KalebTheMaker over 4 years ago in reply to beacon_dave

    I don't have the elevations for those two photos. There is a road that runs along the length, it's about avg 30' from the road and 20' lower than the road. It's mostly above ground, but there are areas where there are large boulders directly in the path, so the water ends up flowing under them. And places where it gets pretty wide and the water gets shallow. 

    The only wildlife I have seen in the stream are bugs. I am fairly certain that it is fed from multiple springs about a mile above my property. I have not seen any fish, and I highly doubt I ever will. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago

    "...I think this qualifies as a "low head" system..."

    According to the definition at:
    https://www.energy.gov/energysaver/planning-microhydropower-system

    "...Low head refers to a change in elevation of less than 66 feet (20 meters), and ultralow head refers to a change in elevation of less than 10 feet (3 meters)..."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • KalebTheMaker
    KalebTheMaker over 4 years ago in reply to robogary

    It will take a bit of upfront to get this going, but it will eventually be worth it. If this can offset my generator fuel cost, even a little, it will pay for itself over time.

    One kind of interesting part of the process for me is that currently, I have no solar or hydro and am running purely off of a battery that I charge with a generator at just over a gallon of fuel a day at $6.50ish/gal. With my current temporary setup, I would only need to have something like 53w on the hydro system to completely charge my battery. Going from access to so little power, to what I will have at the end of (these) projects will be an amazing difference. Basically camping, to modern living.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • KalebTheMaker
    KalebTheMaker over 4 years ago in reply to DAB

    This is completely a backup system, I will get most of my power from the solar array. I am in California, and we have a lot of sunny days even during winter. And from some of the videos I have seen, and the low-head generators available, I am hopeful to get some real usable wattage out of the system. 

    There is a second site, it's a seasonal creek, and I have no idea how much flow there is, or how long it flows after a rain, but there is a 40ish foot waterfall and much more elevation difference in a shorter distance. It actually runs right to the bottom of the hill below where my batteries will be.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>