Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum audio
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 41 subscribers
  • Views 433 views
  • Users 0 members are here
  • Controllers
Related

audio

e14 Contributor
e14 Contributor over 10 years ago

i need help or ideas on an audio signal splitter...... a 3 to 1 type i have 4 speakers but 3 different devices to hook up, 1 already has volume comtrol so im looking to build like a switch which would let the first device play regular but then when i switch it to the other device it will shut off the sound from the first device and let the 2nd device sound play thru the speakers but also control the volume for the second device......also the same for the third device

  • Sign in to reply
  • Cancel
  • shabaz
    shabaz over 10 years ago

    It is not a splitter, more a selector that you're looking for (or a mixer for a more general purpose solution).

    Easiest way would be to use some 1k-ohm resistors and combine the signals from all your inputs into a common point (if you're

    talking about analog line outputs because you've not mentioned any detail in this area).

    You could use toggle switches to switch off some inputs if needed.

    So, if only a single source has audio then that is all you'll hear, with no switch interaction needed.

    If you have multiple sources playing you can kill any of them (or all of them) by your toggle switch.

    Or use a single rotary switch - usually more expensive - to switch off all except one.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • supper_slash
    supper_slash over 10 years ago

    I would like more information on the project, please.

    As an example of the visual, I have 2 thoughts in mind.

    (1)

    2 cd players with non-powered 4 channel outputs and one mixer/Amp combo that is powered with 4 speakers outputs.

    All needing to be connected to speakers.

    OR

    (2)

    2 guitars that need to be selectable, alongside a keyboard. All of wich needs to be patched out to 4 speakers.

    ......

     

    Or am I totally off base? Please let me know where we are going with this.