Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Briefcase sized, portable plastic grinder/filament extruder/spooler
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 43 subscribers
  • Views 3609 views
  • Users 0 members are here
  • 3D Printing
Related

Briefcase sized, portable plastic grinder/filament extruder/spooler

e14 Contributor
e14 Contributor over 10 years ago

Enjoyed the video on the briefcase sized 3D Printer.  How about a companion unit to make filament?  Should be able to take suitably sized plastics, grind, extrude and roll onto spools, for use with the briefcase-sized 3D printer, making for a completely portable 3D factory.  Simple menu selection (ie-soda bottles, milk jugs, cd cases, plastic bags, etc.) to set the temperature and extrusion/spooling speed.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to makerkaren +2
    I have a friend that teaches technology, including 3D printing. Part of their class projects is printing and finishing low-cost plastic prosthetics made to fit a specific child in their community. Their…
  • kingrahl
    kingrahl over 10 years ago +2
    I've been working nearly four years (off and on) on an improved design of Ben's Briefcase 3D Printer. One of my intentions was to include (or design separately) a folding filament making station. (about…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to beacon_dave +2
    IMHO, that requires an unnecessary melt, more energy, time, and an additional molding process. Might as well make pellets, at that point. That's really the purpose of using shredded stock, then being able…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    A small shredder, hand-driven by a ratchet...

     

    images?q=tbn:ANd9GcQvUeFPW2eNckalcCts1Yf8Hr0WPP0wTx7QfwD_ZKiCFw5hMw9L

     

    The "Filastruder" uses a soda bottle for a hopper...

     

    uvhHles_1024x1024.jpeg?v=1442545455

     

    These are part of why I think it CAN be done into a small briefcase-size unit, where most of the unit is actually a fold-out hopper that can double as reel storage.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to e14 Contributor

    The shredder might need a motor with quite a bit of torque though depending on the intended duty cycle. Just thinking of typical compact paper shredders here which can overheat after only a few minutes of continuous shredding of a few sheets at a time. Can gear it down but I suspect that shredder blades will have an optimum speed to chip the plastic rather than to chew it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to beacon_dave

    High torque drill, maybe?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to e14 Contributor

    Would perhaps first need to work out how much material needs to be shred in order to have enough raw plastic to extrude a usable amount of filament in one go before choosing an appropriate sized motor.

     

    I'm assuming that if touring with this briefcase then time will be limited, so probably looking at stockpiling the bottles beforehand then straight into near-continuous shredding upon arrival, and extrusion into reels of filament, whilst consultations about prosthetics and 3D design take place. Then as soon as the first reel is ready 3d-printing can start.

     

    I've just weighed an empty 2pint milk carton here and it weighs around 25grams. Googling and you appear to get just over 100m of 3mm diameter filament per kilogram of plastic.

    Filament volume and length – ToyBuilder Labs

    So that's around 2.5m of filament per milk carton, or around 40 such cartons requiring shredding for each 100m spool.

     

    A high torque cordless drill motor is compact however it's not really designed to run continuously for any length of time. Entry level bench pillar drills tend to have 1/3HP or 1/2HP electric motors but they are large and heavy.

     

    My crosscut office shredder here is rated at around 1/5HP and definitely would not be up to the job.

     

    Looking at the Precious Plastic shredder build and they are suggesting a motor rating of around 2.7HP running at  @ 70RPM. Sounds a lot however perhaps required for 'just works' type operation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 10 years ago in reply to e14 Contributor

    Would perhaps first need to work out how much material needs to be shred in order to have enough raw plastic to extrude a usable amount of filament in one go before choosing an appropriate sized motor.

     

    I'm assuming that if touring with this briefcase then time will be limited, so probably looking at stockpiling the bottles beforehand then straight into near-continuous shredding upon arrival, and extrusion into reels of filament, whilst consultations about prosthetics and 3D design take place. Then as soon as the first reel is ready 3d-printing can start.

     

    I've just weighed an empty 2pint milk carton here and it weighs around 25grams. Googling and you appear to get just over 100m of 3mm diameter filament per kilogram of plastic.

    Filament volume and length – ToyBuilder Labs

    So that's around 2.5m of filament per milk carton, or around 40 such cartons requiring shredding for each 100m spool.

     

    A high torque cordless drill motor is compact however it's not really designed to run continuously for any length of time. Entry level bench pillar drills tend to have 1/3HP or 1/2HP electric motors but they are large and heavy.

     

    My crosscut office shredder here is rated at around 1/5HP and definitely would not be up to the job.

     

    Looking at the Precious Plastic shredder build and they are suggesting a motor rating of around 2.7HP running at  @ 70RPM. Sounds a lot however perhaps required for 'just works' type operation.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to beacon_dave

    Drills with the impact and hammer-drill settings are intended for heavier, longer operation, since that is for masonry and concrete.

     

    The collection and prep phase might further be defined, as well.  Suppose that the collection and prep is only one type of bottle, since we've already specified one type of plastic, to reduce the need to disassemble and clean.  Clean and cut into relatively flat pieces, and run them through an office shredder, followed by low-heat, to insure dryness.  Caps, tops, bottoms and handles could be set aside, to be recycled using a larger grinder.  For purposes of airline mobility, restricting the plastic makes sense.  When using an automobile for transportation, it would be easier to have a larger grinder.

     

    Once the smaller pieces are pre-shredded (think typical strip-shredder) for the final-grinder/extruder, the final grinder isn't having to do all the work.  Its' purpose is to make the final pieces small enough to feed into the melt chamber and extruder, not ground-down from chunks.

     

    When things gear-up, it might be practical to have several interchangeable extruder heads, for different plastics, rather than trying to clean one out, for use with different plastics, so designing a setup with multiple temperature presets makes sense, either way.

     

    Realistically, I'm trying to help a teacher do more.  Most of their printing is done in the classroom.  However, a fully portable mini-factory could be considered as a more prudent setup, for those with limited space.  If the extruder and the printer both close down to briefcase size, then it can be more practical for home use, mission trips, demonstrations, etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to e14 Contributor

    A demolition hammer drill motor/gearbox might do the trick - they are rated at around 2HP but are still fairly compact.

     

    I'm not 100% convinced about the cutting of the bottles - you are likely to end up with injuries. Crushing them flat however may help feed them into the shredder cutter. However a shredder like this appears to make quick work of whole bottles and will probably feed ok if there is enough weight of material in the hopper

    https://www.youtube.com/watch?v=j6Ghwd29W-o

    Alternatively some sort of a feed tube where the next bottle inserted effectively pushes the previous one into the cutter

     

    In a later design they added a mesh under the shredder which appears to grate the shredded material into smaller pieces.

    https://www.youtube.com/watch?v=VFIPXgrk7u0#t=10m10s

    Not sure how small you can make a cutter that still will bite into a bottle.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to e14 Contributor

    This video shows pretty coarse plastic pieces going into the extruder unit

    https://www.youtube.com/watch?v=p4NoY33-Tfo#t=15m48s

    so it looks like grinding may not be absolutely necessary.