Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Arduino powered system for electric guitar pickup selection.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 45 subscribers
  • Views 3317 views
  • Users 0 members are here
  • arduino
Related

Arduino powered system for electric guitar pickup selection.

QuantumAberrant
QuantumAberrant over 11 years ago

Electric guitars uses switches to select which pickups are activated at a time. Most designs though do not allow for all possible combinations of pickups. Also there are alternative ways of wiring a guitar, series/parallel wiring changes the tone. Also reversing the phase (polarity) gives you other sounds. Almost no guitar gives the option of selecting all of these options because the wiring becomes too complex. I would like to challenge Ben to create a system by which an Arduino can be used to select any of the different combinations.

 

Here are the wiring diagrams to give you a idea.

 

Series/parallel switching.

http://www.premierguitar.com/articles/Adding_Series_Switching_To_Your_Strat

 

In-Pase./out of phase

Wiring Diagram

 

Current mods to help add pickup combinations include:

 

Wiring Diagram

 

If you put all these ideas together you get something like what Brian May from Queen built. http://www.premierguitar.com/articles/21307-mod-garage-inside-brian-mays-red-special

 

Still there is more, pickups with two coils, called "humbuckers" can be "coil tapped" to be single coils, making one more set of switches one might want.

 

I have a Music Man 'Steve Morse' guitar. http://www.music-man.com/instruments/guitars/steve-morse.html

 

It has 4 pickups, and switching between them is crazy complicated all by itself. Here is the diagram: http://imgur.com/r5As604

 

Finally another guitar mod is know as a 'kill switch'. It's basically just a momentary button used to cut the signal to the amplifier, but when used by people like buckethead uses https://www.youtube.com/watch?v=NM8DuJKYlqE

A micro-controller would automate a killswitch and have lots of selectable patterns.

 

Can you help me Ben? Can all of this be built on to one circuit board controlled by a microcontroller? Possibly even with an LCD display that indicates what mode it's in?

  • Sign in to reply
  • Cancel

Top Replies

  • mayermakes
    mayermakes over 11 years ago +1
    its actually not that hard to do without any mcu Here is the DEIMOS CIV a guitar i have built myself about 6-8 years ago: 3 Pickups (2x Humbuckers) every combination possible is selectable, cut of switch…
  • QuantumAberrant
    QuantumAberrant over 11 years ago in reply to mayermakes +1
    That's a cool guitar but I think you vastly underestimate the space those wires takes up. As an example here is a circuit board used in modern Gibson guitars for volume and tone control. http://s1150.photobucket…
Parents
  • ragin62
    ragin62 over 6 years ago

    Hello Peeps,

    I am working on controlling my guitars pup selection and cap selection...phase series parallel...etcetcetc...with the Arduino, also adding in possibly a Rasp Pi (IF I send any signal through the IC (microcontroller), a shift register or two. The cavity in my guitar thus far is extremely large...it caused me concern so I reinforced the bridge and also made it a floating one...added metal bondo fiberglass and a hand cut piece of red oak painted black on back to cover the extra circuitry and extra springs in there. The guitar resonates better then it did new...it is a Washburn Lyon Black strat-style. So-far out of all my 9 guitars this ones sounds and plays the BEST. I also hand cut a solid copper pickguard...lined the cavity with copper foil creating a Faraday shield...and also tying the neck tightly all the way down to the bridge tremelo that is mounted TO the copper shield and the added metal reinforcements beneath. Giving the guitar a SOLID one piece sound. Very resonant. The pups are twin single coils wired in series as homemade humbuckers with one of each "sin-bucker" ceramic magnets replaced by neodyium...or whatever they are called...lol The bridge pup is a new Seymour Duncan Dimebucker. I am adding a voltage octuppler with mini tesla coil and a booster (preamp) made from discrete components etcetcetc...and THAT is why I am pursuing the arduino microcontroller route...have been for some time now. I am glad I found you...this post. Please tell me if you have made any progress...I have...and when I am certain it will be damn near perfect...I will tell you as well.

    Play loud play often! CHEERS! David Sellers

    Oh! The guitar was very light weight...WAS...it now weighs MORE then an old Les Paul. I LOVE it! Peace out...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ragin62
    ragin62 over 6 years ago

    Hello Peeps,

    I am working on controlling my guitars pup selection and cap selection...phase series parallel...etcetcetc...with the Arduino, also adding in possibly a Rasp Pi (IF I send any signal through the IC (microcontroller), a shift register or two. The cavity in my guitar thus far is extremely large...it caused me concern so I reinforced the bridge and also made it a floating one...added metal bondo fiberglass and a hand cut piece of red oak painted black on back to cover the extra circuitry and extra springs in there. The guitar resonates better then it did new...it is a Washburn Lyon Black strat-style. So-far out of all my 9 guitars this ones sounds and plays the BEST. I also hand cut a solid copper pickguard...lined the cavity with copper foil creating a Faraday shield...and also tying the neck tightly all the way down to the bridge tremelo that is mounted TO the copper shield and the added metal reinforcements beneath. Giving the guitar a SOLID one piece sound. Very resonant. The pups are twin single coils wired in series as homemade humbuckers with one of each "sin-bucker" ceramic magnets replaced by neodyium...or whatever they are called...lol The bridge pup is a new Seymour Duncan Dimebucker. I am adding a voltage octuppler with mini tesla coil and a booster (preamp) made from discrete components etcetcetc...and THAT is why I am pursuing the arduino microcontroller route...have been for some time now. I am glad I found you...this post. Please tell me if you have made any progress...I have...and when I am certain it will be damn near perfect...I will tell you as well.

    Play loud play often! CHEERS! David Sellers

    Oh! The guitar was very light weight...WAS...it now weighs MORE then an old Les Paul. I LOVE it! Peace out...