Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum A magnetic VA wind turbine for your home, gives out 10 kw, and small...can you make this?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 44 subscribers
  • Views 803 views
  • Users 0 members are here
Related

A magnetic VA wind turbine for your home, gives out 10 kw, and small...can you make this?

e14 Contributor
e14 Contributor over 11 years ago

Hi, I'm no expert on this subject, but I was wondering, can you make a "magnetic" Vertical axis wind turbine to create 10kw and small(or at least smaller than other 10kw turbines) and hooked up to your home?

when I say magnetic, I mean replace the turbine blades with magnets(or fix magnets on the blades), have another set mounted to create that constant movement for the generator, that way you wouldn't have to rely on wind anymore, and you could make a weatherproof box for it, hooked to an inverter and then to the fuse box.

could this work?

 

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago +3
    Hi Josh, Anytime you come across a situation where someone is telling you that you can get energy from permanent magnets pulling or pushing on each other you are being conned. Energy is only available…
  • clem57
    clem57 over 11 years ago

    http://www.whirlopedia.com/magnetic-wind-turbines.htm says:

    The MagLev wind turbines generally employ "neodymium" or rare earth magnets that don't require electricity to work as would systems equipped with electromagnets. One of the advantages of magnetic wind turbines is that there is little energy loss due to friction.

    Lets look at where to get:

     

    Neodymium is a chemical element with symbol Nd and atomic number 60. It is a soft silvery metal that tarnishes in air. Neodymium was discovered in 1885 by the Austrian chemist Carl Auer von Welsbach. It is present in significant quantities in the ore minerals monazite and bastnäsite. Neodymium is not found naturally in metallic form or unmixed with other lanthanides, and it is usually refined for general use. Although neodymium is classed as a "rare earth", it is a fairly common element, no rarer than cobalt, nickel, and copper, and is widely distributed in the Earth's crust.[3] Most of the world's neodymium is mined in China.

    Sorry China is far to go to get some... Expensive to buy...

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to clem57

    umm...I found some.

    It seems like a really good deal considering the size and pieces:

     

    CMS MagneticsRegistered Neodymium Magnets 1x1/2x1/16" Rare Earth Magnets 8-Count: Industrial Rare Earth Magnets: Amazon.com: Indu…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to e14 Contributor

    Nice, but you said 10,000 watts per hour. You may need quite a few of these. BTW, no wind? Sounds like "free energy".

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to clem57

    hmm...do you think there is a way to make a homemade generator to produce that much wattage?

    if not, then how many would you guess I would need to make to reach 10kwh?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago

    Hi Josh,

    Anytime you come across a situation where someone is telling you that you can get energy from permanent magnets pulling or pushing on each other you are being conned. Energy is only available as conversion from some other form of energy.  For example we can harvest energy from the motion of the air molecules in the wind with a windmill. The mechanical energy of the windmill can then be converted to electrical energy by having it move a magnetic field across a wire. At every step of the process there is a loss of energy which escapes into the environment as heat. For example if we had 10 joules of energy in the wind we might get 7 joules of energy in the mechanical movement of the windmill. The windmill might in turn produce 5 Joules of electrical energy in the wire of our generator. The 5 joules of lost energy are dissipated as heat and lost in the environment.

     

    The magnetic field of a magnet can store energy and release energy.  For example if we push the north poles of two magnets together it will require that we apply a force. As we get the poles closer and closer together we are storing more and more energy. When we let go of the magnet this energy is released by the magnetic field pushing one magnet away from the other. In a way the magnetic field is like a spring in that we can bend it to store energy and then get some of the energy we put in back out when we remove the force.

     

    I have seen on the internet the demonstrations where magnets are attached to a fan and other magnets are attached around the rim. Magically the fan is made to spin with no apparent source of power and power a light bulb. This is a trick, the power to turn the fan and light the bulb really come from a hidden battery or power supply that is supplying the energy to making things happen. The authors of these tricks benefit as their tricks attract views which make the advertisers on their sites pay them more.

     

    You also asked about supplying 10kW of power. There are 746 Watts of power available from one Horsepower. This means you would have to have at least a 13 horsepower motor 100% efficient to get the 10kW power supply that you want. This is a fairly big motor and you can see that you would have to have a reasonably sized windmill to get this much power.

     

    Sorry there is no magic source of power available as the physics of the real world always demands a source and a payment for the energy we use.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to jw0752

    Magnets are the constant source of misunderstanding with regard to energy and "anti-gravity".   However there is still a lot of mystery around magnetic forces inside molecules and atoms.

     

    I believe in the conservation of energy law, but I do think energy can be harvested from vast sources that we haven't tapped into yet.  It would appear like free energy to us but the conservation law would still hold true, we just don't tap it enough.

     

    Kind of like the earth's rotation concept, the conservation law does apply but it appears to be free energy.

     

    My favorite article:

    http://deanspacedrive.org/?p=216

     

    Everyone should read this and then think about it before submitting any "new idea"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to screamingtiger

    image

     

    This?