Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Super Glue Gun 08: Integrating All Mechs -- Episode 310
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 23 Jul 2017 12:46 AM Date Created
  • Last Updated Last Updated: 29 Sep 2017 7:24 AM
  • Views 3329 views
  • Likes 5 likes
  • Comments 14 comments
Related
Recommended

Super Glue Gun 08: Integrating All Mechs -- Episode 310

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Super Glue Gun
Community Feedback
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Previously, the team added the mechanism for the auto stand using a metal wire stand and a guitar string acting as a cable. The cable is actuated by a servo and utilizes a servo library for the Atmel ATTiny20 Microcontroller they are using.  Now they need to find a capacitive touch sensor library, possibly Qtouch from Atmel, to allow the auto stand to retract when your finger touches the trigger.

 

 

Ben goes to work on Autodesk Fusion 360 to design the parts he’ll need for 3D printing.  He filets the edges to form a round enclosure for the magnet and makes room for the capacitive touching piece.  After he’s printed the two piece he’s ready to build an autostand mock up.

He builds the mockup on top of an existing mock-up and puts it on the glue gun mech for testing before they do a redesign of the case. He flips the barrel around so that the hot block is at the top and gives them more room for their stand. He needs to use a spacer on it because the stand has an extremity that needs to be clear of the heater barrel. This requires hot gluing together the hot glue gun. When he’s done he got a proof of concept that he can use before they redesign the top half of the glue gun.

While Ben is working, Felix is researching the Qtouch library, a proprietary library for Atmel microcontrollers, for use with the touch sensor. Ben’s already printed out the holo trigger and put the magnet in place. The sensor will go on the front with the wire coming out the back.  They’ll glue it together and put in the spring.  After they know the magnets correct orientation they can proceed with placing metal along with wires and use it as the touch sensor.

As it turns out the Atmel Qtouch library supported almost every ATTINY except the one they selected.  Ben and Felix turn to github where they find a library they can possibly use called tiny touch. It’s got an entire Atmel solution file attached to it, as well as, schematics that they can use with their Atmel microcontroller. The user even uses some machine language to do the timing for the neopixels. This allows you to know exactly how many cycles are executed. The code they are looking at works much like the official Qtouch libraries, but with a smaller code footprint.

After modifying code, Ben puts the prototype back together, and looks for the max resolution on his ADCs so he can get a detailed temperature reading from the glue gun.  He’s got a pair of 100K resistors in parallel to cut the resistance down to 50K, the value they want. Ben performs a soldering trick, heating up the wire just enough to cause plastic to contract. He uses a Rohde & Schwarz oscilloscope to double check the signals are in harmony.  He puts the case together, and modifies the code so that instead of blinking an LED when you touch the trigger, it changes the servo to its two different states, to retract and extend the stand.

 

Disclaimer

  • hack
  • super_glue_gun
  • heck
  • ben
  • tbhs_ep
  • episode 310: super glue gun 08: integrating all mechs
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +2
    Nice episode. Have you considered adding a couple of LED's near the output nozzle to illuminate the area where you apply the glue? DAB
  • makerkaren
    makerkaren over 8 years ago in reply to kingrahl +1
    Love your train of thought! Good idea with the cradle in place of the stand.
  • makerkaren
    makerkaren over 8 years ago in reply to beacon_dave +1
    It's not super stable right now, which I'm pretty concerned about. We're considering that we want to keep the nozzle as narrow as possible making it easier to get glue into tight spots. However, we want…
Parents
  • beacon_dave
    beacon_dave over 8 years ago

    Just wondering how stable the glue gun is when in the upright position ? Quite often the weight or springiness of the power cord has the tendency to pull lightweight tools over.

     

    A side-stand may be more stable in this respect but then it needs to be left or right handed which adds complexity to the design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 8 years ago in reply to beacon_dave

    It's not super stable right now, which I'm pretty concerned about. We're considering that we want to keep the nozzle as narrow as possible making it easier to get glue into tight spots. However, we want the stand to extend from the nozzle end, which can be limiting in stand width. An idea Ben had recently was to widen the base of the handle so that you get a tripod effect when the stand extends from the nozzle.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to makerkaren

    makerkaren - how about:

     

    • the stand at the front could be made to splay out more like a bipod as it deploys, as opposed to swinging down at a fixed width.
    • a case/holster which the glue gun can slot into when not in use (and that the power cord can wrap around) which also doubles up as a stand when in use.
    • have a stand incorporated into the base of the handle that is flush with the base of the handle when in use but then rotates 90 degrees as the stand at the front deploys.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 8 years ago in reply to beacon_dave

    We're currently looking at having the stand extend forward out from inside the area around the nozzle. I thought about trying to find a way to have it splay out, but I'm not sure how to execute it. It will depend on what mechanism Ben lands on to deploy the stand. We're looking at a sort of rack and pinion hooked to a continuous rotation servo right now.

     

    As for a separate stand like a soldering station, Ben is adamantly against it. He wants the user to be able to set the gun down anywhere.

     

    I don't think I'm quite following with how the secondary stand would work. I should also point out that we're running out of I/O, so adding another mechanism may not be possible with the hardware we're currently using.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to makerkaren

    makerkaren - cantilever / pantograph type linkages can give you a splaying out type action.

    ( BTW this guy has an impressive collection of mechanical linkage animations on YouTube:

    https://www.youtube.com/user/thang010146/videos?disable_polymer=1  )

     

    I don't think you necessarily need additional IO as you could probably link the two stand mechanisms  together with something like a Bowden cable and thus drive them from the same actuator. They are going to be deployed and retracted at the same time after all.

     

    I was thinking more of a scissor type action for the rear support. If you take a pair of scissors and lay them flat on a table, when closed, they are slender, but if opened so that the blades are 90 degrees from one another then they can provide a wider more stable base. With the glue gun, if the very bottom few mm's of the grip was able to rotate through 90 degrees then you would effectively be able to widen the base to make it more stable.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 8 years ago in reply to makerkaren

    makerkaren - cantilever / pantograph type linkages can give you a splaying out type action.

    ( BTW this guy has an impressive collection of mechanical linkage animations on YouTube:

    https://www.youtube.com/user/thang010146/videos?disable_polymer=1  )

     

    I don't think you necessarily need additional IO as you could probably link the two stand mechanisms  together with something like a Bowden cable and thus drive them from the same actuator. They are going to be deployed and retracted at the same time after all.

     

    I was thinking more of a scissor type action for the rear support. If you take a pair of scissors and lay them flat on a table, when closed, they are slender, but if opened so that the blades are 90 degrees from one another then they can provide a wider more stable base. With the glue gun, if the very bottom few mm's of the grip was able to rotate through 90 degrees then you would effectively be able to widen the base to make it more stable.