Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents Super Glue Gun 08: Integrating All Mechs -- Episode 310
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 23 Jul 2017 12:46 AM Date Created
  • Last Updated Last Updated: 29 Sep 2017 7:24 AM
  • Views 3325 views
  • Likes 5 likes
  • Comments 14 comments
Related
Recommended

Super Glue Gun 08: Integrating All Mechs -- Episode 310

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Super Glue Gun
Community Feedback
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Previously, the team added the mechanism for the auto stand using a metal wire stand and a guitar string acting as a cable. The cable is actuated by a servo and utilizes a servo library for the Atmel ATTiny20 Microcontroller they are using.  Now they need to find a capacitive touch sensor library, possibly Qtouch from Atmel, to allow the auto stand to retract when your finger touches the trigger.

 

 

Ben goes to work on Autodesk Fusion 360 to design the parts he’ll need for 3D printing.  He filets the edges to form a round enclosure for the magnet and makes room for the capacitive touching piece.  After he’s printed the two piece he’s ready to build an autostand mock up.

He builds the mockup on top of an existing mock-up and puts it on the glue gun mech for testing before they do a redesign of the case. He flips the barrel around so that the hot block is at the top and gives them more room for their stand. He needs to use a spacer on it because the stand has an extremity that needs to be clear of the heater barrel. This requires hot gluing together the hot glue gun. When he’s done he got a proof of concept that he can use before they redesign the top half of the glue gun.

While Ben is working, Felix is researching the Qtouch library, a proprietary library for Atmel microcontrollers, for use with the touch sensor. Ben’s already printed out the holo trigger and put the magnet in place. The sensor will go on the front with the wire coming out the back.  They’ll glue it together and put in the spring.  After they know the magnets correct orientation they can proceed with placing metal along with wires and use it as the touch sensor.

As it turns out the Atmel Qtouch library supported almost every ATTINY except the one they selected.  Ben and Felix turn to github where they find a library they can possibly use called tiny touch. It’s got an entire Atmel solution file attached to it, as well as, schematics that they can use with their Atmel microcontroller. The user even uses some machine language to do the timing for the neopixels. This allows you to know exactly how many cycles are executed. The code they are looking at works much like the official Qtouch libraries, but with a smaller code footprint.

After modifying code, Ben puts the prototype back together, and looks for the max resolution on his ADCs so he can get a detailed temperature reading from the glue gun.  He’s got a pair of 100K resistors in parallel to cut the resistance down to 50K, the value they want. Ben performs a soldering trick, heating up the wire just enough to cause plastic to contract. He uses a Rohde & Schwarz oscilloscope to double check the signals are in harmony.  He puts the case together, and modifies the code so that instead of blinking an LED when you touch the trigger, it changes the servo to its two different states, to retract and extend the stand.

 

Disclaimer

  • hack
  • super_glue_gun
  • heck
  • ben
  • tbhs_ep
  • episode 310: super glue gun 08: integrating all mechs
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +2
    Nice episode. Have you considered adding a couple of LED's near the output nozzle to illuminate the area where you apply the glue? DAB
  • makerkaren
    makerkaren over 8 years ago in reply to kingrahl +1
    Love your train of thought! Good idea with the cradle in place of the stand.
  • makerkaren
    makerkaren over 8 years ago in reply to beacon_dave +1
    It's not super stable right now, which I'm pretty concerned about. We're considering that we want to keep the nozzle as narrow as possible making it easier to get glue into tight spots. However, we want…
Parents
  • f5kn
    f5kn over 8 years ago

    Have you seen the Prusa i3 Mk3?

    If not, check out their new extruding mechanism, with the dual Bondtech drive gears. With something like that (concave on the side instead of flat like your brass gear) your glue sticks would get a much better grip, and wouldn't bend on one side. As a bonus, it would also be slimmer than with a gear and a ball bearing.

     

    For the stand, I think you need a mechanism that would make the flipping action faster, snappier. So you don't have to wait for the thing to get to the proper position. Imagine if there's an emergency and you need to place the glue gun on your table as fast as you can...

    You could instead of making it flip into position, make the stand slide out like it was suggested in the video... though it could come down at an angle instead of straight, the side rods staying at the sides of the hot end when retracted, there would be nothing in the way, I don't think. My only concern would be with glue somehow getting stuck on the stand, preventing it from sliding back up and down again. So the flip could prove to be a better solution. Even though there's potential for failure there as well.

    Someone on Youtube suggested a heavy base kind of like that of a cordless drill, so the gun would stand upright. A simpler solution than a motorized stand.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • f5kn
    f5kn over 8 years ago

    Have you seen the Prusa i3 Mk3?

    If not, check out their new extruding mechanism, with the dual Bondtech drive gears. With something like that (concave on the side instead of flat like your brass gear) your glue sticks would get a much better grip, and wouldn't bend on one side. As a bonus, it would also be slimmer than with a gear and a ball bearing.

     

    For the stand, I think you need a mechanism that would make the flipping action faster, snappier. So you don't have to wait for the thing to get to the proper position. Imagine if there's an emergency and you need to place the glue gun on your table as fast as you can...

    You could instead of making it flip into position, make the stand slide out like it was suggested in the video... though it could come down at an angle instead of straight, the side rods staying at the sides of the hot end when retracted, there would be nothing in the way, I don't think. My only concern would be with glue somehow getting stuck on the stand, preventing it from sliding back up and down again. So the flip could prove to be a better solution. Even though there's potential for failure there as well.

    Someone on Youtube suggested a heavy base kind of like that of a cordless drill, so the gun would stand upright. A simpler solution than a motorized stand.