Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Documents SNES Classic Teardown -- Episode 320
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 7 Dec 2017 5:42 PM Date Created
  • Last Updated Last Updated: 8 Dec 2017 8:24 AM
  • Views 1549 views
  • Likes 6 likes
  • Comments 3 comments
Related
Recommended

SNES Classic Teardown -- Episode 320

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

The Learning Circuit
sudo Sergeant
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Felix happens to find an SNES classic Mini and Ben offers to tear it apart. In this episode, Ben does a teardown of the SNES classic to see what's inside, discusses the components that are inside, and compares the board to the NES classic mini from last year.

 

 

Like the NES classic, it comes with a nostalgic poster to remind you of the original SNES. Ben’s curious to see if they left the data connection on the USB port as that is how people hacked into the previous system.  The power and reset buttons move so they are functional , the cover for the controller port is designed to look like the old ports but they flip down to give you the same type of connector found on the Wiimote and NES Classic. In the back there is an HDMI out and a USB port designed to look like a DC in.  It comes with two controllers which was common before the PlayStation.  Like the NES classic before it, the cord to the controller is way too short which as Ben surmises is common with Japanese consoles.  It comes with an HDMI cord, something that is common nowadays.

Ben preferred the Sega Genesis to the SNES back in the day.   The original SNES was half the speed of the Sega Genesis and it had an 8-bit data bus even though it was a 16 bit console.  While the CPU was weak, the graphics and sound were far more advanced than the Sega Genesis.

Ben unscrews the SNES and finds a little separate board for the power switch and the reset button.  So far, the inside is looking a lot like the Mini NES classic. There’s the same RF shielding with a depression in it for the heatsink used for the system-on-on-a-chip.  Ben marked the connections for the controller.  He looks to see what’s under the shield. This also reminds Ben of the NES classic, which he has on hand if he wants to do a side by side comparison. It’s got an Allwinner R16 processor, positioned as a low-cost solution for IoT applications, with support for Android or Linux based software.  Next to it is the RAM, by that is a Macronix NAND flash device that holds the operating system and the games, on the left is an AXP223 highly-integrated power system management IC, and on the back there is a chip that drives the HDMI. Ben rips up the NES Classic mini so he can compare the insides directly.  A few traces and pads are different but it’s essentially the same thing. Minor differences aside, it has the same form factor and the same controller plugs.  The flash is the same, they went with a different vendor for the RAM, the power control chip is the same, and the HDMI chip is also the same.  The original NES mini had 2 GB of RAM whereas the SNES mini has 4GB of RAM.

Disclaimer

  • ram
  • nes classic mini
  • usb port
  • super nintendo classic
  • power system management ic
  • hack
  • snes classic teardown
  • hdmi
  • nintendo classic mini
  • ben heck
  • snes classic mini
  • nand flash
  • cpu
  • r16 processor
  • episode 320: snes classic teardown
  • heck
  • ben
  • ben heck teardown
  • tbhs_ep
  • linux
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +1
    Nice tear down. I am not surprised with the circuit reuse between the two systems. Economy of scale an lower nonrecurring engineering costs probably drove the decisions. Heaven forbid that they actually…
Parents
  • frezik
    frezik over 8 years ago

    Here's a good article about what it takes to emulate the SNES:

     

    https://arstechnica.com/gaming/2011/08/accuracy-takes-power-one-mans-3ghz-quest-to-build-a-perfect-snes-emulator/

     

    It's actually one of the harder consoles to emulate with complete accuracy. Now, SNES Mini has it easy because it doesn't have to aim for 100% accuracy on 100% of the titles. For PC emulators, though, it can easily take a 3GHz Intel CPU to get up to that level. Compare that to the Dolphin emulator, which is already doing pretty well at emulating many Wii(U) games.

     

    BTW--Dolphin's monthly progress reports are always a treat. They can be hard to follow if you don't know all the ins-and-outs of 3D graphics, but there's usually some fascinating tidbit in there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • frezik
    frezik over 8 years ago

    Here's a good article about what it takes to emulate the SNES:

     

    https://arstechnica.com/gaming/2011/08/accuracy-takes-power-one-mans-3ghz-quest-to-build-a-perfect-snes-emulator/

     

    It's actually one of the harder consoles to emulate with complete accuracy. Now, SNES Mini has it easy because it doesn't have to aim for 100% accuracy on 100% of the titles. For PC emulators, though, it can easily take a 3GHz Intel CPU to get up to that level. Compare that to the Dolphin emulator, which is already doing pretty well at emulating many Wii(U) games.

     

    BTW--Dolphin's monthly progress reports are always a treat. They can be hard to follow if you don't know all the ins-and-outs of 3D graphics, but there's usually some fascinating tidbit in there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • baldengineer
    baldengineer over 8 years ago in reply to frezik

    The article is 6 years old. It’s older than the Wii(U).

     

    You’re comparing 100% accuracy with something that, by your own admission, is “doing pretty well”—with [significant] monthly progress. Seems pretty obivous SNES 100% accuracy will be met, if it hasn’t already, long before Dolphin’s on the Wii(U).