element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum LED turn signal car light sequencer
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 35 subscribers
  • Views 2893 views
  • Users 0 members are here
Related

LED turn signal car light sequencer

e14 Contributor
e14 Contributor over 12 years ago

What about an LED turn signal car light sequencer?

Very usefull and pretty Dawn Light style.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +1
    I was Talking about something like this: www.youtube.com/watch
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor +1
    Rui The code to drive the neopixels is there in the post. The best way to learn is try yourself, you'll be amazed with how easy it can be by breaking it down into smaller chunks. Get hold of some neopixels…
  • splatten
    splatten over 8 years ago +1
    I've been working on a NeoPixel CANBus interface for a while now, I have various videos during development on YouTube: Brakes: www.youtube.com/watch Left Indicator: www.youtube.com/watch Right Indicator…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    I was Talking about something like this:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Woah that is awesome.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    Sequencing tail lights were on offer for some vehicles back in 1966.

     

    I built one back in the 80's using a 555 and 4017.

     

    The latest one I helped repair fitted into the lamp socket, and had a chip on it that detected the number of pulses and turned the LEDs on based on that.

    Each one was designed to be in a certain position within the 3 tail lights, and at all times one or more lamps were on.

    They also fitted an electronic flasher since the LED tailights didn't present enough load to flash correctly.

     

    There are a few circuits around for them, but as Samuel has pointed out, they may not be legal, so check first.

     

     

    The ones on the Audi can be done using neopixels and there is some code here.

    Wireless Challenge .... the other bit -2

    Wireless Challenge .... Beer Tap (the other bit) - 4  Assembly

     

    Whether they end up legal may be the issue due to various laws regarding angles, brightness, etc.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    Sequencing tail lights were on offer for some vehicles back in 1966.

     

    I built one back in the 80's using a 555 and 4017.

     

    The latest one I helped repair fitted into the lamp socket, and had a chip on it that detected the number of pulses and turned the LEDs on based on that.

    Each one was designed to be in a certain position within the 3 tail lights, and at all times one or more lamps were on.

    They also fitted an electronic flasher since the LED tailights didn't present enough load to flash correctly.

     

    There are a few circuits around for them, but as Samuel has pointed out, they may not be legal, so check first.

     

     

    The ones on the Audi can be done using neopixels and there is some code here.

    Wireless Challenge .... the other bit -2

    Wireless Challenge .... Beer Tap (the other bit) - 4  Assembly

     

    Whether they end up legal may be the issue due to various laws regarding angles, brightness, etc.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mcb1

    Can anyone help to create something like this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mcb1

    I have seen the circuit you are talking about I think thy call them knight rider circuits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    Rui

    The code to drive the neopixels is there in the post.

     

    The best way to learn is try yourself, you'll be amazed with how easy it can be by breaking it down into smaller chunks.

     

    Get hold of some neopixels from a supplier that has documentation and support (that excludes some of the asian suppliers).

    Try their demos and examples to get it working, then try modifying them to do different things.

     

    This builds your knowledge of using them. (for instance mine wouldn't do what I wanted but I discovered I was starting at 1 instead of zero)

    Then progress until you build what you want, and configure it as you want.

     

     

    If you want these instantly, then I suggest buying the Audi in the video.

    Sorry I have too many other projects to build these.

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    Possibly.

    I was referring to the triple tailights found in some of the sixties cars.

    The original electro mechanical device is VERY expensive ... hence the replacement units using electronics.

     

    The Audi one just starts at 1 and sequences to xx than starts again.

    They obviously detect the flasher signal or they don't use the traditional flasher which is also possible.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mcb1

    Audi uses since 2009, a digital blinker module on almost every model.

    So, no problems with the flashing cadence or load power consumption.

    There is also no problems with canbus errors.

    Here in Europe, this is street legal as long as the brightness is the same as a OEM lamp.

    I'll try to build a prototype. Instead of a regular SMD led, I want to use some Cree led, much more powerful in brightness.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    Here in Europe, this is street legal as long as the brightness is the same as a OEM lamp.

    That's a benefit.

     

    You might be surprised how bright the Neopixels are running at 5v.

    There are the driver chips (WS2811) to allow you to use Super High brightness LEDs.

     

    IMO the Cree type would suit single lamp tailights, but not really suitable for the front indicator shown in the video.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mcb1

    My car is an audi a3 sportback 2009. Non xenon. So no problem with space for the lights.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kingrahl
    kingrahl over 12 years ago in reply to e14 Contributor

    Rui Lima wrote:

     

    Can anyone help to create something like this.

    Here is a link to the wiring diagram and parts to the circuit I had previously mentioned. http://homemadecircuitsandschematics.blogspot.com/2011/12/how-to-make-car-led-chasing-tail-light.html

     

    If you wish to sequence more than 6 LEDs, you will either need to program a microcontroller or connect multiples of this circuit in a series.

     

    The title describes it as a taillight/ brake light circuit. In the description, it mentions the circuit may also be connected to the turn signals.